L-com Global Connectivity
  
Cart is Empty
  
USA & Canada (800) 341-5266     International +1 (978) 682-6936

L-com Launches Ceiling-Mount Public Safety DAS Antenna
(Thursday, August 18, 2016)
 

NORTH ANDOVER, Mass. (August 18, 2016) - L-com Global Connectivity, a preferred manufacturer of wired and wireless connectivity products, announced today that it has released a ceiling-mount public safety DAS antenna.

L-com’s HyperLink brand HG35805CUPR-NF is an IP67-rated, multi-band, low-PIM, Omni-directional, ceiling-mount antenna specifically designed for in-building wireless networks.  With coverage from 380 MHz to 6000 MHz, this antenna is ideal for standard and public safety Distributed Antenna Systems (DAS) used to disseminate Cellular/LTE and Wi-Fi signals throughout an area or building.

“The HG35805CUPR-NF was designed to be an integral part of a public safety DAS network. Not only does it provide coverage for both cellular and Wi-Fi networks, it can provide low-band coverage allowing public safety services and first responders to stay connected within a specific location or structure during emergency situations,” said Ken Burgner, Product Manager.

With low-band operational coverage down to 380 MHz, this antenna supports UHF, 600 MHz, 1390-1432 MHz, AWS-3 bands and TETRA-compliant 2-way radios.  It has a low-PIM rating of <-150 dBc which meets low-PIM requirements for LTE/4G bands and DAS applications. The multi-band design allows one antenna to be used for an array of in-building, wide-coverage wireless applications, which simplifies installation.

The HG35805CUPR-NF is designed to be aesthetically pleasing in almost any indoor environment. It can be easily mounted through a single 1.0 inch hole in a solid or suspended ceiling up to 1.2 inches thick. It features a 12 inch coax lead terminated with an N-Female connector. Special order connectors are also available.

For more information about this release, please contact:
Peter McNeil, Marketing Manager
978-682-6936 x1174, pmcneil@l-com.com

About L-com Global Connectivity:

L-com Global Connectivity, a preferred manufacturer of wired and wireless connectivity products, offers a wide range of solutions and unrivaled customer service for the electronics and data communications industries. The company's product portfolio includes cable assemblies, connectors, adapters, computer networking equipment, and custom products, as well as their HyperLink® brand of wireless products which include antennas, RF amplifiers, coaxial lightning and surge protectors, and NEMA rated enclosures. L-com's HyperLink® wireless products are designed for WiFi, WiMAX, SCADA, 802.11a/b/g/n/ac, RFID and Bluetooth applications. In addition to HyperLink® , L-com’s other brands include MilesTek®, specialists in Military/Aeronautics connectivity solutions, Aiconics®, a leading manufacturer of electrical connector products and Point Six™ Wireless, pioneers in the design and manufacture of wireless sensors used in IoT applications. Trusted for more than 30 years, L-com, which is headquartered in North Andover, Mass., is ISO 9001: 2008 certified and many of its products are UL® recognized. For more information, please visit:  http://www.L-com.com/

Other press releases that may be of interest to you:
 
5/30/2018 L-com Launches New Ruggedized, IP68-Rated, Electroless Nickel Finish, Cat6 Receptacles, Plugs and Jam Nuts
5/25/2018 L-com Releases New High-Flex, Continuous Motion, Braided Shield Ethernet Cable Assemblies
5/23/2018 L-com Debuts New Tool-less RJ45 Jacks with PoE+ Compliance
5/3/2018 L-com Introduces a New Series of Data-line Lightning and Surge Protectors for Ethernet and Serial Data Applications
4/26/2018 L-com Now Stocks Icron Technologies’ New Raven USB 3-2-1 Extenders
4/25/2018 L-com Launches New Line of Coaxial RF Lightning and Surge Protectors
4/9/2018 L-com Introduces New IP67 Category5e/6 Dual Use Waterproof Ethernet Cables
3/8/2018 L-com Releases USB 2.0 Type-C Cables with Panel-Mount Connectors
3/6/2018 L-com Launches New 20-Pin DisplayPort Cables with Power Support
3/5/2018 L-com Appoints M-RF Co., Ltd. as Authorized Distributor in Japan
2/27/2018 L-com Now Stocking High-Flex USB 3.0 Cable Assemblies with Type-A to Type-C Connectors
2/22/2018 L-com Introduces New Low-Smoke Zero-Halogen USB 2.0 Bulk Cable with 28/28 AWG Conductors
2/20/2018 L-com Releases Cat5e/6 Patch Panels with PoE + Interfaces
2/15/2018 L-com Launches New IP67-Rated Industrial USB 3.0 Cable Assemblies and Coupler
1/31/2018 L-com Now Offers Waterproof IP67-Rated USB Type-A/A Cable Assemblies
1/30/2018 L-com Unveils New Extended-Length Active HDMI Cables
1/26/2018 L-com Releases M12 and M8 Field Term Connectors, Couplers, Adapters and Receptacles
1/25/2018 L-com Launches New Plenum Rated, Shielded Cat6 Cable Assemblies with 23 AWG Solid Conductors
1/18/2018 L-com Introduces New Cat6a Low-Smoke Zero-Halogen Cable Assemblies and Bulk Cable
11/28/2017 L-com Releases a New Line of Versatile HDMI Adapters
  Page:  1 of 25
    
 
Free Newsletter
L-com Global Connectivity           50 High Street           North Andover, MA 01845
www.L-com.com E-mail: sales@L-com.com 1-800-341-5266 www.Facebook.com/LcomGlobal


© Infinite Electronics International, Inc.
an Infinite company