L-com Global Connectivity
  
Cart is Empty
  
USA & Canada (800) 341-5266     International +1 (978) 682-6936

To our valued customers: Our offices will be closed Monday, May 28th, in observance of the Memorial Day holiday.

L-com Introduces Plenum-Rated, Low-PIM Coaxial Cable Assemblies
(Thursday, April 14, 2016)
 

Low-PIM Coax CableNORTH ANDOVER, Mass. (April 14, 2016) - L-com Global Connectivity, a preferred manufacturer of wired and wireless connectivity products, announced today that it has launched two series of plenum-rated, low-PIM coaxial cable assemblies. 

L-com’s RG401 and RG402 plenum-rated, low-PIM cable assemblies are constructed using jacketed, high-performance, formable RG401 or RG402 coaxial cable. These plenum-rated cable assemblies feature passive intermodulation (PIM) specifications as low as -150dBc and are ideal for applications that incorporate Distributed Antenna Systems (DAS). These cable assemblies are available with either 7/16 DIN Male or Type N-Male connectors.

“High levels of PIM in the transmission path directly result in poor performance of a DAS network. Our plenum-rated, low-PIM coaxial cable assemblies ensure strong signal and more bandwidth by limiting PIM in the connection between wireless components,” said Ken Burgner, Product Manager.

L-com’s RG401 and RG402 plenum-rated, low-PIM cable assemblies are built to order using an online cable configurator. The configurator allows customers to price and purchase cables that are designed to their specifications through L-com’s website. Customers can select the cable type, connectors, and length in inches, feet or meters. The configurator generates pricing for the custom cable, which can then be added to the online cart, allowing customers to order specifically what they need.

Low-PIM RG401 and RG402 bulk cable is also available by the foot for those who want to build their own cable assemblies. In addition to low-PIM cable and cable assemblies, L-com also offers low-PIM coax connectors, coax adapters, coax lightning protectors, and antennas.

For more information about this release, please contact:
Peter McNeil, Marketing Manager
978-682-6936 x1174, mailto:pmcneil@l-com.com

About L-com Global Connectivity

L-com Global Connectivity, a preferred manufacturer of wired and wireless connectivity products, offers a wide range of solutions and unrivaled customer service for the electronics and data communications industries. The company's product portfolio includes cable assemblies, connectors, adapters, computer networking equipment, and custom products, as well as their HyperLink® brand of wireless products which include antennas, RF amplifiers, coaxial lightning and surge protectors, and NEMA rated enclosures. L-com's HyperLink® wireless products are designed for WiFi, WiMAX, SCADA, 802.11a/b/g/n/ac, RFID and Bluetooth applications. In addition to HyperLink® , L-com’s other brands include MilesTek®, specialists in Military/Aeronautics connectivity solutions, Aiconics®, a leading manufacturer of electrical connector products and Point Six™ Wireless, pioneers in the design and manufacture of wireless sensors used in IoT applications. Trusted for more than 30 years, L-com, which is headquartered in North Andover, Mass., is ISO 9001: 2008 certified and many of its products are UL® recognized. For more information, please visit:  http://www.L-com.com/


Other press releases that may be of interest to you:
 
5/23/2018 L-com Debuts New Tool-less RJ45 Jacks with PoE+ Compliance
5/3/2018 L-com Introduces a New Series of Data-line Lightning and Surge Protectors for Ethernet and Serial Data Applications
4/26/2018 L-com Now Stocks Icron Technologies’ New Raven USB 3-2-1 Extenders
4/25/2018 L-com Launches New Line of Coaxial RF Lightning and Surge Protectors
4/9/2018 L-com Introduces New IP67 Category5e/6 Dual Use Waterproof Ethernet Cables
3/8/2018 L-com Releases USB 2.0 Type-C Cables with Panel-Mount Connectors
3/6/2018 L-com Launches New 20-Pin DisplayPort Cables with Power Support
3/5/2018 L-com Appoints M-RF Co., Ltd. as Authorized Distributor in Japan
2/27/2018 L-com Now Stocking High-Flex USB 3.0 Cable Assemblies with Type-A to Type-C Connectors
2/22/2018 L-com Introduces New Low-Smoke Zero-Halogen USB 2.0 Bulk Cable with 28/28 AWG Conductors
2/20/2018 L-com Releases Cat5e/6 Patch Panels with PoE + Interfaces
2/15/2018 L-com Launches New IP67-Rated Industrial USB 3.0 Cable Assemblies and Coupler
1/31/2018 L-com Now Offers Waterproof IP67-Rated USB Type-A/A Cable Assemblies
1/30/2018 L-com Unveils New Extended-Length Active HDMI Cables
1/26/2018 L-com Releases M12 and M8 Field Term Connectors, Couplers, Adapters and Receptacles
1/25/2018 L-com Launches New Plenum Rated, Shielded Cat6 Cable Assemblies with 23 AWG Solid Conductors
1/18/2018 L-com Introduces New Cat6a Low-Smoke Zero-Halogen Cable Assemblies and Bulk Cable
11/28/2017 L-com Releases a New Line of Versatile HDMI Adapters
11/14/2017 L-com Launches New USB 2.0 ECF-Style Panel Mount USB Adapter Cables
10/26/2017 L-com Introduces New Line of Universal Sub-Panels with USB, DisplayPort and Cat6a RJ45 Couplers
  Page:  1 of 25
    
 
Free Newsletter
L-com Global Connectivity           50 High Street           North Andover, MA 01845
www.L-com.com E-mail: sales@L-com.com 1-800-341-5266 www.Facebook.com/LcomGlobal


© Infinite Electronics International, Inc.
an Infinite company