L-com Global Connectivity
  
Cart is Empty
  
USA & Canada (800) 341-5266     International +1 (978) 682-6936

L-com Now Offers UL® Listed Black NEMA Enclosures
(Thursday, March 03, 2016)
 

NORTH ANDOVER, Mass. (March 3, 2016) - L-com Global Connectivity, a preferred manufacturer of wired and wireless connectivity products, announced today that it has launched a new series of black UL® listed weatherproof industrial NEMA enclosures.

Constructed from molded halogen-free and self-extinguishing fiberglass reinforced polyester (FRP), these new enclosures are well suited for use in extreme temperature or corrosive environments.
 
The NBB121 series (12x10x5 in.), NBB100 series (10x8x5 in.), NBB141 series (14x12x7 in.), and NBB181 series  (10x8x5 in.) are available with aluminum mounting plates, non-metallic mounting plates or without mounting plates. The black color of these new NEMA enclosures makes them ideal for use in security and surveillance applications as they blend in seamlessly with existing municipal landscapes.

“Adding additional sizes and models to our existing NBB enclosure line gives our customers an even wider selection of standard products to choose from," said Ken Burgner, Product Manager. "Furthermore, we can build custom versions of these enclosures to address both wired and wireless applications," he added.

These new NEMA rated enclosures feature fully gasketed lids and integral mounting flanges that allow them to be mounted on walls and flat surfaces without the need for additional mounting hardware. Optional pole mounting kits are also available.

For more information about this release, please contact:
Peter McNeil, Marketing Manager
978-682-6936 x1174, mailto:pmcneil@l-com.com

About L-com Global Connectivity:

L-com Global Connectivity, a preferred manufacturer of wired and wireless connectivity products, offers a wide range of solutions and unrivaled customer service for the electronics and data communications industries. The company's product portfolio includes cable assemblies, connectors, adapters, computer networking equipment, and custom products, as well as their HyperLink® brand of wireless products which include antennas, RF amplifiers, coaxial lightning and surge protectors, and NEMA rated enclosures. L-com's HyperLink® wireless products are designed for WiFi, WiMAX, SCADA, 802.11a/b/g/n/ac, RFID and Bluetooth applications. In addition to HyperLink® , L-com’s other brands include MilesTek®, specialists in Military/Aeronautics connectivity solutions, Aiconics®, a leading manufacturer of electrical connector products and Point Six™ Wireless, pioneers in the design and manufacture of wireless sensors used in IoT applications. Trusted for more than 30 years, L-com, which is headquartered in North Andover, Mass., is ISO 9001: 2008 certified and many of its products are UL® recognized. For more information, please visit:  http://www.L-com.com/


Other press releases that may be of interest to you:
 
2/22/2018 L-com Introduces New Low-Smoke Zero-Halogen USB 2.0 Bulk Cable with 28/28 AWG Conductors
2/20/2018 L-com Releases Cat5e/6 Patch Panels with PoE + Interfaces
2/15/2018 L-com Launches New IP67-Rated Industrial USB 3.0 Cable Assemblies and Coupler
1/31/2018 L-com Now Offers Waterproof IP67-Rated USB Type-A/A Cable Assemblies
1/30/2018 L-com Unveils New Extended-Length Active HDMI Cables
1/26/2018 L-com Releases M12 and M8 Field Term Connectors, Couplers, Adapters and Receptacles
1/25/2018 L-com Launches New Plenum Rated, Shielded Cat6 Cable Assemblies with 23 AWG Solid Conductors
1/18/2018 L-com Introduces New Cat6a Low-Smoke Zero-Halogen Cable Assemblies and Bulk Cable
11/28/2017 L-com Releases a New Line of Versatile HDMI Adapters
11/14/2017 L-com Launches New USB 2.0 ECF-Style Panel Mount USB Adapter Cables
10/26/2017 L-com Introduces New Line of Universal Sub-Panels with USB, DisplayPort and Cat6a RJ45 Couplers
10/25/2017 L-com Releases New M12 Connectors, Coupler and Receptacles
10/24/2017 L-com Debuts New Windowed NEMA Enclosures
10/5/2017 L-com Launches New USB 3.0 High-Flex Cable Assemblies
10/3/2017 L-com Introduces Ruggedized IP68-Rated Cat6 Receptacles, Plugs and Jam Nuts
9/28/2017 L-com Debuts New USB 3.0 ECF-Style Panel Mount USB Adapter Cables
9/19/2017 L-com Introduces New USB 3.0 Armored Cables for Extreme Environments
9/14/2017 L-com Releases New USB 3.0 Bulk Cable
8/29/2017 L-com Debuts New High Flex HDMI Cable Assemblies
8/24/2017 L-com Launches new USB 2.0 and 3.0 Cables with Ferrite Beads
  Page:  1 of 25
    
 
Free Newsletter
L-com Global Connectivity           50 High Street           North Andover, MA 01845
www.L-com.com E-mail: sales@L-com.com 1-800-341-5266 www.Facebook.com/LcomGlobal


© L-com, Inc. All Rights Reserved. L-com, Inc., 50 High Street, West Mill, 3rd Floor, Suite #30, North Andover, MA 01845
an Infinite company