L-com Global Connectivity
  
Cart is Empty
  
USA & Canada (800) 341-5266     International +1 (978) 682-6936

L-com Introduces Slim-Line 28 AWG Ethernet Patch Cables
(Thursday, February 18, 2016)
 

NORTH ANDOVER, Mass. (February 18, 2016) - L-com Global Connectivity, a preferred manufacturer of wired and wireless connectivity products, announced today that it has launched two new series of slim-line 28 AWG Ethernet patch cables.

L-com’s new slim-line 28 AWG Ethernet patch cables are engineered for high-density patching applications. The patent pending spline-free design offers a reduced diameter profile, ideal for applications that require a smaller, more flexible cable. The low-profile short boot design saves additional space on the patch panel, giving a clean, organized look to patch bays.

 “L-com’s slim-line high-performance cable assemblies offer a 38% smaller cross-sectional area and a tighter bend radius than standard patch cables. This improves airflow in high-density patching applications and saves space in confined areas,” said Dave Gallagher, Product Manager.

These cables are available in performance ratings of Category 6 (TRD628BL-series) and Category 6A (TRD628ABL- series) and support data rates up to 10Gbps for high-speed voice, video, and data applications. They feature high-performance RJ45 plugs with molded boots and 50u gold plated contacts. The slim-line 28 AWG Ethernet patch cables are available off-the-shelf in lengths of 1 ft, 3 ft, 5 ft, 7 ft, 10 ft and 14 ft, and are also available in custom length and color variations.

For more information about this release, please contact:
Peter McNeil, Marketing Manager
978-682-6936 x1174, mailto:pmcneil@l-com.com

About L-com Global Connectivity:

L-com Global Connectivity, a preferred manufacturer of wired and wireless connectivity products, offers a wide range of solutions and unrivaled customer service for the electronics and data communications industries. The company's product portfolio includes cable assemblies, connectors, adapters, computer networking equipment, and custom products, as well as their HyperLink® brand of wireless products which include antennas, RF amplifiers, coaxial lightning and surge protectors, and NEMA rated enclosures. L-com's HyperLink® wireless products are designed for WiFi, WiMAX, SCADA, 802.11a/b/g/n/ac, RFID and Bluetooth applications. In addition to HyperLink® , L-com’s other brands include MilesTek®, specialists in Military/Aeronautics connectivity solutions, Aiconics®, a leading manufacturer of electrical connector products and Point Six™ Wireless, pioneers in the design and manufacture of wireless sensors used in IoT applications. Trusted for more than 30 years, L-com, which is headquartered in North Andover, Mass., is ISO 9001: 2008 certified and many of its products are UL® recognized. For more information, please visit:  http://www.L-com.com/


Other press releases that may be of interest to you:
 
10/10/2019 L-com Introduces New Pressure and Level Sensors to Address Growing IoT Applications
10/8/2019 L-com Introduces New GPS Timing Antennas and UHF Antenna to Address the Growing Mobile Wireless Market
10/1/2019 L-com Releases New Ethernet Lightning and Surge Protectors with PoE, PoE+ and PoE ++ Support
9/26/2019 L-com Launches New Low PIM Coaxial Surge Protectors with 4.3-10 Connectors
9/25/2019 L-com Introduces New 50/125, Multimode, OM3, OM4 and OM5 Fiber Cables with MPO, LC, SC and ST Connectors
9/10/2019 L-com Now Stocks Fixed RF Attenuators with SMA and Type-N Interfaces
8/13/2019 L-com Releases New Cat6 and Cat6a Plenum +105°C, 28AWG, Shielded, Slim Ethernet Patch Cords
8/8/2019 L-com Debuts New UL Listed NEMA-Rated Equipment Enclosures
8/6/2019 New Latching USB 3.0 Cable Assemblies Address Heavy Vibration Applications
8/1/2019 L-com Launches New Triple-Speed Ethernet Switches to Address Industrial Network Applications
7/30/2019 L-com Releases Cat6a Continuous Flex, ZHFR-PUR, Double Shielded Cable Assemblies
7/26/2019 L-com Debuts New Wall-Mount Cabinets and Racks to Address LAN Connectivity Applications
7/25/2019 L-com Introduces new Polycarbonate NEMA-Rated Equipment Enclosures for Wired and Wireless Applications
7/23/2019 L-com Releases New 1U and 2U Cat5e, Cat6 and Cat6a Patch Panels
7/18/2019 L-com Introduces New Active Optical Cables for use in High-Speed Data Center Applications
7/17/2019 L-com Launches New 900 MHz Omni and Sector Antennas
7/16/2019 L-com Unveils Premium 8-Position, A-code, M12 Cable Assemblies for Sensor, Actuator and Fieldbus Applications
7/11/2019 L-com Releases New OM5 Fiber Cables for High-Speed Data Center Applications
6/27/2019 L-com Releases New Small Cell and Outdoor Power Protection Enclosures
6/26/2019 L-com Adds New Premium RJ45 to M12 Female Panel-Mount Cable Assemblies
  Page:  1 of 28
    
 
Free Newsletter



L-com Global Connectivity           50 High Street           North Andover, MA 01845
www.L-com.com E-mail: sales@L-com.com 1-800-341-5266 www.Facebook.com/LcomGlobal


© Infinite Electronics International, Inc.