L-com Global Connectivity
  
Cart is Empty
  
USA & Canada (800) 341-5266     International +1 (978) 682-6936
 
L-com Releases 180-Degree MIMO Sector Antennas
(Thursday, November 19, 2015)
 

NORTH ANDOVER, Mass. (November 19, 2015) - L-com Global Connectivity, a preferred manufacturer of wired and wireless connectivity products, announced today that it has developed two MIMO sector antennas that provide true 180-degree coverage.

L-com’s HG2458-13P-180 is a 180-degree dual-band MIMO sector antenna that combines high-gain and dual-band support for applications in the 2.4 GHz (2400-2500 MHz) and 5 GHz (4900-5850 MHz) frequency bands.

“The HG2458-13P-180 stands out from our competitors sector antennas because it is a true 180-degree dual-band sector antenna that features patent pending technology,” said Ken Burgner, Product Manager.

The HG5813DP-180 is a 180-degree dual-polarized MIMO sector antenna. It delivers high-gain with vertical and horizontal polarization for applications in the 4.9 GHz to 5.8 GHz frequency bands.

“The HG5813DP-180 features the same patent pending technology as the HG2458-13P-180. This technology enables it to provide true 180-degree coverage in addition to dual-polarization,” added Burgner.

Both of these antennas feature a dual-feed system via two integral N-Female connectors. The HG2458-13P-180 antennas utilize a separate feed for 2.4 GHz and 5 GHz bandwidths. The HG5813DP-180 offers separate feeds for horizontal and vertical polarization.

These antennas feature heavy-duty UV-resistant plastic radomes for all-weather operation. Additionally, they are supplied with a stainless steel tilt and swivel mast mount kit, which allows installation with various degrees of up/down tilt for easy alignment.

For more information about this release, please contact:
Peter McNeil, Marketing Manager
978-682-6936 x1174, mailto:pmcneil@l-com.com

About L-com Global Connectivity:

L-com Global Connectivity, a preferred manufacturer of wired and wireless connectivity products, offers a wide range of solutions and unrivaled customer service for the electronics and data communications industries. The company's product portfolio includes cable assemblies, connectors, adapters, computer networking components, and custom products, as well as their HyperLink® brand of wireless products which include antennas, RF amplifiers, coaxial lightning and surge protectors, and NEMA rated enclosures. L-com's HyperLink® wireless products are designed for WiFi, WiMAX, SCADA, 802.11a/b/g/n/ac, RFID and Bluetooth applications. In addition to HyperLink® , L-com’s other brands include MilesTek®, specialists in Military/Aeronautics connectivity solutions and Aiconics®, a leading manufacturer of electrical connector products.  Trusted for more than 30 years, L-com, which is headquartered in North Andover, Mass., is ISO 9001: 2008 certified and many of its products are UL® recognized. For more information, please visit:  http://www.L-com.com/


Other press releases that may be of interest to you:
 
7/17/2018 L-com Introduces New Flat HDMI Cables for Tight Space A/V Applications
7/12/2018 L-com Introduces New IP67 Rated HDMI Cables and Coupler for Extreme Connectivity Applications
6/26/2018 L-com Expands MPO Fiber Cable Product Line with OM4 and OM3 24 Channel Assemblies
5/30/2018 L-com Launches New Ruggedized, IP68-Rated, Electroless Nickel Finish, Cat6 Receptacles, Plugs and Jam Nuts
5/25/2018 L-com Releases New High-Flex, Continuous Motion, Braided Shield Ethernet Cable Assemblies
5/23/2018 L-com Debuts New Tool-less RJ45 Jacks with PoE+ Compliance
5/3/2018 L-com Introduces a New Series of Data-line Lightning and Surge Protectors for Ethernet and Serial Data Applications
4/26/2018 L-com Now Stocks Icron Technologies’ New Raven USB 3-2-1 Extenders
4/25/2018 L-com Launches New Line of Coaxial RF Lightning and Surge Protectors
4/9/2018 L-com Introduces New IP67 Category5e/6 Dual Use Waterproof Ethernet Cables
3/8/2018 L-com Releases USB 2.0 Type-C Cables with Panel-Mount Connectors
3/6/2018 L-com Launches New 20-Pin DisplayPort Cables with Power Support
3/5/2018 L-com Appoints M-RF Co., Ltd. as Authorized Distributor in Japan
2/27/2018 L-com Now Stocking High-Flex USB 3.0 Cable Assemblies with Type-A to Type-C Connectors
2/22/2018 L-com Introduces New Low-Smoke Zero-Halogen USB 2.0 Bulk Cable with 28/28 AWG Conductors
2/20/2018 L-com Releases Cat5e/6 Patch Panels with PoE + Interfaces
2/15/2018 L-com Launches New IP67-Rated Industrial USB 3.0 Cable Assemblies and Coupler
1/31/2018 L-com Now Offers Waterproof IP67-Rated USB Type-A/A Cable Assemblies
1/30/2018 L-com Unveils New Extended-Length Active HDMI Cables
1/26/2018 L-com Releases M12 and M8 Field Term Connectors, Couplers, Adapters and Receptacles
  Page:  1 of 26
    
 
Free Newsletter
L-com Global Connectivity           50 High Street           North Andover, MA 01845
www.L-com.com E-mail: sales@L-com.com 1-800-341-5266 www.Facebook.com/LcomGlobal


© Infinite Electronics International, Inc.
an Infinite company