L-com Global Connectivity
  
Cart is Empty
  
USA & Canada (800) 341-5266     International +1 (978) 682-6936
New L-com USB Jack Dust Covers Have Lanyards
(Wednesday, December 12, 2012)
 

New L-com USB Jack Dust Covers Have Lanyards

L-com's new USB dust cover with lanyard attached to L-com's ECF style USB coupler

NORTH ANDOVER, MA - 12/12/12 - L-com, Inc., a designer and manufacturer of wired and wireless connectivity products, today released a new version of their popular USB connector dust covers, adding a plastic lanyard and modifying the grip. The lanyard ties the dust cap to a location close to the jack so that it is not lost when removed.

USB jack ports on equipment are large enough to allow damaging particulates and dust to enter when not in use. This challenge becomes greater as the equipment is used in dusty and dirty environments. L-com has long carried dust covers for the USB male plugs, the USB female jacks, and even the mini-B 5 and micro-B connectors. Until now, these covers were stand-alone items that could be lost when removed from the jack.  The lanyards built into the new covers are easy to screw-attach to the panel near the jack, and are ideal to use with L-com's ECF or UPM style panel mount products.

"We hear from a lot of customers who are using USB-connected products in the field," said Steve Smith, Product Manager. "In dusty wiring closets, factory settings, or outdoors, the jacks on these products can be damaged, ruining the connectivity and therefore the product itself. We listened to our customers and developed this solution for them."

The new dust covers are available for USB type A and type B female jacks, sold in packages of 10.  They will be stocked in L-com's Massachusetts fulfillment facility for same day shipment starting in January, 2013.

For a high resolution version of the image suitable for print publication, click here:
http://www.l-com.com/lcom_emails/2012/121212/cap_a_usb_lan_off.jpg

For more information about this release, please contact:
Dave Fallon, Internet Marketing Strategist
978-682-6936 x1169, dfallon@l-com.com

L-com, a global designer and manufacturer of wired and wireless connectivity products, offers a wide range of solutions and unmatched customer service for the audio/video, OEM, military/aerospace, IT, and wireless RF industries. The company's product portfolio includes cable assemblies, connectors, adapters, computer networking components, and custom products, as well as the HyperLink® line of wireless antennas, amplifiers, filters/splitters, lightning protectors, weatherproof enclosures, and much more. Trusted for more than 30 years, L-com, Inc. is headquartered in North Andover, Massachusetts, USA, and is ISO 9001: 2008-certified. For more information, please visit:  http://www.L-com.com/

###


Other press releases that may be of interest to you:
 
7/18/2019 L-com Introduces New Active Optical Cables for use in High-Speed Data Center Applications
7/17/2019 L-com Launches New 900 MHz Omni and Sector Antennas
7/16/2019 L-com Unveils Premium 8-Position, A-code, M12 Cable Assemblies for Sensor, Actuator and Fieldbus Applications
7/11/2019 L-com Releases New OM5 Fiber Cables for High-Speed Data Center Applications
6/27/2019 L-com Releases New Small Cell and Outdoor Power Protection Enclosures
6/26/2019 L-com Adds New Premium RJ45 to M12 Female Panel-Mount Cable Assemblies
6/13/2019 L-com Releases New Flat HDMI Cables with LSZH Jackets
5/23/2019 L-com Launches New Indoor and Outdoor-Rated Cat6a Lightning and Surge Protectors
5/14/2019 L-com Introduces New Cat7 LSZH Cable Assemblies for Shipboard, Aerospace and Defense Applications
5/9/2019 L-com Launches New M12 Field Termination Connectors and In-line Adapters to Address Industrial Networking Applications
5/7/2019 L-com Releases New Cat6a Outdoor-Rated, High-Flex Ethernet Cable Assemblies
4/25/2019 L-com Expands Outdoor Industrial Ethernet Cable Line with Additional Length Options Available with Same-Day Shipping
4/4/2019 L-com Releases New Patch Panels with N-Type Couplers and 0.630” D-Holes
4/2/2019 L-com Adds New Power Cords for Server, PC, Laptop, PDU Applications and More
3/21/2019 L-com now Stocks 12G-SDI, HD-BNC Connectors for use in Broadcast Video Applications
3/19/2019 L-com Launches New Line of Rugged Category 7 Cables with 10 Gig Rating for Outdoor and Industrial Applications
3/15/2019 L-com Launches Right-Angle USB 3.0 Cable Assemblies with Female Connectors
3/14/2019 L-com Introduces New Right-Angle Panel-Mount DisplayPort Cables
3/12/2019 L-com Unveils New DisplayPort to HDMI Cables with LSZH Jackets
3/5/2019 L-com Debuts New Line of Dual-Rated Slim-Line Ethernet Cables with Spline-Free Design and UL CM Burn Rating
  Page:  1 of 28
    
 
Free Newsletter
L-com Global Connectivity           50 High Street           North Andover, MA 01845
www.L-com.com E-mail: sales@L-com.com 1-800-341-5266 www.Facebook.com/LcomGlobal


© Infinite Electronics International, Inc.