L-com Global Connectivity
  
Cart is Empty
  
USA & Canada (800) 341-5266     International +1 (978) 682-6936
L-com Adds New Right Angle USB Cables to Address Confined Space Applications
(Friday, December 07, 2012)
 

L-com Adds New Right Angle USB Cables to Address Confined Space Applications

L-com's Right Angle USB Cables

NORTH ANDOVER, MA - 12/7/12 - L-com, Inc., a designer and manufacturer of wired and wireless connectivity products, has expanded its line of right angle USB cable assemblies to address confined and tight space USB connectivity applications.

L-com has added 18 new configurations to its highly successful right angle USB cable series. These new angled USB 2.0 cable assemblies feature every right angle combination off-the-shelf.
L-com's specialized USB cables solve difficult connection issues in tight places. Each cable assembly is constructed with USB 2.0 compliant cable with 26 AWG power leads and feature 30 micro-inch gold plated contacts which provide reliable connections even with repeated mating cycles. Additionally, eight lengths are available for each series ranging from 0.3 meters to 5 meters.

"We have seen great success with the initial release of our right angle USB series," said Steve Smith, Product Manager. "We were seeing more requests coming in for different right angle combinations that became custom cable orders. By adding these additional new configurations to our stock product offering, we can provide faster delivery and easier ordering for our customers."

The angled USB cables are now available for shipment and can be ordered directly from L-com or from
L-com's authorized distributors.  A .pdf tip explaining the different right angle combinations is available for free download from L-com's website.

For a high resolution version of the image suitable for print publication, click here:
http://www.l-com.com/lcom_emails/2012/120712/ca90la_90lb_m.jpg

For more information about this release, please contact:
Dave Fallon, Internet Marketing Strategist
978-682-6936 x1450, newsletters@L-com.com

L-com, a global designer and manufacturer of wired and wireless connectivity products, offers a wide range of solutions and unmatched customer service for the electronics and data communications industries. The company's product portfolio includes cable assemblies, connectors, adapters, computer networking components, and custom products, as well as the Hyperlink line of wireless products. Trusted for more than 30 years, L-com, Inc. is headquartered in North Andover, Mass., and is ISO 9001: 2008-certified. For more information, please visit: http://www.L-com.com/

###

 


Other press releases that may be of interest to you:
 
1/18/2018 L-com Introduces New Cat6a Low-Smoke Zero-Halogen Cable Assemblies and Bulk Cable
11/28/2017 L-com Releases a New Line of Versatile HDMI Adapters
11/14/2017 L-com Launches New USB 2.0 ECF-Style Panel Mount USB Adapter Cables
10/26/2017 L-com Introduces New Line of Universal Sub-Panels with USB, DisplayPort and Cat6a RJ45 Couplers
10/25/2017 L-com Releases New M12 Connectors, Coupler and Receptacles
10/24/2017 L-com Debuts New Windowed NEMA Enclosures
10/5/2017 L-com Launches New USB 3.0 High-Flex Cable Assemblies
10/3/2017 L-com Introduces Ruggedized IP68-Rated Cat6 Receptacles, Plugs and Jam Nuts
9/28/2017 L-com Debuts New USB 3.0 ECF-Style Panel Mount USB Adapter Cables
9/19/2017 L-com Introduces New USB 3.0 Armored Cables for Extreme Environments
9/14/2017 L-com Releases New USB 3.0 Bulk Cable
8/29/2017 L-com Debuts New High Flex HDMI Cable Assemblies
8/24/2017 L-com Launches new USB 2.0 and 3.0 Cables with Ferrite Beads
8/22/2017 L-com Introduces New Mini-HDMI to Mini-HDMI Cables
7/25/2017 L-com Releases IP68 Fiber Plugs, Receptacles and Jam Nuts
7/18/2017 L-com Debuts New Line of Space Saving Mini-Coupler Patch Panels
7/11/2017 L-com Launches New Line of IP68-Rated Cable Glands and Couplers
6/29/2017 L-com Introduces Cat6 Low-Smoke Zero-Halogen Cable Assemblies
6/22/2017 L-com Expands Portfolio of Outdoor Cables for Industrial Ethernet Applications
6/20/2017 L-com Releases Cat5e TPE and PUR High Flex Outdoor Industrial Ethernet Cables
  Page:  1 of 25
    
 
Free Newsletter
L-com Global Connectivity           50 High Street           North Andover, MA 01845
www.L-com.com E-mail: sales@L-com.com 1-800-341-5266 www.Facebook.com/LcomGlobal


© L-com, Inc. All Rights Reserved. L-com, Inc., 50 High Street, West Mill, 3rd Floor, Suite #30, North Andover, MA 01845
an Infinite company