L-com Global Connectivity
  
Cart is Empty
  
USA & Canada (800) 341-5266     International +1 (978) 682-6936
L-com Introduces All-in-One HyperLink PoE DC Injectors/Power Supplies
(Friday, August 31, 2012)
 

L-com Introduces All-in-One HyperLink PoE DC Injectors/Power Supplies

L-com's HyperLink All-in-One Wall Mount PoE Midspan

NORTH ANDOVER, MA - 08/31/12 - L-com, Inc., a designer and manufacturer of wired and wireless connectivity products, has introduced a new line of HyperLink brand Power-over-Ethernet (PoE) Injector/Midspans with integral power supplies. These devices simplify PoE installations since a separate DC Injector and Power Supply are not required. These all-in-one Injector/Power Supplies are available in 12VDC, 24VDC, 48VDC, and 56VDC voltages.

In addition to the standard desktop type models which are commonly offered in the industry, L-com also offers its new wall mount models. These compact all-in-one Injectors/Power Supplies can be plugged directly into a wall electrical outlet, eliminating the need for additional power cables. This simplicity and size easily fits in crowded spaces such as 120V AC Industrial Enclosures and AC Universal Outlet Enclosures. All models feature built in protection circuits and are either IEEE 802.3af or 802.3af/at compatible depending on the model.

"Everything is getting smaller and tighter when it comes to connectivity," said Patrick Pesa, L-com's Director of Product Development. "We are actively working on ways to make the setup of networked equipment smaller and easier for our users so they can maximize the use of their networking equipment spaces."

All of the new PoE midspans are in stock at L-com's HyperLink distribution center in Florida, USA, for shipment on the same day that orders are received. The L-com website features free downloads of datasheets, diagrams, and 2D drawings for these products.

For a high resolution version of the image suitable for print publication, click here:
http://www.l-com.com/lcom_emails/2012/083112/PSW1212_POE.jpg

For more information about this release, please contact:
Dave Fallon, Internet Marketing Strategist
978-682-6936 x1450, newsletters@L-com.com

L-com, a global designer and manufacturer of wired and wireless connectivity products, offers a wide range of solutions and unmatched customer service for the electronics and data communications industries. The company's product portfolio includes cable assemblies, connectors, adapters, computer networking components, and custom products, as well as the Hyperlink line of wireless products. Trusted for more than 30 years, L-com, Inc. is headquartered in North Andover, Mass., and is ISO 9001: 2008-certified. For more information, please visit: http://www.L-com.com/

###


Other press releases that may be of interest to you:
 
8/13/2019 L-com Releases New Cat6 and Cat6a Plenum +105°C, 28AWG, Shielded, Slim Ethernet Patch Cords
8/8/2019 L-com Debuts New UL Listed NEMA-Rated Equipment Enclosures
8/6/2019 New Latching USB 3.0 Cable Assemblies Address Heavy Vibration Applications
8/1/2019 L-com Launches New Triple-Speed Ethernet Switches to Address Industrial Network Applications
7/30/2019 L-com Releases Cat6a Continuous Flex, ZHFR-PUR, Double Shielded Cable Assemblies
7/26/2019 L-com Debuts New Wall-Mount Cabinets and Racks to Address LAN Connectivity Applications
7/25/2019 L-com Introduces new Polycarbonate NEMA-Rated Equipment Enclosures for Wired and Wireless Applications
7/23/2019 L-com Releases New 1U and 2U Cat5e, Cat6 and Cat6a Patch Panels
7/18/2019 L-com Introduces New Active Optical Cables for use in High-Speed Data Center Applications
7/17/2019 L-com Launches New 900 MHz Omni and Sector Antennas
7/16/2019 L-com Unveils Premium 8-Position, A-code, M12 Cable Assemblies for Sensor, Actuator and Fieldbus Applications
7/11/2019 L-com Releases New OM5 Fiber Cables for High-Speed Data Center Applications
6/27/2019 L-com Releases New Small Cell and Outdoor Power Protection Enclosures
6/26/2019 L-com Adds New Premium RJ45 to M12 Female Panel-Mount Cable Assemblies
6/13/2019 L-com Releases New Flat HDMI Cables with LSZH Jackets
5/23/2019 L-com Launches New Indoor and Outdoor-Rated Cat6a Lightning and Surge Protectors
5/14/2019 L-com Introduces New Cat7 LSZH Cable Assemblies for Shipboard, Aerospace and Defense Applications
5/9/2019 L-com Launches New M12 Field Termination Connectors and In-line Adapters to Address Industrial Networking Applications
5/7/2019 L-com Releases New Cat6a Outdoor-Rated, High-Flex Ethernet Cable Assemblies
4/25/2019 L-com Expands Outdoor Industrial Ethernet Cable Line with Additional Length Options Available with Same-Day Shipping
  Page:  1 of 28
    
 
Free Newsletter
L-com Global Connectivity           50 High Street           North Andover, MA 01845
www.L-com.com E-mail: sales@L-com.com 1-800-341-5266 www.Facebook.com/LcomGlobal


© Infinite Electronics International, Inc.