L-com Global Connectivity
  
Cart is Empty
  
USA & Canada (800) 341-5266     International +1 (978) 682-6936

To our valued customers: Our offices will be closed Monday, May 27th, in observance of the Memorial Day Holiday.

L-com's Metal Armored USB Cables Resist Up To 1500 PSI Crushes and Impacts
(Thursday, August 16, 2012)
 

L-com's Metal Armored USB Cables Resist Up To 1500 PSI Crushes and Impacts

Metal Armored USB Cable - Type A - A Connectors, Revision 2.0 CompliantNORTH ANDOVER, MA - 08/16/12 - L-com, Inc., a designer and manufacturer of wired and wireless connectivity products, has released two new USB 2.0 cable assembly lines with metal armor around the cables. The new Type A male to Type A male and Type A male to Type B male cables boast a crush resistance of 1500 PSI (Pounds per Square Inch).

L-com's extensive USB cabling offering has long included many unique products such as latching USB cables, high flex USB cables, right angle USB cables, and waterproof USB cables. These new armored USB cables are needed for many applications including military/aerospace, security, medical facility, and industrial environment applications. Last week, L-com announced that they now carry armored HDMI cables for similar applications.

"We've dedicated a lot of our resources to finding niche solutions to common problems with USB cabling," said Steve Smith, Product Manager. "Providing a crush-resistant option is one of our many USB products we stock or custom manufacture."

The new armored USB cables are expected to be stocked in seven different length options in L-com's Massachusetts, USA distribution center for same-day shipment. Engineering drawings are available for free download on L-com's website.

For a high-resolution version of the image suitable for print publication, please click here:
http://www.l-com.com/lcom_emails/2012/081612/CSMUAA_MT_.jpg

For more information about this release, please contact:
Dave Fallon, Internet Marketing Strategist
978-682-6936 x1450, newsletters@L-com.com

L-com, a global designer and manufacturer of wired and wireless connectivity products, offers a wide range of solutions and unmatched customer service for the electronics and data communications industries. The company's product portfolio includes cable assemblies, connectors, adapters, computer networking components, and custom products, as well as the Hyperlink line of wireless products. Trusted for more than 30 years, L-com, Inc. is headquartered in North Andover, Mass., and is ISO 9001: 2008-certified. For more information, please visit: http://www.L-com.com/

###


Other press releases that may be of interest to you:
 
5/23/2019 L-com Launches New Indoor and Outdoor-Rated Cat6a Lightning and Surge Protectors Supporting 10/100/1000/10000 Applications
5/14/2019 L-com Introduces New Cat7 LSZH Cable Assemblies for Shipboard, Aerospace and Defense Applications
5/9/2019 L-com Launches New M12 Field Termination Connectors and In-line Adapters to Address Industrial Networking Applications
5/7/2019 L-com Releases New Cat6a Outdoor-Rated, High-Flex Ethernet Cable Assemblies
4/25/2019 L-com Expands Outdoor Industrial Ethernet Cable Line with Additional Length Options Available with Same-Day Shipping
4/4/2019 L-com Releases New Patch Panels with N-Type Couplers and 0.630” D-Holes
4/2/2019 L-com Adds New Power Cords for Server, PC, Laptop, PDU Applications and More
3/21/2019 L-com now Stocks 12G-SDI, HD-BNC Connectors for use in Broadcast Video Applications
3/19/2019 L-com Launches New Line of Rugged Category 7 Cables with 10 Gig Rating for Outdoor and Industrial Applications
3/15/2019 L-com Launches Right-Angle USB 3.0 Cable Assemblies with Female Connectors
3/14/2019 L-com Introduces New Right-Angle Panel-Mount DisplayPort Cables
3/12/2019 L-com Unveils New DisplayPort to HDMI Cables with LSZH Jackets
3/5/2019 L-com Debuts New Line of Dual-Rated Slim-Line Ethernet Cables with Spline-Free Design and UL CM Burn Rating
2/28/2019 L-com Releases New USB 3.1 Gen 2 Type-C Cables with Low-Smoke Zero-Halogen and PVC Jackets
2/21/2019 L-com Debuts New Cat5e, Cat6 and Cat6a Universal Sub-panels with PoE+ Compliant Jacks
2/14/2019 L-com Introduces New RJ45 Termination Block for Field Termination and Repair Applications
2/12/2019 L-com Debuts New Black and White Flat Cat5e and Cat6 Ethernet Cables
2/7/2019 L-com Releases New Cat5e Double-Shielded Outdoor High-Flex PoE Industrial Ethernet Cables
2/5/2019 L-com Debuts New Fiber LC Couplers with Internal Dustproof Shutters
1/31/2019 L-com Releases Aerial and Outdoor Bulk Cable for use in Demanding OSP Networks
  Page:  1 of 27
    
 
Free Newsletter
L-com Global Connectivity           50 High Street           North Andover, MA 01845
www.L-com.com E-mail: sales@L-com.com 1-800-341-5266 www.Facebook.com/LcomGlobal


© Infinite Electronics International, Inc.