L-com Global Connectivity
  
Cart is Empty
  
USA & Canada (800) 341-5266     International +1 (978) 682-6936

To our valued customers: Our offices will be closed Monday, May 27th, in observance of the Memorial Day Holiday.

L-com Adds New Sizes to Its Non-Powered Weatherproof Industrial Enclosures Line
(Monday, August 13, 2012)
 

L-com Adds New Sizes to Its Non-Powered Weatherproof Industrial Enclosures Line

16x14x6 Inch UL® Listed Weatherproof NEMA 4X Enclosures with Blank Aluminum or Blank Non-Metallic Mounting Plate

NORTH ANDOVER, MA - 8/13/12 - L-com, Inc., a designer and manufacturer of wired and wireless connectivity products, has added three new sized weatherproof industrial enclosures with and without mounting plates included to supplement their popular weatherproof enclosures: 8x6x4, 10x8x5, and 16x14x6 inch enclosures. The new options feature either a blank aluminum mounting plate, a blank non-metallic Starboard mounting plate, or no mounting plate included.  The mounting plates can be custom drilled on-location to suit the equipment that is stored within the boxes.

L-com's non-powered industrial enclosures are popular for their many size options and broad range of applications that they can be used in.  All of them are designed to be installed to hold sensitive equipment in locations where weather, impact, or security are issues. Without the power outlets that are featured in L-com's 240V AC powered enclosures and 120V AC powered enclosures, the non-powered enclosures can offer more room for equipment that does not need AC power or that can accept direct Power over Ethernet.

"We have carried other sized enclosures for a long time and they have been very popular," said Patrick Pesa, Director of Product Development. "We know we cannot plan for every one of the myriad applications for our enclosures, so offering a large variety of sizes and mounting options helps accommodate the majority of our customers."

Along with the enclosure/plate kits, L-com sells the mounting plates separately, and they can custom-drill mounting plates in their factory upon request.

For a high-resolution version of the image suitable for print publication, click here:
http://www.l-com.com/lcom_emails/2012/081312/NB161406_KIT.jpg

For more information about this release, please contact:
Dave Fallon, Internet Marketing Strategist
978-682-6936 x1450, newsletters@L-com.com

L-com, a global designer and manufacturer of wired and wireless connectivity products, offers a wide range of solutions and unmatched customer service for the electronics and data communications industries. The company's product portfolio includes cable assemblies, connectors, adapters, computer networking components, and custom products, as well as the Hyperlink line of wireless products. Trusted for more than 30 years, L-com, Inc. is headquartered in North Andover, Mass., and is ISO 9001: 2008-certified. For more information, please visit: http://www.L-com.com/

###


Other press releases that may be of interest to you:
 
5/14/2019 L-com Introduces New Cat7 LSZH Cable Assemblies for Shipboard, Aerospace and Defense Applications
5/9/2019 L-com Launches New M12 Field Termination Connectors and In-line Adapters to Address Industrial Networking Applications
5/7/2019 L-com Releases New Cat6a Outdoor-Rated, High-Flex Ethernet Cable Assemblies
4/25/2019 L-com Expands Outdoor Industrial Ethernet Cable Line with Additional Length Options Available with Same-Day Shipping
4/4/2019 L-com Releases New Patch Panels with N-Type Couplers and 0.630” D-Holes
4/2/2019 L-com Adds New Power Cords for Server, PC, Laptop, PDU Applications and More
3/21/2019 L-com now Stocks 12G-SDI, HD-BNC Connectors for use in Broadcast Video Applications
3/19/2019 L-com Launches New Line of Rugged Category 7 Cables with 10 Gig Rating for Outdoor and Industrial Applications
3/15/2019 L-com Launches Right-Angle USB 3.0 Cable Assemblies with Female Connectors
3/14/2019 L-com Introduces New Right-Angle Panel-Mount DisplayPort Cables
3/12/2019 L-com Unveils New DisplayPort to HDMI Cables with LSZH Jackets
3/5/2019 L-com Debuts New Line of Dual-Rated Slim-Line Ethernet Cables with Spline-Free Design and UL CM Burn Rating
2/28/2019 L-com Releases New USB 3.1 Gen 2 Type-C Cables with Low-Smoke Zero-Halogen and PVC Jackets
2/21/2019 L-com Debuts New Cat5e, Cat6 and Cat6a Universal Sub-panels with PoE+ Compliant Jacks
2/14/2019 L-com Introduces New RJ45 Termination Block for Field Termination and Repair Applications
2/12/2019 L-com Debuts New Black and White Flat Cat5e and Cat6 Ethernet Cables
2/7/2019 L-com Releases New Cat5e Double-Shielded Outdoor High-Flex PoE Industrial Ethernet Cables
2/5/2019 L-com Debuts New Fiber LC Couplers with Internal Dustproof Shutters
1/31/2019 L-com Releases Aerial and Outdoor Bulk Cable for use in Demanding OSP Networks
1/29/2019 L-com Now Stocks Moldable M12 Connecters for Rugged Applications
  Page:  1 of 27
    
 
Free Newsletter
L-com Global Connectivity           50 High Street           North Andover, MA 01845
www.L-com.com E-mail: sales@L-com.com 1-800-341-5266 www.Facebook.com/LcomGlobal


© Infinite Electronics International, Inc.