L-com Global Connectivity
  
Cart is Empty
  
USA & Canada (800) 341-5266     International +1 (978) 682-6936
L-com Introduces Armored HDMI Audio/Video Cable Assemblies
(Friday, August 10, 2012)
 

L-com Introduces Armored HDMI Audio/Video Cable Assemblies

Metal Armored HDMI®  Cable with Ethernet, Male/Male 0.5M

NORTH ANDOVER, MA - 8/10/12 - L-com, Inc., a designer and manufacturer of wired and wireless connectivity products, has introduced a line of HDMI audio/video cables with Ethernet that have a crush-resistant armor over the cable length. The new cables are available in either plastic armor, with a crush resistance of 1000 PSI (Pounds per Square Inch), or metal armor, with a crush resistance of 1500 PSI.

These cables have many applications where they would potentially be exposed to excessive force, such as military, security, and industrial environment applications. The cables feature 30 microinch gold plated contacts and double shielding to protect the sensitive audio and video signals from interference. The cables are stocked in six different lengths and will be available off-the-shelf for same day shipment.

"HDMI technology is used in many more applications than just home theater and digital signage," said Steve Smith, Product Manager. "We saw a need for HDMI connectivity in environments where the cables may be crushed or impacted, and often those environments are the type where downtime is not an option. We designed these cables to serve that market and we're happy to provide them off-the-shelf."

The new cables will be stocked in L-com's Massachusetts, USA, distribution center for same-day shipment. Specifications, a 2D engineering drawing, and 3D CAD models are all available on L-com's website for free download.

For a high-resolution image suitable for print publication, click here:
http://www.L-com.com/lcom_emails/2012/081012/hdcamt_.jpg

For more information about this release, please contact:
Dave Fallon, Internet Marketing Strategist
978-682-6936 x1450, newsletters@L-com.com

L-com, a global designer and manufacturer of wired and wireless connectivity products, offers a wide range of solutions and unmatched customer service for the electronics and data communications industries. The company's product portfolio includes cable assemblies, connectors, adapters, computer networking components, and custom products, as well as the Hyperlink line of wireless products. Trusted for more than 30 years, L-com, Inc. is headquartered in North Andover, Mass., and is ISO 9001: 2008-certified. For more information, please visit: http://www.L-com.com/

###


Other press releases that may be of interest to you:
 
7/18/2019 L-com Introduces New Active Optical Cables for use in High-Speed Data Center Applications
7/17/2019 L-com Launches New 900 MHz Omni and Sector Antennas
7/16/2019 L-com Unveils Premium 8-Position, A-code, M12 Cable Assemblies for Sensor, Actuator and Fieldbus Applications
7/11/2019 L-com Releases New OM5 Fiber Cables for High-Speed Data Center Applications
6/27/2019 L-com Releases New Small Cell and Outdoor Power Protection Enclosures
6/26/2019 L-com Adds New Premium RJ45 to M12 Female Panel-Mount Cable Assemblies
6/13/2019 L-com Releases New Flat HDMI Cables with LSZH Jackets
5/23/2019 L-com Launches New Indoor and Outdoor-Rated Cat6a Lightning and Surge Protectors
5/14/2019 L-com Introduces New Cat7 LSZH Cable Assemblies for Shipboard, Aerospace and Defense Applications
5/9/2019 L-com Launches New M12 Field Termination Connectors and In-line Adapters to Address Industrial Networking Applications
5/7/2019 L-com Releases New Cat6a Outdoor-Rated, High-Flex Ethernet Cable Assemblies
4/25/2019 L-com Expands Outdoor Industrial Ethernet Cable Line with Additional Length Options Available with Same-Day Shipping
4/4/2019 L-com Releases New Patch Panels with N-Type Couplers and 0.630” D-Holes
4/2/2019 L-com Adds New Power Cords for Server, PC, Laptop, PDU Applications and More
3/21/2019 L-com now Stocks 12G-SDI, HD-BNC Connectors for use in Broadcast Video Applications
3/19/2019 L-com Launches New Line of Rugged Category 7 Cables with 10 Gig Rating for Outdoor and Industrial Applications
3/15/2019 L-com Launches Right-Angle USB 3.0 Cable Assemblies with Female Connectors
3/14/2019 L-com Introduces New Right-Angle Panel-Mount DisplayPort Cables
3/12/2019 L-com Unveils New DisplayPort to HDMI Cables with LSZH Jackets
3/5/2019 L-com Debuts New Line of Dual-Rated Slim-Line Ethernet Cables with Spline-Free Design and UL CM Burn Rating
  Page:  1 of 28
    
 
Free Newsletter
L-com Global Connectivity           50 High Street           North Andover, MA 01845
www.L-com.com E-mail: sales@L-com.com 1-800-341-5266 www.Facebook.com/LcomGlobal


© Infinite Electronics International, Inc.