L-com Global Connectivity
  
Cart is Empty
  
USA & Canada (800) 341-5266     International +1 (978) 682-6936
L-com's New Dual Polarity Dish Antennas Provide 4.9-5.8 GHz Broadband Signal in Both Vertical and Horizontal Polarizations
(Thursday, August 09, 2012)
 

L-com's New Dual Polarity Dish Antennas Provide 4.9-5.8 GHz Broadband Signal in Both Vertical and Horizontal Polarizations

4.9-5.8 GHz Dual Polarity Dish Antenna

NORTH ANDOVER, MA - 8/9/12 - L-com, Inc., a designer and manufacturer of wired and wireless connectivity products, has added new dual polarity antennas to its already broad line of HyperLink brand MIMO / 802.11n antennas. The new antennas are designed for high performance in the 4.9 GHz to 5.8 GHz range of applications, including:

  • 4.9/5.1/5.3/5.4/5.8 GHz ISM and UNII Band applications
  • MIMO and IEEE 802.11a/n applications
  • 4.9 GHz Homeland Security and Public Safety Services applications
  • WiMAX applications
  • Long distance backhaul and Point to Point data links
  • Commercial installers
  • State and Federal Complexes
  • Transportation Terminals (Air, Train, Bus, etc)

The new dish antennas feature a strong, highly-directive signal beam particularly common in point-to-point applications. The dual polarity feature allows multi-thread communication, or transmitting data on one polarization and receiving it on the other simultaneously. There are three HyperLink models available with 25 dBi, 30 dBi, or 34 dBi gains.

"We have been supporting the important 4.9 GHz to 5.8 GHz band for years, but until now we did not have a dual polarity option with this much gain," said Patrick Pesa, Director of Product Development. "These antennas will allow superior wireless communication in many essential applications."

The new antennas use type N-Female connectors and include tilt and swivel mast mounting hardware so they can be shipped to and set up on-site. They are priced very competitively to ensure availability on nearly any budget, and will be stocked domestically in L-com's HyperLink distribution center in Boca Raton, FL, for same-day shipment.

For a high-res version of the image suitable for print publication, please click here.

For more information about this release, please contact:
Dave Fallon, Internet Marketing Strategist
978-682-6936 x1450, newsletters@L-com.com

L-com, a global designer and manufacturer of wired and wireless connectivity products, offers a wide range of solutions and unmatched customer service for the electronics and data communications industries. The company's product portfolio includes cable assemblies, connectors, adapters, computer networking components, and custom products, as well as the Hyperlink line of wireless products. Trusted for more than 30 years, L-com, Inc. is headquartered in North Andover, Mass., and is ISO 9001: 2008-certified. For more information, please visit: http://www.L-com.com/

###


Other press releases that may be of interest to you:
 
7/18/2019 L-com Introduces New Active Optical Cables for use in High-Speed Data Center Applications
7/17/2019 L-com Launches New 900 MHz Omni and Sector Antennas
7/16/2019 L-com Unveils Premium 8-Position, A-code, M12 Cable Assemblies for Sensor, Actuator and Fieldbus Applications
7/11/2019 L-com Releases New OM5 Fiber Cables for High-Speed Data Center Applications
6/27/2019 L-com Releases New Small Cell and Outdoor Power Protection Enclosures
6/26/2019 L-com Adds New Premium RJ45 to M12 Female Panel-Mount Cable Assemblies
6/13/2019 L-com Releases New Flat HDMI Cables with LSZH Jackets
5/23/2019 L-com Launches New Indoor and Outdoor-Rated Cat6a Lightning and Surge Protectors
5/14/2019 L-com Introduces New Cat7 LSZH Cable Assemblies for Shipboard, Aerospace and Defense Applications
5/9/2019 L-com Launches New M12 Field Termination Connectors and In-line Adapters to Address Industrial Networking Applications
5/7/2019 L-com Releases New Cat6a Outdoor-Rated, High-Flex Ethernet Cable Assemblies
4/25/2019 L-com Expands Outdoor Industrial Ethernet Cable Line with Additional Length Options Available with Same-Day Shipping
4/4/2019 L-com Releases New Patch Panels with N-Type Couplers and 0.630” D-Holes
4/2/2019 L-com Adds New Power Cords for Server, PC, Laptop, PDU Applications and More
3/21/2019 L-com now Stocks 12G-SDI, HD-BNC Connectors for use in Broadcast Video Applications
3/19/2019 L-com Launches New Line of Rugged Category 7 Cables with 10 Gig Rating for Outdoor and Industrial Applications
3/15/2019 L-com Launches Right-Angle USB 3.0 Cable Assemblies with Female Connectors
3/14/2019 L-com Introduces New Right-Angle Panel-Mount DisplayPort Cables
3/12/2019 L-com Unveils New DisplayPort to HDMI Cables with LSZH Jackets
3/5/2019 L-com Debuts New Line of Dual-Rated Slim-Line Ethernet Cables with Spline-Free Design and UL CM Burn Rating
  Page:  1 of 28
    
 
Free Newsletter
L-com Global Connectivity           50 High Street           North Andover, MA 01845
www.L-com.com E-mail: sales@L-com.com 1-800-341-5266 www.Facebook.com/LcomGlobal


© Infinite Electronics International, Inc.