L-com Global Connectivity
  
Cart is Empty
  
USA & Canada (800) 341-5266     International +1 (978) 682-6936
L-com Debuts Right Angle USB Mini B5 and Micro B Cables
(Thursday, July 05, 2012)
 

L-com Debuts Right Angle USB Mini B5 and Micro B Cables

Right Angle USB 2.0 Mini B5 Cable from L-comNORTH ANDOVER, MA - 07/05/12 - L-com, Inc., a designer and manufacturer of wired and wireless connectivity products, has released two new lines of right angle USB cables, with mini B5 male or micro B connector options. The move comes as L-com continues to expand its extensive right angle product offering, with popular solutions like Ethernet, DVI, HDMI, D-Subminiature, and fiber optic right angle cable assemblies.

Right angle USB cables and adapters are not new to L-com. Last November, the company released right angle mini B5 adapters to support the demand, and plans to release right angle micro B adapters in July. The company first announced it would carry two right angle products for USB in May, 2009, and in the ensuing 36 months its offering has expanded to more than 100 unique items.

"Over and over what we are hearing is engineers and technicians want right angle USB for their designs and projects," said Steve Smith, Product Manager. "Designing right angle cables that meet the USB 2.0 standard took some effort, but I'm very proud of the results. We now have one of the most extensive right angle USB offerings available."

Along with the release of the new cable assemblies, L-com posted helpful "Angled USB Cables" tips to help customers purchase the correct part. The company has also announced that it will offer custom length cables with the right angle USB mini B5 or micro B connectors upon request.

To download a high resolution version of the image suitable for print publication, click this link:
http://www.L-com.com/lcom_emails/2012/070512/caa_90rmb5_.jpg

For more information about this release, please contact:
Dave Fallon, Internet Marketing Strategist
978-682-6936 x1450, newsletters@L-com.com

L-com, a global designer and manufacturer of wired and wireless connectivity products, offers a wide range of solutions and unmatched customer service for the electronics and data communications industries. The company's product portfolio includes cable assemblies, connectors, adapters, computer networking components, and custom products, as well as the Hyperlink line of wireless products. Trusted for more than 30 years, L-com, Inc. is headquartered in North Andover, Mass., and is ISO 9001: 2008-certified. For more information, please visit: http://www.L-com.com/

###


Other press releases that may be of interest to you:
 
8/13/2019 L-com Releases New Cat6 and Cat6a Plenum +105°C, 28AWG, Shielded, Slim Ethernet Patch Cords
8/8/2019 L-com Debuts New UL Listed NEMA-Rated Equipment Enclosures
8/6/2019 New Latching USB 3.0 Cable Assemblies Address Heavy Vibration Applications
8/1/2019 L-com Launches New Triple-Speed Ethernet Switches to Address Industrial Network Applications
7/30/2019 L-com Releases Cat6a Continuous Flex, ZHFR-PUR, Double Shielded Cable Assemblies
7/26/2019 L-com Debuts New Wall-Mount Cabinets and Racks to Address LAN Connectivity Applications
7/25/2019 L-com Introduces new Polycarbonate NEMA-Rated Equipment Enclosures for Wired and Wireless Applications
7/23/2019 L-com Releases New 1U and 2U Cat5e, Cat6 and Cat6a Patch Panels
7/18/2019 L-com Introduces New Active Optical Cables for use in High-Speed Data Center Applications
7/17/2019 L-com Launches New 900 MHz Omni and Sector Antennas
7/16/2019 L-com Unveils Premium 8-Position, A-code, M12 Cable Assemblies for Sensor, Actuator and Fieldbus Applications
7/11/2019 L-com Releases New OM5 Fiber Cables for High-Speed Data Center Applications
6/27/2019 L-com Releases New Small Cell and Outdoor Power Protection Enclosures
6/26/2019 L-com Adds New Premium RJ45 to M12 Female Panel-Mount Cable Assemblies
6/13/2019 L-com Releases New Flat HDMI Cables with LSZH Jackets
5/23/2019 L-com Launches New Indoor and Outdoor-Rated Cat6a Lightning and Surge Protectors
5/14/2019 L-com Introduces New Cat7 LSZH Cable Assemblies for Shipboard, Aerospace and Defense Applications
5/9/2019 L-com Launches New M12 Field Termination Connectors and In-line Adapters to Address Industrial Networking Applications
5/7/2019 L-com Releases New Cat6a Outdoor-Rated, High-Flex Ethernet Cable Assemblies
4/25/2019 L-com Expands Outdoor Industrial Ethernet Cable Line with Additional Length Options Available with Same-Day Shipping
  Page:  1 of 28
    
 
Free Newsletter
L-com Global Connectivity           50 High Street           North Andover, MA 01845
www.L-com.com E-mail: sales@L-com.com 1-800-341-5266 www.Facebook.com/LcomGlobal


© Infinite Electronics International, Inc.