L-com Global Connectivity
  
Cart is Empty
  
USA & Canada (800) 341-5266     International +1 (978) 682-6936
L-com Re-introduces 2.4 GHz Grid Antenna Line
(Monday, June 18, 2012)
 

L-com Re-introduces 2.4 GHz Grid Antenna Line

2.4 GHz 15 dBi Die-cast Grid AntennasNORTH ANDOVER, MA - 06/18/12 - L-com, Inc., a designer and manufacturer of wired and wireless connectivity products, has re-introduced the HyperLink Wireless brand of 2.4 GHz grid antennas designed to reduce the product cost without sacrificing quality or performance. The "EG" line of antennas sells for as little as $35.00 each with discounts for bulk purchases. These products replace the popular standard grid antennas that HyperLink had first offered years ago, and they increase L-com's competitiveness in the Wi-Fi antenna market.

Grid antennas are used in the 2.4GHz ISM band to transmit directional signals, usually for the 802.11b/g/n standards of wireless Ethernet technology. As this application has become more and more common, the competitive landscape for these types of antennas has grown. The HyperLink Wireless brand of antennas has had a reputation for their high quality for decades. Now, with new manufacturing techniques, L-com has produced an antenna line that costs up to 22% less, while still meeting their high quality standards.

Here is a table showing the new product lines:

Old Base
Part Number
Gain (dBi) New Base
Part Number
Gain (dBi) List Price Savings
HG2415G 15 HG2415EG 15 $35.00 5.38%
HG2419G 19 HG2420EG 20 $40.00 16.65%
HG2424G 24 HG2424EG 24 $45.00 22.40%

"The HyperLink brand has a very high-quality reputation to maintain," said Patrick Pesa, Director of Product Development. "We worked long and hard to find a solution that would save our customers money but not sacrifice quality or performance."

The new antennas are assembled and stocked in the USA for same-day shipment. Along with the various connector options available, many models can be purchased in packages of five to further reduce the per-piece cost.

To download the image as a high-resolution .jpg suitable for print publication, click here:
http://www.L-com.com/lcom_emails/2012/061812/hg2415g_3.jpg

For more information about this release, please contact:
Dave Fallon, Internet Marketing Strategist
978-682-6936 x1450, newsletters@L-com.com

L-com, a global designer and manufacturer of wired and wireless connectivity products, offers a wide range of solutions and unmatched customer service for the electronics and data communications industries. The company's product portfolio includes cable assemblies, connectors, adapters, computer networking components, and custom products, as well as the Hyperlink line of wireless products. Trusted for more than 30 years, L-com, Inc. is headquartered in North Andover, Mass., and is ISO 9001: 2008-certified. For more information, please visit: http://www.L-com.com/

###


Other press releases that may be of interest to you:
 
7/18/2019 L-com Introduces New Active Optical Cables for use in High-Speed Data Center Applications
7/17/2019 L-com Launches New 900 MHz Omni and Sector Antennas
7/16/2019 L-com Unveils Premium 8-Position, A-code, M12 Cable Assemblies for Sensor, Actuator and Fieldbus Applications
7/11/2019 L-com Releases New OM5 Fiber Cables for High-Speed Data Center Applications
6/27/2019 L-com Releases New Small Cell and Outdoor Power Protection Enclosures
6/26/2019 L-com Adds New Premium RJ45 to M12 Female Panel-Mount Cable Assemblies
6/13/2019 L-com Releases New Flat HDMI Cables with LSZH Jackets
5/23/2019 L-com Launches New Indoor and Outdoor-Rated Cat6a Lightning and Surge Protectors
5/14/2019 L-com Introduces New Cat7 LSZH Cable Assemblies for Shipboard, Aerospace and Defense Applications
5/9/2019 L-com Launches New M12 Field Termination Connectors and In-line Adapters to Address Industrial Networking Applications
5/7/2019 L-com Releases New Cat6a Outdoor-Rated, High-Flex Ethernet Cable Assemblies
4/25/2019 L-com Expands Outdoor Industrial Ethernet Cable Line with Additional Length Options Available with Same-Day Shipping
4/4/2019 L-com Releases New Patch Panels with N-Type Couplers and 0.630” D-Holes
4/2/2019 L-com Adds New Power Cords for Server, PC, Laptop, PDU Applications and More
3/21/2019 L-com now Stocks 12G-SDI, HD-BNC Connectors for use in Broadcast Video Applications
3/19/2019 L-com Launches New Line of Rugged Category 7 Cables with 10 Gig Rating for Outdoor and Industrial Applications
3/15/2019 L-com Launches Right-Angle USB 3.0 Cable Assemblies with Female Connectors
3/14/2019 L-com Introduces New Right-Angle Panel-Mount DisplayPort Cables
3/12/2019 L-com Unveils New DisplayPort to HDMI Cables with LSZH Jackets
3/5/2019 L-com Debuts New Line of Dual-Rated Slim-Line Ethernet Cables with Spline-Free Design and UL CM Burn Rating
  Page:  1 of 28
    
 
Free Newsletter
L-com Global Connectivity           50 High Street           North Andover, MA 01845
www.L-com.com E-mail: sales@L-com.com 1-800-341-5266 www.Facebook.com/LcomGlobal


© Infinite Electronics International, Inc.