L-com Global Connectivity
  
Cart is Empty
  
USA & Canada (800) 341-5266     International +1 (978) 682-6936
New 3.5 GHz 802.16e WiMAX Compatible Amplifiers Add 1 Watt Power to Wireless Transmissions
(Thursday, June 14, 2012)
 

New 3.5 GHz 802.16e WiMAX Compatible Amplifiers Add 1 Watt Power to Wireless Transmissions

1 Watt 3.5 GHz 802.16e WiMAX Compatible Outdoor AmplifierNORTH ANDOVER, MA - 6/14/12 - L-com, Inc., a designer and manufacturer of wired and wireless connectivity products, has released two new wireless RF amplifiers designed to add 1 Watt of power to 3.5 GHz transmissions, typically used in 802.16e WiMAX wireless applications. The new amplifiers, which are available for export, military, licensed amateur radio and OEM component sales only, can add up to 30 dBm output power to 3.5 GHz antennas. The HA3501I-1000 is for indoor applications only, while the HA3501-1000 is designed for outdoor applications and comes with a DC injector, 12 VDC power supply, and mast mount kit.

Worldwide Interoperability for Microwave Access (WiMAX) is an IP based wireless broadband access technology that provides performance similar to 802.11 and Wi-Fi networks but has the coverage and quality of service (QOS) of cellular networks. Standardized by IEEE 802.16, it is intended for wireless "metropolitan area networks". The new amplifiers suit these applications where a greater range or signal strength is desired.

"HyperLink's brand amplifiers have been a mainstay in our industry for decades," said Patrick Pesa, Director of Product Development. "Now under the L-com brand, we are extending our already broad range of products to support cutting edge wireless applications."

Due to FCC regulations, the new amplifiers are not offered for general sale within the USA (see FCC Part 15 and Part 97 Notice in L-com's Terms & Conditions). For FCC supported applications, the new amplifiers will be stocked in L-com's Florida distribution center for same-day shipments.

To download a high-resolution version of the image suitable for print publication, please click this link:
http://www.L-com.com/lcom_emails/2012/061412/HA5801-1000.jpg

For more information about this release, please contact:
Dave Fallon, Internet Marketing Strategist
978-682-6936 x1450, newsletters@L-com.com

L-com, a global designer and manufacturer of wired and wireless connectivity products, offers a wide range of solutions and unmatched customer service for the electronics and data communications industries. The company's product portfolio includes cable assemblies, connectors, adapters, computer networking components, and custom products, as well as the Hyperlink line of wireless products. Trusted for more than 30 years, L-com, Inc. is headquartered in North Andover, Mass., and is ISO 9001: 2008-certified. For more information, please visit: http://www.L-com.com/

###


Other press releases that may be of interest to you:
 
7/18/2019 L-com Introduces New Active Optical Cables for use in High-Speed Data Center Applications
7/17/2019 L-com Launches New 900 MHz Omni and Sector Antennas
7/16/2019 L-com Unveils Premium 8-Position, A-code, M12 Cable Assemblies for Sensor, Actuator and Fieldbus Applications
7/11/2019 L-com Releases New OM5 Fiber Cables for High-Speed Data Center Applications
6/27/2019 L-com Releases New Small Cell and Outdoor Power Protection Enclosures
6/26/2019 L-com Adds New Premium RJ45 to M12 Female Panel-Mount Cable Assemblies
6/13/2019 L-com Releases New Flat HDMI Cables with LSZH Jackets
5/23/2019 L-com Launches New Indoor and Outdoor-Rated Cat6a Lightning and Surge Protectors
5/14/2019 L-com Introduces New Cat7 LSZH Cable Assemblies for Shipboard, Aerospace and Defense Applications
5/9/2019 L-com Launches New M12 Field Termination Connectors and In-line Adapters to Address Industrial Networking Applications
5/7/2019 L-com Releases New Cat6a Outdoor-Rated, High-Flex Ethernet Cable Assemblies
4/25/2019 L-com Expands Outdoor Industrial Ethernet Cable Line with Additional Length Options Available with Same-Day Shipping
4/4/2019 L-com Releases New Patch Panels with N-Type Couplers and 0.630” D-Holes
4/2/2019 L-com Adds New Power Cords for Server, PC, Laptop, PDU Applications and More
3/21/2019 L-com now Stocks 12G-SDI, HD-BNC Connectors for use in Broadcast Video Applications
3/19/2019 L-com Launches New Line of Rugged Category 7 Cables with 10 Gig Rating for Outdoor and Industrial Applications
3/15/2019 L-com Launches Right-Angle USB 3.0 Cable Assemblies with Female Connectors
3/14/2019 L-com Introduces New Right-Angle Panel-Mount DisplayPort Cables
3/12/2019 L-com Unveils New DisplayPort to HDMI Cables with LSZH Jackets
3/5/2019 L-com Debuts New Line of Dual-Rated Slim-Line Ethernet Cables with Spline-Free Design and UL CM Burn Rating
  Page:  1 of 28
    
 
Free Newsletter
L-com Global Connectivity           50 High Street           North Andover, MA 01845
www.L-com.com E-mail: sales@L-com.com 1-800-341-5266 www.Facebook.com/LcomGlobal


© Infinite Electronics International, Inc.