L-com Global Connectivity
  
Cart is Empty
  
USA & Canada (800) 341-5266     International +1 (978) 682-6936

To our valued customers: Our offices will be closed Monday, May 27th, in observance of the Memorial Day Holiday.

L-com Supports Emerging Standard with Middle Atlantic Products' New HRF Series Half Rack Systems
(Monday, April 30, 2012)
 

L-com Supports Emerging Standard with Middle Atlantic Products' New HRF Series Half Rack Systems

HRF Series Half-Rack Systems Available at L-com.comNORTH ANDOVER, MA - 4/30/12 - L-com, Inc., a designer and manufacturer of wired and wireless connectivity products, announced today that it will begin carrying half rack products from Middle Atlantic Products. The new items were released by Middle Atlantic in early February serving to help develop an ECIA standard for the half-width rack format. L-com's commitment to carry these products represents strong support for the emerging standard.

Unlike the standard 19" racks and panels, the HRF series have an overall standardized width of 10 5/8". This is ideal for using racks to organize cables and equipment in confined areas. The standard set forth by the ECIA would allow HRF series products to be used with equipment from a variety of manufacturers, opening the door for manufacturers like L-com to design patch panels, storage drawers and shelves, and cable management accessories to fit the smaller width.

"Tight spaces can ruin any cable system or network, causing strains on cables, ventilation problems, and an extremely difficult working condition," said Patrick Pesa, L-com's Director of Product Management. "Unfortunately, such situations are becoming more and more common. L-com's commitment to alleviate these problems is without peer, and includes right angle cables and adapters, precisely cut length cables, and now a new compact standard of rack enclosure."

Currently, L-com is carrying a variety of rack frames, universal multi-shelves, and thermal management blank and vented panels. L-com has formally distributed Middle Atlantic Products items for over seven years.

To download a high-resolution version of the image suitable for print publication, please click here.

For more information about this release, please contact:
Dave Fallon, Internet Marketing Strategist
978-682-6936 x1450, newsletters@L-com.com

L-com, a global designer and manufacturer of wired and wireless connectivity products, offers a wide range of solutions and unmatched customer service for the electronics and data communications industries. The company's product portfolio includes cable assemblies, connectors, adapters, computer networking components, and custom products, as well as the Hyperlink line of wireless products. Trusted for more than 25 years, L-com, Inc. is headquartered in North Andover, Mass., and is ISO 9001: 2008-certified. For more information, please visit: http://www.L-com.com/

###

 


Other press releases that may be of interest to you:
 
5/14/2019 L-com Introduces New Cat7 LSZH Cable Assemblies for Shipboard, Aerospace and Defense Applications
5/9/2019 L-com Launches New M12 Field Termination Connectors and In-line Adapters to Address Industrial Networking Applications
5/7/2019 L-com Releases New Cat6a Outdoor-Rated, High-Flex Ethernet Cable Assemblies
4/25/2019 L-com Expands Outdoor Industrial Ethernet Cable Line with Additional Length Options Available with Same-Day Shipping
4/4/2019 L-com Releases New Patch Panels with N-Type Couplers and 0.630” D-Holes
4/2/2019 L-com Adds New Power Cords for Server, PC, Laptop, PDU Applications and More
3/21/2019 L-com now Stocks 12G-SDI, HD-BNC Connectors for use in Broadcast Video Applications
3/19/2019 L-com Launches New Line of Rugged Category 7 Cables with 10 Gig Rating for Outdoor and Industrial Applications
3/15/2019 L-com Launches Right-Angle USB 3.0 Cable Assemblies with Female Connectors
3/14/2019 L-com Introduces New Right-Angle Panel-Mount DisplayPort Cables
3/12/2019 L-com Unveils New DisplayPort to HDMI Cables with LSZH Jackets
3/5/2019 L-com Debuts New Line of Dual-Rated Slim-Line Ethernet Cables with Spline-Free Design and UL CM Burn Rating
2/28/2019 L-com Releases New USB 3.1 Gen 2 Type-C Cables with Low-Smoke Zero-Halogen and PVC Jackets
2/21/2019 L-com Debuts New Cat5e, Cat6 and Cat6a Universal Sub-panels with PoE+ Compliant Jacks
2/14/2019 L-com Introduces New RJ45 Termination Block for Field Termination and Repair Applications
2/12/2019 L-com Debuts New Black and White Flat Cat5e and Cat6 Ethernet Cables
2/7/2019 L-com Releases New Cat5e Double-Shielded Outdoor High-Flex PoE Industrial Ethernet Cables
2/5/2019 L-com Debuts New Fiber LC Couplers with Internal Dustproof Shutters
1/31/2019 L-com Releases Aerial and Outdoor Bulk Cable for use in Demanding OSP Networks
1/29/2019 L-com Now Stocks Moldable M12 Connecters for Rugged Applications
  Page:  1 of 27
    
 
Free Newsletter
L-com Global Connectivity           50 High Street           North Andover, MA 01845
www.L-com.com E-mail: sales@L-com.com 1-800-341-5266 www.Facebook.com/LcomGlobal


© Infinite Electronics International, Inc.