L-com Global Connectivity
  
Cart is Empty
  
USA & Canada (800) 341-5266     International +1 (978) 682-6936
New Dual Line Telephone/DSL/T1 Lightning Protector Added to Extensive Offering
(Thursday, April 12, 2012)
 

New Dual Line Telephone/DSL/T1 Lightning Protector Added to Extensive Offering

L-com's Dual Line Telephone/DSL/T1 Lightning Surge ProtectorNORTH ANDOVER, MA - 04/12/12 - L-com, Inc., a designer and manufacturer of wired  and wireless connectivity products, has added a new Telephone/DSL/T1 lightning protector that provides high-power protection to two lines with a single protector. The new unit is the twentieth item added to an extensive product line including Telephone/DSL/T1 lightning protectors with RJ11 jacks, punch-down terminals, and screw terminals; for indoor, outdoor, and industrial applications; and in forms for rack-mounting, wall-mounting, and in-wall electrical box mounting. 

The new item, HGLN-D2T, complements the HGLN-DT model by protecting two lines instead of one at the same price. It is made for indoor installations, providing high-power protection.  It comprises a single pair of RJ11 jacks (one for input, and one for protected output) in an industrial grade cast aluminum body with integral mounting feet that can be shelf-mounted or wall-mounted. The HGLN-D2T uses three terminal differential gas discharge tubes to provide protection for two separate lines with a clamping voltage of +/- 230 volts.

"Among all the signal cables in commercial buildings, the telephone, DSL, and T1 lines are usually the most extensive and therefore most vulnerable to transient voltages," said Patrick Pesa, Director of Product Management. "We've therefore spent a lot of time designing and producing lightning and surge protectors for those lines, giving us one of the broadest product offerings in the industry for this application."

L-com will manufacture and stock the new lightning protector in its Florida, USA production and warehouse facilities. 

Please click here to download a high-resolution version of the image suitable for print publication.

For more information about this release, please contact:
Dave Fallon, Internet Marketing Strategist
978-682-6936 x1450, newsletters@L-com.com

L-com, a global designer and manufacturer of wired and wireless connectivity products, offers a wide range of solutions and unmatched customer service for the electronics and data communications industries. The company's product portfolio includes cable assemblies, connectors, adapters, computer networking components, and custom products, as well as the Hyperlink line of wireless products. Trusted for more than 25 years, L-com, Inc. is headquartered in North Andover, Mass., and is ISO 9001: 2008-certified. For more information, please visit: http://www.L-com.com/

###


Other press releases that may be of interest to you:
 
7/18/2019 L-com Introduces New Active Optical Cables for use in High-Speed Data Center Applications
7/17/2019 L-com Launches New 900 MHz Omni and Sector Antennas
7/16/2019 L-com Unveils Premium 8-Position, A-code, M12 Cable Assemblies for Sensor, Actuator and Fieldbus Applications
7/11/2019 L-com Releases New OM5 Fiber Cables for High-Speed Data Center Applications
6/27/2019 L-com Releases New Small Cell and Outdoor Power Protection Enclosures
6/26/2019 L-com Adds New Premium RJ45 to M12 Female Panel-Mount Cable Assemblies
6/13/2019 L-com Releases New Flat HDMI Cables with LSZH Jackets
5/23/2019 L-com Launches New Indoor and Outdoor-Rated Cat6a Lightning and Surge Protectors
5/14/2019 L-com Introduces New Cat7 LSZH Cable Assemblies for Shipboard, Aerospace and Defense Applications
5/9/2019 L-com Launches New M12 Field Termination Connectors and In-line Adapters to Address Industrial Networking Applications
5/7/2019 L-com Releases New Cat6a Outdoor-Rated, High-Flex Ethernet Cable Assemblies
4/25/2019 L-com Expands Outdoor Industrial Ethernet Cable Line with Additional Length Options Available with Same-Day Shipping
4/4/2019 L-com Releases New Patch Panels with N-Type Couplers and 0.630” D-Holes
4/2/2019 L-com Adds New Power Cords for Server, PC, Laptop, PDU Applications and More
3/21/2019 L-com now Stocks 12G-SDI, HD-BNC Connectors for use in Broadcast Video Applications
3/19/2019 L-com Launches New Line of Rugged Category 7 Cables with 10 Gig Rating for Outdoor and Industrial Applications
3/15/2019 L-com Launches Right-Angle USB 3.0 Cable Assemblies with Female Connectors
3/14/2019 L-com Introduces New Right-Angle Panel-Mount DisplayPort Cables
3/12/2019 L-com Unveils New DisplayPort to HDMI Cables with LSZH Jackets
3/5/2019 L-com Debuts New Line of Dual-Rated Slim-Line Ethernet Cables with Spline-Free Design and UL CM Burn Rating
  Page:  1 of 28
    
 
Free Newsletter
L-com Global Connectivity           50 High Street           North Andover, MA 01845
www.L-com.com E-mail: sales@L-com.com 1-800-341-5266 www.Facebook.com/LcomGlobal


© Infinite Electronics International, Inc.