New Dual Line Telephone/DSL/T1 Lightning Protector Added to Extensive Offering NORTH ANDOVER, MA - 04/12/12 - L-com, Inc., a designer and manufacturer of wired and wireless connectivity products, has added a new Telephone/DSL/T1 lightning protector that provides high-power protection to two lines with a single protector. The new unit is the twentieth item added to an extensive product line including Telephone/DSL/T1 lightning protectors with RJ11 jacks, punch-down terminals, and screw terminals; for indoor, outdoor, and industrial applications; and in forms for rack-mounting, wall-mounting, and in-wall electrical box mounting. The new item, HGLN-D2T, complements the HGLN-DT model by protecting two lines instead of one at the same price. It is made for indoor installations, providing high-power protection. It comprises a single pair of RJ11 jacks (one for input, and one for protected output) in an industrial grade cast aluminum body with integral mounting feet that can be shelf-mounted or wall-mounted. The HGLN-D2T uses three terminal differential gas discharge tubes to provide protection for two separate lines with a clamping voltage of +/- 230 volts. "Among all the signal cables in commercial buildings, the telephone, DSL, and T1 lines are usually the most extensive and therefore most vulnerable to transient voltages," said Patrick Pesa, Director of Product Management. "We've therefore spent a lot of time designing and producing lightning and surge protectors for those lines, giving us one of the broadest product offerings in the industry for this application." L-com will manufacture and stock the new lightning protector in its Florida, USA production and warehouse facilities. Please click here to download a high-resolution version of the image suitable for print publication. For more information about this release, please contact: Dave Fallon, Internet Marketing Strategist 978-682-6936 x1450, newsletters@L-com.com L-com, a global designer and manufacturer of wired and wireless connectivity products, offers a wide range of solutions and unmatched customer service for the electronics and data communications industries. The company's product portfolio includes cable assemblies, connectors, adapters, computer networking components, and custom products, as well as the Hyperlink line of wireless products. Trusted for more than 25 years, L-com, Inc. is headquartered in North Andover, Mass., and is ISO 9001: 2008-certified. For more information, please visit: http://www.L-com.com/ ### |