L-com Global Connectivity
  
Cart is Empty
  
USA & Canada (800) 341-5266     International +1 (978) 682-6936

To our valued customers: Our offices will be closed Monday, May 27th, in observance of the Memorial Day Holiday.

New Four-Port Wall/Shelf-Mount and Rack-Mount Gas Tube Lightning Protectors Protect Cat 6 Lines
(Wednesday, March 28, 2012)
 

New Four-Port Wall/Shelf-Mount and Rack-Mount Gas Tube Lightning Protectors Protect Cat 6 Lines

Wall-Mount and Shelf-Mount Four-Port Lightning/Surge Protector for Category 6 Lines
Rack-Mount Four-Port Lightning/Surge Protector for Category 6 Lines

NORTH ANDOVER, MA - 3/28/12 - L-com, Inc., a designer and manufacturer of wired and wireless connectivity products, has introduced two new gas tube lightning protectors designed to protect up to four Category 6 Ethernet cable lines. Designed to stop transient voltages or power spikes from damaging sensitive electronic equipment, these new wall/shelf-mount and rack-mount models offer even better protection than the diode versions that L-com has carried since 2009.

L-com's earlier models of four-port Cat 6 lightning protectors used ultra-low capacitance diodes to stop spikes of up to 65 Volts. The new models use gas discharge tubes to provide low line-to-line and line-to-ground capacitance, minimizing distortion of high-speed signals. They stop spikes up to 90 Volts and have L-com's highest power rating available. The new parts are also compatible with 802.3af/at PoE devices.

"We know that power surges cause massive expenses to businesses world-wide every year," said Patrick Pesa, Director of Product Management. "We're glad we're able to offer such high-power protection with nearly no impact at all in signal speed or quality. Now customers can easily protect high-speed Ethernet devices with the convenience of a wall or rack mount protector for up to four separate lines."

The new protectors are built in the USA and stocked in L-com's Florida distribution center for shipment on the same day as ordered. Detailed datasheets for the wall/shelf-mount and the rack-mount products are available for free download on the L-com.com web site. 

Please click here to download a high-resolution version of the first image suitable for print publication.

Please click here to download a high-resolution version of the second image suitable for print publication.

For more information about this release, please contact:
Dave Fallon, Internet Marketing Strategist
978-682-6936 x1450, newsletters@L-com.com

L-com, a global designer and manufacturer of wired and wireless connectivity products, offers a wide range of solutions and unmatched customer service for the electronics and data communications industries. The company’s product portfolio includes cable assemblies, connectors, adapters, computer networking components, and custom products, as well as the Hyperlink line of wireless products. Trusted for more than 25 years, L-com, Inc. is headquartered in North Andover, Mass., and is ISO 9001: 2008-certified. For more information, please visit: http://www.L-com.com/


Other press releases that may be of interest to you:
 
5/23/2019 L-com Launches New Indoor and Outdoor-Rated Cat6a Lightning and Surge Protectors Supporting 10/100/1000/10000 Applications
5/14/2019 L-com Introduces New Cat7 LSZH Cable Assemblies for Shipboard, Aerospace and Defense Applications
5/9/2019 L-com Launches New M12 Field Termination Connectors and In-line Adapters to Address Industrial Networking Applications
5/7/2019 L-com Releases New Cat6a Outdoor-Rated, High-Flex Ethernet Cable Assemblies
4/25/2019 L-com Expands Outdoor Industrial Ethernet Cable Line with Additional Length Options Available with Same-Day Shipping
4/4/2019 L-com Releases New Patch Panels with N-Type Couplers and 0.630” D-Holes
4/2/2019 L-com Adds New Power Cords for Server, PC, Laptop, PDU Applications and More
3/21/2019 L-com now Stocks 12G-SDI, HD-BNC Connectors for use in Broadcast Video Applications
3/19/2019 L-com Launches New Line of Rugged Category 7 Cables with 10 Gig Rating for Outdoor and Industrial Applications
3/15/2019 L-com Launches Right-Angle USB 3.0 Cable Assemblies with Female Connectors
3/14/2019 L-com Introduces New Right-Angle Panel-Mount DisplayPort Cables
3/12/2019 L-com Unveils New DisplayPort to HDMI Cables with LSZH Jackets
3/5/2019 L-com Debuts New Line of Dual-Rated Slim-Line Ethernet Cables with Spline-Free Design and UL CM Burn Rating
2/28/2019 L-com Releases New USB 3.1 Gen 2 Type-C Cables with Low-Smoke Zero-Halogen and PVC Jackets
2/21/2019 L-com Debuts New Cat5e, Cat6 and Cat6a Universal Sub-panels with PoE+ Compliant Jacks
2/14/2019 L-com Introduces New RJ45 Termination Block for Field Termination and Repair Applications
2/12/2019 L-com Debuts New Black and White Flat Cat5e and Cat6 Ethernet Cables
2/7/2019 L-com Releases New Cat5e Double-Shielded Outdoor High-Flex PoE Industrial Ethernet Cables
2/5/2019 L-com Debuts New Fiber LC Couplers with Internal Dustproof Shutters
1/31/2019 L-com Releases Aerial and Outdoor Bulk Cable for use in Demanding OSP Networks
  Page:  1 of 27
    
 
Free Newsletter
L-com Global Connectivity           50 High Street           North Andover, MA 01845
www.L-com.com E-mail: sales@L-com.com 1-800-341-5266 www.Facebook.com/LcomGlobal


© Infinite Electronics International, Inc.