L-com Global Connectivity
  
Cart is Empty
  
USA & Canada (800) 341-5266     International +1 (978) 682-6936


Organize your fiber network with racks and enclosures
(Tuesday, February 14, 2012)
 
L-com Global Connectivity
 
Fiber Network Architecture
  Quick Order Free Catalog Custom / OEM New Products Sale Items  

Mounting Fiber Optic Adapters to Organize and Neaten your Network Architecture

Wall mount rack frame with panels

Any wired network can quickly become a tangled mess, especially as that network grows over time.  For that reason, it is a good idea to future-proof your network by building in a network architecture that is neat, organized and scalable. Often, the first place to start with developing such an architecture is with the racks and enclosures in the networking closet or room.

What do we mean by architecture?

A network is composed of two parts: the hardware and the software, and the hardware is usually the hardest to keep controlled. The architecture of a network is the planned layout of the hardware such that operators can make changes, ideally by simply plugging a cable into a panel-mounted adapter that is clearly marked and easily accessible. 

L-com’s FSP Series for Superior Fiber Network Architecture

L-com FSP Fiber Sub PanelL-com offers many convenient products to iron down the fiber optic network architecture in no time. Start with the FSP series wall-mount enclosures, 19" rack-mount enclosures, DIN-rail mount enclosures or 19" rack panels.  Then, simply add as many FSP series sub-panels as you need.  We carry them with ST, SC, LC (keyed and un-keyed), MTRJ, and FC. They come in an array of colors to help color-code your network.  Or you can purchase blank and unpopulated FSP panels and put the fiber optic adapters on yourself. 

MPO Cassettes for breaking out a multi-fiber cable

Often, fiber optic cables are used as backbone wiring to a network. One convenient way to carry multiple signals on a single fiber cable is an MPO ribbon fiber cable.  But breaking out a ribbon fiber cable into separate ports can be a hassle.  L-com's MPO Cassettes make it easy!  They can break one or two 12-fiber MPO connectors into separate SC or LC ports. All of the fiber wiring is done internal to the cassette, meaning someone with very little training can quickly and easily install them. You can have your fiber network up and running in no time, and make it perfectly scalable for future growth.  These MPO Cassettes fit in both the wall mount and rack mount enclosures as well as the FSP 19" panels but they don't fit in the DIN-rail mount enclosures yet.

MPO Cassettes fit in FSP series rack panelsInside an MPO Cassette
The MPO Cassettes fit perfectly in the FSP series rack panels.The inside of the MPO Cassettes are pre-wired for easy set-up.
Connect with L-com
Follow L-com on Twitter
Follow L-com on Facebook
Follow L-com on YouTube
Follow L-com on Google+

Latest News
Get the latest press releases from L-com here!

Helpful Links
L-com Home Page
Authorized Distributors
Custom Cables
Product Wizards
Product Comparisons
Technical Resources
Newsletter Archive
Newsletter Feedback
Friendly & Knowledgeable Service · In Stock Availability & Same Day Shipping · 100% Satisfaction Guaranteed

Other newsletters that may be of interest to you:
 
6/13/2016 The Benefits of 24 AWG Cable
5/24/2016 Why our Premium D-Sub Cables are Superior
5/17/2016 An A to Z review of the 802.11 standards
4/12/2016 USB Type-C Cable Assemblies Provide Legacy USB Connectivity
3/1/2016 Passive Intermodulation (PIM) Explained
2/2/2016 The Industrial Internet of Things (IIoT)
12/15/2015 Cable Shielding - How it Works
12/1/2015 Embedded Antennas and the IoT
11/10/2015 Long Live RS-232!
9/22/2015 The Differences between Solid and Stranded Cable
9/15/2015 Coaxial Connector Termination: Which Technique is Right for You
8/11/2015 802.11ah Breathes New Life to the 900 MHz Frequency Band
7/14/2015 Cable Options For Every Application
7/7/2015 900 MHz - Your NLOS Friend
6/2/2015 802.11ax Offers Blazing Fast Wi-Fi Connectivity
5/12/2015 The NBASE-T Alliance - Fostering Multi-Gig Speeds over Cat5e/6 Cabling
4/7/2015 L-com and The Internet of Things (IoT)
3/3/2015 802.3bt the Promise for Higher Power PoE
1/6/2015 L-com's Family of Brands - A Solution for Every Application
12/9/2014 Cat6a Products for High-Speed Networking
  Page:  1 of 15
    
 
Free Newsletter
L-com Global Connectivity           50 High Street           North Andover, MA 01845
www.L-com.com E-mail: sales@L-com.com 1-800-341-5266 www.Facebook.com/LcomGlobal


© Infinite Electronics International, Inc.
an Infinite company