L-com Global Connectivity
  
Cart is Empty
  
USA & Canada (800) 341-5266     International +1 (978) 682-6936

L-com's New USB 2.0 IP67 Field Installable Connectors
(Tuesday, September 20, 2011)
 
 
L-com Global Connectivity
 
L-com's New USB 2.0 IP67 Field Installable Connectors
  Quick Order Free Catalog Custom / OEM New Products Sale Items  

View L-com's New IP67 Field Install USB ConnectorsUSB 2.0 Type A IP67 Field Installable Connector

L-com’s USB 2.0 Field-Installable Connectors
L-com’s new USB field installable IP67 connectors allow you to make your own cable assemblies (using bulk USB cable) that are weatherproof and waterproof. They mate with all of the other waterproof USB cables and connectors that L-com carries, and they also work with the waterproof caps.

What does IP67 mean?
IP stands for ingress protection.  It is a rating of how much resistance to ingress a cable, connector, or adapter has. The first number after the IP is for the part’s protection against solid objects like dust and sand.  The second number after the IP is for the part’s protection against liquids.  An IP67 cable or connector is totally resistant to dust and protected against temporary immersion in water between 15cm and 1m deep for up to 30 minutes. 

Click here for a full chart of IP ratings.

Profile of IP67 Field Install ConnectorHow do L-com’s IP67-rated USB products work?
Remember that the IP67 rating on products is only effective if the product is used correctly.  L-com’s IP67- rated USB products work by using a gasket and a nut to tighten the mating connectors together. The new field installable connectors work the same way, except they have a sealing nut that also tightens the connector to the bulk cable. Once the connector is installed correctly, you have a IP67 rated cable custom made to your needs. All of these connectors can be panel-mounted by cutting a hole in the panel (download the engineering drawing for recommended panel opening dimensions), inserting the connector, and tightening the nut and gasket.


Connect with L-com
Follow L-com on Twitter
Follow L-com on Facebook
Follow L-com on YouTube
 
 

Latest News
Get the latest press releases from L-com here!

Helpful Links
L-com Home Page
Authorized Distributors
Product Configurator
Product Wizards
Product Comparisons
Technical Resources
Newsletter Archive
Newsletter Feedback
Friendly & Knowledgeable Service · In Stock Availability & Same Day Shipping · 100% Satisfaction Guaranteed

Other newsletters that may be of interest to you:
 
6/13/2016 The Benefits of 24 AWG Cable
5/24/2016 Why our Premium D-Sub Cables are Superior
5/17/2016 An A to Z review of the 802.11 standards
4/12/2016 USB Type-C Cable Assemblies Provide Legacy USB Connectivity
3/1/2016 Passive Intermodulation (PIM) Explained
2/2/2016 The Industrial Internet of Things (IIoT)
12/15/2015 Cable Shielding - How it Works
12/1/2015 Embedded Antennas and the IoT
11/10/2015 Long Live RS-232!
9/22/2015 The Differences between Solid and Stranded Cable
9/15/2015 Coaxial Connector Termination: Which Technique is Right for You
8/11/2015 802.11ah Breathes New Life to the 900 MHz Frequency Band
7/14/2015 Cable Options For Every Application
7/7/2015 900 MHz - Your NLOS Friend
6/2/2015 802.11ax Offers Blazing Fast Wi-Fi Connectivity
5/12/2015 The NBASE-T Alliance - Fostering Multi-Gig Speeds over Cat5e/6 Cabling
4/7/2015 L-com and The Internet of Things (IoT)
3/3/2015 802.3bt the Promise for Higher Power PoE
1/6/2015 L-com's Family of Brands - A Solution for Every Application
12/9/2014 Cat6a Products for High-Speed Networking
  Page:  1 of 15
    
 
Free Newsletter
L-com Global Connectivity           50 High Street           North Andover, MA 01845
www.L-com.com E-mail: sales@L-com.com 1-800-341-5266 www.Facebook.com/LcomGlobal


© Infinite Electronics International, Inc.
an Infinite company