L-com's 2.4 GHz FCC Certified WiFi Amplifier Kits
In the United States, Part 15 of the FCC rules and regulations specifies that RF power amplifiers can only be used in a system which has obtained authorization. Such systems are granted an FCC Identifier, also known as an FCC ID number. This restricts the marketing and sales of amplifiers since they can only be used with the system configuration with which it was approved and not as a separate product. A typical system may include a WiFi Radio, Antenna and Amplifier. Due to these regulations L-com is pleased to offer its 2.4 GHz FCC Certified Amplifier Kits which are available to all our US customers. These ready-to-go kits come complete with an 802.11g Wireless Ethernet Adapter, Rubber Duck Antenna and HyperLink brand 802.11g Amplifier. Indoor and outdoor versions from 100mW to 1 Watt are available.
Try L-com’s Amplifier Wizard to find Amplifiers fast!
High power 2.4GHz Amplifiers up to 25 Watts!
Power Over Ethernet amplifiers for the unique requirements of PoE
Note: Some amplifier products are available only for export, military, licensed amateur radio and OEM component sales and are not offered for general sale within the USA. See our web site for more information on specific amplifier models.
L-com Global Connectivity 45 Beechwood Drive North Andover, MA 01845www.L-com.com E-mail: sales@L-com.com Phone: 1-800-341-5266 Fax: 1-978-689-9484