Cart is Empty
Home   Request Catalog   Custom Cables   Product Wizards   Technical Resources   Contact Us

To our valued customers: The L-com offices will be closed Monday, May 27th, in observance of the Memorial Day holiday.

D-Subs Continue to Lock Down Dependability - Vol. 9 No. 63
(Tuesday, December 22, 2009)
 
 
L-com Global Connectivity
USB: The Future and the Past
 Quick OrderRequest/Download a catalogCustom/OEM ProductsNew ProductsOverstock and Sale Items 
Volume 9, Number 63

D-Subs Continue to Lock Down Dependability

Like the 40-ish professional athlete, D-Sub connector technology is no longer considered fast or sleek, but it is still going strong for one reason–it gets the job done.

BY STEVE SMITH, L-com


The D-Sub connector interface has survived being replaced by newer, faster, more compact interfaces. USB, among others, has replaced D-Sub serial and parallel ports on computers and printers. And DVI, HDMI, and the new DisplayPort interface have started to compete with SVGA (HD15 D-Sub) as the primary video interface on computer monitors as well. Nevertheless, D-Sub survival is due to several product features:

  • Engineers prefer the lock-down mating hardware between screw and standoff to the non-secure retention of USB, Firewire, HDMI, etc. Simply put, D-Sub hardware can be permanently locked down and will not come loose due to vibration or jostling.

  • Standard D-Sub connectors range from 9-position to 50-position, and high-density D-Sub connectors allow for up to 78 positions, giving designers flexibility depending on how many signals are required in their application.

  • Costs for connectors and cable assemblies are reasonably low.

  • Connectors and cable assemblies are available with many options. Printed circuit board (PCB) connectors are available as through-hole or surface-mount, can be stacked, and are also available filtered for high electromagnetic interference/radio frequency interference (EMI/RFI) environments. Cable connectors have multiple options for termination: solder, crimp/poke, insulation displacement, wire wrap and mass termination. Also available are combination connectors that reduce the number of signal contacts to accommodate coaxial, high current or high voltage contacts.

FIGURE 1. D-Sub connectors remain popular in part because they can be permanently locked down and will not come loose via vibration or jostling.

D-Sub Cables Not MatedD-Sub Cables Mated

Although they are called D-Subminiature, by today’s standards, these connectors are anything but miniature. Most designers look to reduce the size of their products, so valuable real estate is taken up quickly with D-Sub connectors.

Standard vs. high-density D-Sub Configurations

FIGURE 2.
Contacts are arranged in parallel rows varying from 2 to 4 rows depending on connector size.

In addition, because D-Sub connectors are connected to an unlimited variety of cable, there is no defined speed that the user can rely on without calculating and/or testing individual scenarios. Also, with the exception of some custom cable assemblies using larger AWG conductors, D-Sub connectors are considered signal–not power–connectors. Therefore, they do not readily and economically combine transmission of power and signal as do USB and Firewire.

D-Subminiature connectors were developed in the 1950s, and are distinguishable by their “D” shape, which ensures correct orientation. When mated, the female connector fits snugly inside the male connector. Because D-Subs are metal, a continuous, 360° shield can be created throughout the entire cable assembly and connector system.
Contacts are arranged in parallel rows varying from 2 to 4 rows depending on connector size. There are five basic shell sizes–standard contact arrangements range from 9 to 50 positions, while high density versions range from 15 to 78 positions.


FIGURE 3. In one D-Sub application, L-com helped a company design daisy-chain assemblies containing several smaller cables, all wired into larger 37- or 62-pin D-Sub connectors.
Somat D-Sub 37 position cable assembly
Somat D-Sub engineering drawing

Industry-standard commercial contacts are stamped metal while military-rated contacts are screw machined. Contacts are typically gold-plated–anywhere from 3 microinch gold flash to 30 microinch, depending on how many mating cycles they are expected to withstand.

Current Applications


Jim Smith, production engineer at HBM Somat (www.somat.com), a provider of rugged, portable data acquisition systems, states D-Sub connectivity is used throughout the company’s product lines because of its “reliability and convenience.”

Thirty-two signals are required to wire Somat’s thermocouple PCB to a cold junction compensation box. Somat designed in a standard, off-the-shelf 37-position D-Sub cable assembly to make the connections. For more complicated interconnet challenges, Somat designed a few daisy chain assemblies containing several smaller cables, all wired into larger DB37 and HD62 connectors (Figure 3). These cables make assembly easy, allow for multiple interfaces to be used, and take advantage of D-Sub’s high contact count and secure connection between cable assembly and PCB.

D-Sub Molded BackshellD-Sub - Bad Cable Example

FIGURE 4.
An L-com solution (L) for one company helped eliminate the problem of backshells that can’t provide adequate strain relief due to the non-uniform shape of the cable bundle, and individual cables occasionally pulling out of the backshell strain relief (R).

Another benefit of utilizing D-Sub connectors in these cables is the ability to mold the backshell, resulting in an exceptionally durable product. Initially, Somat had the cables manufactured with assembled/mechanical backshells. But because these assembled backshells can’t provide adequate strain relief due to the non-uniform shape of the cable bundle, individual cables occasionally pulled out of the backshell strain relief.
L-com proposed a molded backshell solution, which has eliminated this problem and provided a more professional appearance (Figure 4).

Tom Baker, electrical design engineer at Bally Technologies (www.ballytech.com), a manufacturer of casino games and slot machines, also uses D-Sub technology in a variety of applications. According to Baker, Bally uses well-shielded SVGA cable assemblies featuring HD15 connectors to “pass stringent EMI emissions requirements.” Bally also uses serial RS232 DB9 cables for their touchscreen interactive video games, some of which utilize bulkhead-mounted, dual-sided adapters to pass cables through enclosures.

FIGURE 5. To help a company meet stringent shielding requirements, L-com designed a cable assembly that provides enhanced shielding, with the shell connecting the braid to the D-Sub connector and ensuring 360° shielding throughout the assembly.

Matt Nitka, lead engineer for a medical product manufacturer, shares Bally’s use of 9-pin D-Sub serial RS232 cables for touchscreen monitor displays. Also similar to Bally but with serial cables, Nitka states they must pass rigorous UL emissions demands and require 360° shielding with negligible EMI leakage.

Industry-standard cables use a foil/mylar shield and carry this shield from connector to connector via an electrically connected drain wire. These cables may or may not shield the area under the backshell mold. L-com’s premium line of cables, however, adds a tinned copper braid shield over the foil/mylar shield and a steel internal shell under the overmold. As shown in Figure 5, the braid provides additional shielding and the shell connects the cable braid to the connector, ensuring 360° shielding throughout the assembly.

A Versatile Solution


With numerous applications taking advantage of the attractive features of this connector system, D-Sub connectors appear to be in no danger of extinction. They are simply too versatile, reliable, and offer many options for passing signals from point A to B.

Latest News
L-com Expands Its Shielded Modular Line with a Shielded Side-Exit Cat5e Jack

Helpful Links
L-com Home Page
About L-com
Custom Products
and OEM Services
HyperLink Wireless ProductsHyperLink
Wireless Products
RoHS Compliance
Product Wizards
Product Configurator
Product Comparisons
Technical Resources
Press Release Archive
Newsletter Archive
Request Print Catalog
and Download PDF Files
Newsletter Feedback
Friendly & Knowledgeable Service
         

Other newsletters that may be of interest to you:
 
5/21/2013 Pros-and-Cons-of-Switching-to-a-Fiber-Optic-LAN
5/14/2013 Ethernet Media Converter Applications
5/7/2013 Product Spotlight - L-com's best selling WiFi Antenna
4/23/2013 900 MHz Antennas and Amplifiers for SCADA, Industrial and RFID applications
4/23/2013 HDMI® Active Extenders, Splitters, and Switches
4/16/2013 Installing a Security and Surveillance Camera
4/16/2013 L-com's Antenna Product Wizard
4/9/2013 Which Right Angle Product is Right for You?
4/9/2013 Line of Sight (LOS) Overview
3/26/2013 PoE Offers Cost Savings and Installation Flexibility
3/19/2013 Broadband Antennas for DAS Applications and More
3/12/2013 Manually Switching Serial Data Lines
3/5/2013 What is an Antenna Array?
2/19/2013 Power Management Systems and UPSs
2/19/2013 Antenna Gain Patterns and Wireless Network Design
2/12/2013 Determining Access Point Connector Types
2/12/2013 What is Ingress Protection (IP)?
2/5/2013 Wireless Network System Overview
1/22/2013 how-to-make-your-own-wall-plates-and-rack-panels
1/22/2013 Weatherproof NEMA-Rated Enclosures
1/15/2013 How To Order Large Quantity Custom Products
1/8/2013 Wireless Network Application Overviews
1/1/2013 When Too Much Gain Is a Bad Thing
1/1/2013 L-com's Authorized Distributors
12/18/2012 L-com's Universal Rack Panels (UPR series)
12/11/2012 What is a MIMO antenna? MIMO Antennas Explained
12/11/2012 Bend Insensitive Fiber Optic Cables
12/4/2012 WiFi Antenna Polarization
11/20/2012 LSZH USB Cable Assemblies
11/20/2012 Wireless Access Points and Wireless USB Adapters
11/13/2012 Digital Video Interface Overview
11/13/2012 Choosing the Right WiFi Antenna for Your Application
11/6/2012 Which Frequency is Best for My Application?
10/23/2012 Cable Management Accessories
10/23/2012 How to Set Up a Laptop WiFi Booster Kit For Indoor Use
10/16/2012 Name Brands that L-com Distributes
10/9/2012 L-com Explains Low Loss Coax Cable
10/9/2012 Tight Angle Audio/Video Products
10/2/2012 HyperLink Brand Ceiling Mount MIMO Antennas
9/18/2012 How to set up a HyperLink brand outdoor WiFi Booster
9/18/2012 The Custom Manufacturing Quandary
9/11/2012 New Whitepaper - WiFi Antenna Installation Best Practices
9/11/2012 Ruggedized USB and HDMI Cable Assemblies
8/21/2012 USB Cables that Don't Pop Out of the Port
8/14/2012 HyperLink Brand Indoor WiFi Boosters
7/24/2012 Using Shielded Cable to Protect Data from EMI/RFI
7/17/2012 Converting Ethernet from Copper to Fiber and Back
7/10/2012 Grid Antennas that Steal the Show!
6/19/2012 In the Age of Right Angles
6/12/2012 Don't Skip Lightning Protection!
5/22/2012 Customer-Premises Equipment for Wireless Networks
5/15/2012 PVC, LSZH, and Polyurethane: Know your cable jacket choices
4/24/2012 What are lightning protectors?
4/17/2012 RJ45 Coupler Overview
4/10/2012 L-com's CA-400 Low Loss Coaxial Cable for Antenna Systems
3/20/2012 Unique USB cable designs from L-com
3/13/2012 Typical LAN structured cabling system
2/14/2012 Organize your fiber network with racks and enclosures
1/17/2012 Common Fiber Problems
1/10/2012 Commercial Networking vs Industrial Networking
12/20/2011 Customizable USB Products
12/13/2011 OTDR Fiber Testers - Feature Packed, Aggressively Priced
11/15/2011 Right angle D-Sub adapters solve problems
11/8/2011 What does SCSI mean?
10/18/2011 New industrial ethernet switches
10/11/2011 Heated Weatherproof Enclosure Options
9/20/2011 L-com's New USB 2.0 IP67 Field Installable Connectors
9/13/2011 2.4 GHz Wireless Amplifiers
8/23/2011 Protect Your 15 VDC and 24 VDC PoE Lines
8/16/2011 A new angle on Ethernet cabling
8/9/2011 How lightning affects electronics and how to stop it
7/19/2011 Why use Field Termination D-Sub Connectors?
7/12/2011 A/V Splitters, Switches and Extension Solutions from L-com
6/14/2011 HyperAmp-High-Powered-Amplifiers
5/17/2011 Don't leave yourself exposed and unprotected!
5/3/2011 Media Converters Solve Ethernet Distance Problems
4/19/2011 Latching USB Technology
4/12/2011 L-com's FCC-Certified 2.4GHz Amplifier Kits
3/15/2011 LSZH for Data Cables
3/2/2011 How to buy a passive PoE Injector/Tap
2/15/2011 2.4 GHz Omni directional WiFi Antennas
1/25/2011 Why You Need Weatherproof Industrial Enclosures
1/19/2011 Everything Telecom/Modular Bulk Cable
1/4/2011 Why USB Technology Pervades Connectivity - Vol. 11 No. 1
12/21/2010 Getting Started With Power-over-Ethernet - Vol. 10 No. 40
11/25/2010 L-com's New SC-232 Series Interface Converters - Vol. 10 No. 36
10/28/2010 L-com's 2.4 GHz FCC Certified WiFi Amplifier Kits - Vol. 10 No. 35
10/26/2010 Coaxial Products to Fill Every Need - Vol. 10 No. 34
9/30/2010 Tips on Selecting the Right Coaxial Cable - Vol. 10 No. 28
9/9/2010 Lightning Never Strikes Twice - Vol. 10 No. 29
8/24/2010 Power over Ethernet - Vol. 10 No. 26
8/19/2010 USB 2.0 and 3.0 Products Available at L-com - Vol. 10 No. 25
7/27/2010 Want a clear wireless signal? It starts with the antenna! - Vol. 10 No. 24
7/20/2010 IEEE-488 Tutorial - Vol. 10 No. 23
7/8/2010 Cat 5e, Cat 6, Cables, Connectors, and more! - Vol. 10 No. 22
6/29/2010 Fiber Optic Tutorial - Vol. 10 No. 20
6/25/2010 NEMA Enclosures Tutorial - Vol. 10 No. 16
6/1/2010 Lightning and Surge Protectors Tutorial - Vol. 10 No. 18
5/4/2010 What Are "Rubber Duck" Antennas - Vol. 10 No. 12
3/16/2010 L-com now offers M12 cables, connectors, and adapters! - Vol. 10 No. 11
2/23/2010 L-com Has Your USB 2.0 Application Covered - Vol. 10 No. 7
2/16/2010 PoE Products: L-com sells Power over Ethernet - Vol. 10 No. 6
2/9/2010 Testing a WiFi Amplifier - The Dos and Don’ts - Vol. 10 No. 5
2/2/2010 Antenna Polarization and How it Works for You - Vol. 10 No. 3
1/26/2010 What is a Reverse Polarized Connector? - Vol. 10 No. 2
12/22/2009 D-Subs Continue to Lock Down Dependability - Vol. 9 No. 63
12/15/2009 USB: The Future and the Past - Vol. 9 No.62
12/1/2009 HDMI Evolution - Vol. 9 No. 61
11/24/2009 Common Tech Questions - Vol. 9 No. 60
11/10/2009 Rack Systems & Patch Panels - Vol. 9 No. 58
11/3/2009 What Is 10 Gigabit Fiber? - Vol. 9 No. 57
10/27/2009 Media Converters - Vol. 9 No. 56
10/15/2009 NEMA Rated Weatherproof Enclosures for European Applications - Vol. 9 No. 54
10/13/2009 L-com's Online Cable Configurator - Vol. 9 No. 53
10/8/2009 Signal Splitters / Signal Combiners - Vol. 9 No. 52
10/6/2009 Flatscreen TVs and the Cables Used On Them - Vol. 9 No. 51
9/24/2009 NEMA Rated Outdoor Enclosures - Vol. 9 No. 49
9/3/2009 USB Mini-B Connectors and Cables - Vol. 9 No. 45
9/1/2009 Niche Products - Vol. 9 No. 44
8/27/2009 New Wireless LAN Radios from L-com - Vol. 9 No. 43
8/25/2009 Reverse Polarized Connector - Vol. 9 No. 42
8/18/2009 Different Shielding Types - Vol. 9 No. 41
8/6/2009 Inside L-com's Master Catalog - Vol. 9 No. 39
7/30/2009 L-com Video - Grid Antenna - Vol. 9 No. 37
7/23/2009 Right Angle RJ45 Couplers - Vol. 9 No. 36
7/7/2009 Antenna Gain - Vol. 9 No. 33
6/30/2009 Coaxial 101 - Vol. 9 No. 32
6/18/2009 Coaxial Crimping Tools - Vol. 9 No. 31
6/2/2009 Fiber Cable Colors - What do they mean? - Vol. 9 No. 28
5/26/2009 Keeping it Green at L-com - Vol. 9 No. 27
5/19/2009 KVM Switching Over IP - Vol. 9 No. 26
5/5/2009 L-com Product Solutions for A/V Installers - Vol. 9 No. 24
4/30/2009 Wires in a Wireless World - Vol. 9 No. 23
4/28/2009 L-com Introduces its New Online Cable Configurator - Vol. 9 No. 22
4/23/2009 IP67 Products and Ratings - Vol. 9 No. 21
4/21/2009 Digital Signage Support from L-com - Vol. 9 No. 20
4/7/2009 DisplayPort Interfaces - Vol. 9 No. 17
3/31/2009 New USB Type A to Type A LSZH Cables from L-com - Vol. 9 No. 16
3/19/2009 The Security Industry and L-com Products - Vol. 9 No. 15
3/10/2009 New Products Make Your Job Easier! - Vol. 9 No. 12
3/3/2009 Industrial Connectivity Products - Vol. 9 No. 11
2/26/2009 Modular Cable Colors - Vol. 9 No. 10
2/24/2009 Plenum vs. LSZH - Vol. 9 No. 9
2/12/2009 We Want To Hear From You!
2/10/2009 Flatscreen TVs and the Cables Used on Them - Vol. 9 No. 5
1/29/2009 How is a Cable Born? - Vol. 9 No. 3
1/29/2009 Signal Splitters / Signal Combiners
1/27/2009 Colored Fiber Optic Cables - Vol. 9 No. 2
10/28/2008 Let the Magic of L-com's Product Wizards Work for You! - Vol. 8 No. 22
10/14/2008 An Expert's Opinion About DisplayPort Interfaces - Vol. 8 No. 21
10/7/2008 Fundamentals of a USB Cable - Vol. 8 No. 20
9/30/2008 Things to Know When Selecting a Modular Plug - Vol. 8 No. 19
9/2/2008 L-com Sells HyperLink Wireless Equipment - Vol. 8 No. 18
8/26/2008 Get a Clear Signal with L-com's Fiber Optic Testers - Vol. 8 No. 17
8/19/2008 Connector Covers: Protect Your Ports! - Vol. 8 No. 16
7/29/2008 Custom Cable Assembly Lengths and Wiring Schemes - Vol. 8 No. 15
7/1/2008 Category 5E vs. Category 6 - What is the Difference? - Vol. 8 No. 12
6/24/2008 Redundant Network Architecture - Vol. 8 No. 9
5/20/2008 Standard Grade SVGA Cables - Vol. 8 No. 5
4/1/2008 What is a Reverse Polarized Connector? - Vol. 8 No. 7
1/22/2008 Origins of BNC, SMA and Other Connectors - Vol. 8 No. 1
12/26/2007 IEEE-1394 (Firewire) Technology
11/27/2007 L-com's Fiber Optic Capabilities
11/12/2007 Converting USB
10/30/2007 Field-Friendly Products
10/10/2007 Bulk Cable
10/10/2007 Extending Video Over Long Distances
9/10/2007 Thermal Management Best Practices: Racks and Enclosures
7/10/2007 Longer Length HDMI Cables
6/19/2007 Clipped LC Connector Cables
6/19/2007 MTP Fiber Cables
6/5/2007 RJ (Registered Jack) Style Modular Plugs
5/8/2007 How to Integrate FieldBus and Serial Technology to Ethernet
4/3/2007 Right Angle D-Subminiature Adapters
3/14/2007 USB Technology
2/13/2007 Video Over Alternative Media Types
1/10/2007 Custom Cable Assembly Lengths and Wiring Schemes
12/8/2006 Ethernet Myths Revealed
11/14/2006 What's Your Choice - Cable Management or Network Downtime?
10/31/2006 Securing Your Network
9/19/2006 Shielded Cabling and Network Components
9/19/2006 KVM Switching Over IP
8/29/2006 Shielded Network and Cabling Components
7/11/2006 Data Protocol Conversion
6/13/2006 IEEE-488 GPIB Fundamentals
5/9/2006 Video Display Fundamentals
4/11/2006 Redundant Network Architectures
3/14/2006 USB Conversion
2/14/2006 Panel Mount Adapters
1/17/2006 Waterproof Connectors
12/13/2005 How to Extend Your Network
11/15/2005 Coaxial Cabling - What is it and where is it used?
10/18/2005 Plenum vs. LSZH Video Cables
10/4/2005 Structured Wiring Components
9/20/2005 Fundamentals of SCSI - What Is It and Where Is It Used?
9/7/2005 Basic Operation of a Fiber Cable
8/23/2005 DVI and HDMI Interfaces Worth Knowing
8/16/2005 Category 5E vs. Category 6 - What is the difference?
7/26/2005 Understanding Data Cable Characteristics
7/12/2005 KVM Switches and Extenders
6/7/2005 New Additions - L-com's Fiber Products
4/5/2005 Cable Tester Month
3/22/2005 Fundamentals of Firewire
3/8/2005 75 Ohm, 50 Ohm - Which one is right for you?
2/22/2005 Industrial Ethernet
2/8/2005 Cable Management
1/25/2005 Fundamentals of USB
9/1/2004 Structured Wiring
8/2/2004 IEEE-1394 / Firewire
5/3/2004 SOHO Wireless Networking
4/1/2004 Universal Serial Bus (USB)
3/1/2004 Network Media Conversion