A signal splitter / signal combiner is defined as a transmission component which divides or sums power between two or more ports. L-com signal splitters / signal combiners are commonly used for connecting more than one antenna to a single radio. The following are some examples:
L-com's HyperGain® series signal splitters / signal combiners feature cast aluminum weather-proof construction and can be installed indoors or outdoors. They are available in 2-way, 3-way and 4-way models and feature N-female or reverse polarity TNC jack connectors supporting the most popular RF connector types. Additionally these versatile filters will pass DC power to all ports when used with an amplified system.
L-com's signal splitter product offering covers the following frequencies: 900 MHz, 2.4 GHz, 3.5 GHZ, 5.4 GHz, 5.8 GHz and wideband signal splitters, which are designed to cover a frequency range of 750 MHz to 2700 MHz.
Note: To ensure proper operation, any open splitter ports should be terminated with a high quality 50 Ohm terminator. We recommend the ANM-TERM1, 0-6 GHz Type N Male Terminator 50 Ohm
L-com Global Connectivity 45 Beechwood Drive North Andover, MA 01845www.L-com.com E-mail: sales@L-com.com Phone: 1-800-341-5266 Fax: 1-978-689-9484