Cart is Empty
Home   Request Catalog   Custom Cables   Product Wizards   Technical Resources   Contact Us

To our valued customers: The L-com offices will be closed Monday, May 27th, in observance of the Memorial Day holiday.

Basic Operation of a Fiber Cable
(Wednesday, September 07, 2005)
 
 
www.L-com.com

Volume 4, Number 18

Ordering and Technical Support
800-343-1455   
www.L-com.com
Basic Operation of a Fiber Cable
The basic operation of a fiber cable whether it be glass or plastic fiber is the same. An optical transceiver sends pulses of light via an LED (Light Emitting Diode) or Laser into the core of the fiber cable where the light then "bounces" off the interior walls of the fiber core and is then received by the optical transceiver on the opposite end of the cable. The phenomenon where the light "bounces" off the walls of the fiber core is called Total Internal Reflection. Total Internal Reflection reflects 100% of the light being sent down the fiber cable. Both glass and plastic fiber cable have a coating called cladding which surrounds the core where the light travels. The cladding keeps the light from escaping the core ensuring it reaches its destination.

Total Internal Reflection
Glass Optical Fiber Cables

There are two types of glass fiber optic cables, multimode and singlemode. The word mode (ray of light) refers to the fact that either several (multi), or just one mode (single), will pass through the cable at the same time. Singlemode cable can transmit voice, video and data over a longer distance (up to 100 Kilometers!) than multimode fiber cable and is typically used with laser driven transceivers at each end of the cable. These laser transceivers are sometimes four times the cost of multimode transceivers. Multimode cable is generally used for distances less than two kilometers and can be used with less expensive LED driven transceivers.

The basic construction of a glass fiber optic cable consists of the following:

Fiber: Is made up of the core which is the glass that the light travels through and the Cladding which is a glass coating over the core that keeps light in.

Buffer Coating: Protective cover (typically plastic) over Cladding

Strength Member: Usually Kevlar strands that add strength to the cable

Jacket : Outside layer of the cable typically PVC, Plenum or LSZH

Both Glass and Plastic optical cable experience attenuation, or loss of light. Over distance, the effectiveness of the light pulse decreases causing errors in the data being transmitted. The physical properties of singlemode fiber offer very low attenuation over distance, which is why singlemode fiber is used to connect cities, campuses and wide area telephone and data networks. Multimode fiber cables experience more attenuation, or loss, per the same distance than singlemode fiber.

Typically Multimode fiber is used within buildings and to connect buildings together in a campus environment. Lastly, plastic optical fiber has the highest attenuation, or loss of light per distance compared to the glass fiber cable types mentioned above. For many applications the maximum distance for plastic fiber cable is less than 10 meters.

Glass Fiber specifications list the core and cladding diameters as a ratio. The example below details the core to cladding ratio for the three most common types of glass fiber cable. Multimode fiber is commonly 62.5/125 or 50/125 micron, singlemode fiber is commonly 9/125 micron.

View Video Clip

Types of Polishes on Glass Fiber Connectors

The polish on a fiber connector dictates the amount of back reflection. Back reflection is a measure of the light reflected off the polished end of a fiber connector measured in negative dB. In some singlemode fiber applications the amount of back reflection on the connectors can be critical.

View Video Clip

Typical Applications for Glass Fiber Optic Cables



Plastic Optical Fiber Cables

Plastic optical fiber cables experience high loss or attenuation and are used on short distance applications such as in cars, in airplanes and with high-end audio equipment such as DVD players, CD players and MP3 and DAT recorders. The low cost and ease of connectorization make plastic optical fiber the logical choice for these short distance applications.

Plastic optical fiber, like glass fiber is immune to lightning, and EMI and RFI.
Using plastic fiber on high-end audio systems eliminates the distortion caused
by capacitance and resistance of traditional wire audio cables, guaranteeing a "pure" sound.

Anatomy of a Plastic Optical Cable

Core:

Plastic fiber where light pulses
travel through.
Cladding: Coating around the plastic core
which keeps the light from escaping.
Jacket: Outer protective coating,
typically made of PVC.

Typical applications for Plastic fiber optic cables

Audio Equipment
Aircraft Control Systems
Automobile Control Systems
         

Other newsletters that may be of interest to you:
 
5/21/2013 Pros-and-Cons-of-Switching-to-a-Fiber-Optic-LAN
5/14/2013 Ethernet Media Converter Applications
5/7/2013 Product Spotlight - L-com's best selling WiFi Antenna
4/23/2013 900 MHz Antennas and Amplifiers for SCADA, Industrial and RFID applications
4/23/2013 HDMI® Active Extenders, Splitters, and Switches
4/16/2013 Installing a Security and Surveillance Camera
4/16/2013 L-com's Antenna Product Wizard
4/9/2013 Which Right Angle Product is Right for You?
4/9/2013 Line of Sight (LOS) Overview
3/26/2013 PoE Offers Cost Savings and Installation Flexibility
3/19/2013 Broadband Antennas for DAS Applications and More
3/12/2013 Manually Switching Serial Data Lines
3/5/2013 What is an Antenna Array?
2/19/2013 Power Management Systems and UPSs
2/19/2013 Antenna Gain Patterns and Wireless Network Design
2/12/2013 Determining Access Point Connector Types
2/12/2013 What is Ingress Protection (IP)?
2/5/2013 Wireless Network System Overview
1/22/2013 how-to-make-your-own-wall-plates-and-rack-panels
1/22/2013 Weatherproof NEMA-Rated Enclosures
1/15/2013 How To Order Large Quantity Custom Products
1/8/2013 Wireless Network Application Overviews
1/1/2013 When Too Much Gain Is a Bad Thing
1/1/2013 L-com's Authorized Distributors
12/18/2012 L-com's Universal Rack Panels (UPR series)
12/11/2012 What is a MIMO antenna? MIMO Antennas Explained
12/11/2012 Bend Insensitive Fiber Optic Cables
12/4/2012 WiFi Antenna Polarization
11/20/2012 LSZH USB Cable Assemblies
11/20/2012 Wireless Access Points and Wireless USB Adapters
11/13/2012 Digital Video Interface Overview
11/13/2012 Choosing the Right WiFi Antenna for Your Application
11/6/2012 Which Frequency is Best for My Application?
10/23/2012 Cable Management Accessories
10/23/2012 How to Set Up a Laptop WiFi Booster Kit For Indoor Use
10/16/2012 Name Brands that L-com Distributes
10/9/2012 L-com Explains Low Loss Coax Cable
10/9/2012 Tight Angle Audio/Video Products
10/2/2012 HyperLink Brand Ceiling Mount MIMO Antennas
9/18/2012 How to set up a HyperLink brand outdoor WiFi Booster
9/18/2012 The Custom Manufacturing Quandary
9/11/2012 New Whitepaper - WiFi Antenna Installation Best Practices
9/11/2012 Ruggedized USB and HDMI Cable Assemblies
8/21/2012 USB Cables that Don't Pop Out of the Port
8/14/2012 HyperLink Brand Indoor WiFi Boosters
7/24/2012 Using Shielded Cable to Protect Data from EMI/RFI
7/17/2012 Converting Ethernet from Copper to Fiber and Back
7/10/2012 Grid Antennas that Steal the Show!
6/19/2012 In the Age of Right Angles
6/12/2012 Don't Skip Lightning Protection!
5/22/2012 Customer-Premises Equipment for Wireless Networks
5/15/2012 PVC, LSZH, and Polyurethane: Know your cable jacket choices
4/24/2012 What are lightning protectors?
4/17/2012 RJ45 Coupler Overview
4/10/2012 L-com's CA-400 Low Loss Coaxial Cable for Antenna Systems
3/20/2012 Unique USB cable designs from L-com
3/13/2012 Typical LAN structured cabling system
2/14/2012 Organize your fiber network with racks and enclosures
1/17/2012 Common Fiber Problems
1/10/2012 Commercial Networking vs Industrial Networking
12/20/2011 Customizable USB Products
12/13/2011 OTDR Fiber Testers - Feature Packed, Aggressively Priced
11/15/2011 Right angle D-Sub adapters solve problems
11/8/2011 What does SCSI mean?
10/18/2011 New industrial ethernet switches
10/11/2011 Heated Weatherproof Enclosure Options
9/20/2011 L-com's New USB 2.0 IP67 Field Installable Connectors
9/13/2011 2.4 GHz Wireless Amplifiers
8/23/2011 Protect Your 15 VDC and 24 VDC PoE Lines
8/16/2011 A new angle on Ethernet cabling
8/9/2011 How lightning affects electronics and how to stop it
7/19/2011 Why use Field Termination D-Sub Connectors?
7/12/2011 A/V Splitters, Switches and Extension Solutions from L-com
6/14/2011 HyperAmp-High-Powered-Amplifiers
5/17/2011 Don't leave yourself exposed and unprotected!
5/3/2011 Media Converters Solve Ethernet Distance Problems
4/19/2011 Latching USB Technology
4/12/2011 L-com's FCC-Certified 2.4GHz Amplifier Kits
3/15/2011 LSZH for Data Cables
3/2/2011 How to buy a passive PoE Injector/Tap
2/15/2011 2.4 GHz Omni directional WiFi Antennas
1/25/2011 Why You Need Weatherproof Industrial Enclosures
1/19/2011 Everything Telecom/Modular Bulk Cable
1/4/2011 Why USB Technology Pervades Connectivity - Vol. 11 No. 1
12/21/2010 Getting Started With Power-over-Ethernet - Vol. 10 No. 40
11/25/2010 L-com's New SC-232 Series Interface Converters - Vol. 10 No. 36
10/28/2010 L-com's 2.4 GHz FCC Certified WiFi Amplifier Kits - Vol. 10 No. 35
10/26/2010 Coaxial Products to Fill Every Need - Vol. 10 No. 34
9/30/2010 Tips on Selecting the Right Coaxial Cable - Vol. 10 No. 28
9/9/2010 Lightning Never Strikes Twice - Vol. 10 No. 29
8/24/2010 Power over Ethernet - Vol. 10 No. 26
8/19/2010 USB 2.0 and 3.0 Products Available at L-com - Vol. 10 No. 25
7/27/2010 Want a clear wireless signal? It starts with the antenna! - Vol. 10 No. 24
7/20/2010 IEEE-488 Tutorial - Vol. 10 No. 23
7/8/2010 Cat 5e, Cat 6, Cables, Connectors, and more! - Vol. 10 No. 22
6/29/2010 Fiber Optic Tutorial - Vol. 10 No. 20
6/25/2010 NEMA Enclosures Tutorial - Vol. 10 No. 16
6/1/2010 Lightning and Surge Protectors Tutorial - Vol. 10 No. 18
5/4/2010 What Are "Rubber Duck" Antennas - Vol. 10 No. 12
3/16/2010 L-com now offers M12 cables, connectors, and adapters! - Vol. 10 No. 11
2/23/2010 L-com Has Your USB 2.0 Application Covered - Vol. 10 No. 7
2/16/2010 PoE Products: L-com sells Power over Ethernet - Vol. 10 No. 6
2/9/2010 Testing a WiFi Amplifier - The Dos and Don’ts - Vol. 10 No. 5
2/2/2010 Antenna Polarization and How it Works for You - Vol. 10 No. 3
1/26/2010 What is a Reverse Polarized Connector? - Vol. 10 No. 2
12/22/2009 D-Subs Continue to Lock Down Dependability - Vol. 9 No. 63
12/15/2009 USB: The Future and the Past - Vol. 9 No.62
12/1/2009 HDMI Evolution - Vol. 9 No. 61
11/24/2009 Common Tech Questions - Vol. 9 No. 60
11/10/2009 Rack Systems & Patch Panels - Vol. 9 No. 58
11/3/2009 What Is 10 Gigabit Fiber? - Vol. 9 No. 57
10/27/2009 Media Converters - Vol. 9 No. 56
10/15/2009 NEMA Rated Weatherproof Enclosures for European Applications - Vol. 9 No. 54
10/13/2009 L-com's Online Cable Configurator - Vol. 9 No. 53
10/8/2009 Signal Splitters / Signal Combiners - Vol. 9 No. 52
10/6/2009 Flatscreen TVs and the Cables Used On Them - Vol. 9 No. 51
9/24/2009 NEMA Rated Outdoor Enclosures - Vol. 9 No. 49
9/3/2009 USB Mini-B Connectors and Cables - Vol. 9 No. 45
9/1/2009 Niche Products - Vol. 9 No. 44
8/27/2009 New Wireless LAN Radios from L-com - Vol. 9 No. 43
8/25/2009 Reverse Polarized Connector - Vol. 9 No. 42
8/18/2009 Different Shielding Types - Vol. 9 No. 41
8/6/2009 Inside L-com's Master Catalog - Vol. 9 No. 39
7/30/2009 L-com Video - Grid Antenna - Vol. 9 No. 37
7/23/2009 Right Angle RJ45 Couplers - Vol. 9 No. 36
7/7/2009 Antenna Gain - Vol. 9 No. 33
6/30/2009 Coaxial 101 - Vol. 9 No. 32
6/18/2009 Coaxial Crimping Tools - Vol. 9 No. 31
6/2/2009 Fiber Cable Colors - What do they mean? - Vol. 9 No. 28
5/26/2009 Keeping it Green at L-com - Vol. 9 No. 27
5/19/2009 KVM Switching Over IP - Vol. 9 No. 26
5/5/2009 L-com Product Solutions for A/V Installers - Vol. 9 No. 24
4/30/2009 Wires in a Wireless World - Vol. 9 No. 23
4/28/2009 L-com Introduces its New Online Cable Configurator - Vol. 9 No. 22
4/23/2009 IP67 Products and Ratings - Vol. 9 No. 21
4/21/2009 Digital Signage Support from L-com - Vol. 9 No. 20
4/7/2009 DisplayPort Interfaces - Vol. 9 No. 17
3/31/2009 New USB Type A to Type A LSZH Cables from L-com - Vol. 9 No. 16
3/19/2009 The Security Industry and L-com Products - Vol. 9 No. 15
3/10/2009 New Products Make Your Job Easier! - Vol. 9 No. 12
3/3/2009 Industrial Connectivity Products - Vol. 9 No. 11
2/26/2009 Modular Cable Colors - Vol. 9 No. 10
2/24/2009 Plenum vs. LSZH - Vol. 9 No. 9
2/12/2009 We Want To Hear From You!
2/10/2009 Flatscreen TVs and the Cables Used on Them - Vol. 9 No. 5
1/29/2009 How is a Cable Born? - Vol. 9 No. 3
1/29/2009 Signal Splitters / Signal Combiners
1/27/2009 Colored Fiber Optic Cables - Vol. 9 No. 2
10/28/2008 Let the Magic of L-com's Product Wizards Work for You! - Vol. 8 No. 22
10/14/2008 An Expert's Opinion About DisplayPort Interfaces - Vol. 8 No. 21
10/7/2008 Fundamentals of a USB Cable - Vol. 8 No. 20
9/30/2008 Things to Know When Selecting a Modular Plug - Vol. 8 No. 19
9/2/2008 L-com Sells HyperLink Wireless Equipment - Vol. 8 No. 18
8/26/2008 Get a Clear Signal with L-com's Fiber Optic Testers - Vol. 8 No. 17
8/19/2008 Connector Covers: Protect Your Ports! - Vol. 8 No. 16
7/29/2008 Custom Cable Assembly Lengths and Wiring Schemes - Vol. 8 No. 15
7/1/2008 Category 5E vs. Category 6 - What is the Difference? - Vol. 8 No. 12
6/24/2008 Redundant Network Architecture - Vol. 8 No. 9
5/20/2008 Standard Grade SVGA Cables - Vol. 8 No. 5
4/1/2008 What is a Reverse Polarized Connector? - Vol. 8 No. 7
1/22/2008 Origins of BNC, SMA and Other Connectors - Vol. 8 No. 1
12/26/2007 IEEE-1394 (Firewire) Technology
11/27/2007 L-com's Fiber Optic Capabilities
11/12/2007 Converting USB
10/30/2007 Field-Friendly Products
10/10/2007 Bulk Cable
10/10/2007 Extending Video Over Long Distances
9/10/2007 Thermal Management Best Practices: Racks and Enclosures
7/10/2007 Longer Length HDMI Cables
6/19/2007 Clipped LC Connector Cables
6/19/2007 MTP Fiber Cables
6/5/2007 RJ (Registered Jack) Style Modular Plugs
5/8/2007 How to Integrate FieldBus and Serial Technology to Ethernet
4/3/2007 Right Angle D-Subminiature Adapters
3/14/2007 USB Technology
2/13/2007 Video Over Alternative Media Types
1/10/2007 Custom Cable Assembly Lengths and Wiring Schemes
12/8/2006 Ethernet Myths Revealed
11/14/2006 What's Your Choice - Cable Management or Network Downtime?
10/31/2006 Securing Your Network
9/19/2006 Shielded Cabling and Network Components
9/19/2006 KVM Switching Over IP
8/29/2006 Shielded Network and Cabling Components
7/11/2006 Data Protocol Conversion
6/13/2006 IEEE-488 GPIB Fundamentals
5/9/2006 Video Display Fundamentals
4/11/2006 Redundant Network Architectures
3/14/2006 USB Conversion
2/14/2006 Panel Mount Adapters
1/17/2006 Waterproof Connectors
12/13/2005 How to Extend Your Network
11/15/2005 Coaxial Cabling - What is it and where is it used?
10/18/2005 Plenum vs. LSZH Video Cables
10/4/2005 Structured Wiring Components
9/20/2005 Fundamentals of SCSI - What Is It and Where Is It Used?
9/7/2005 Basic Operation of a Fiber Cable
8/23/2005 DVI and HDMI Interfaces Worth Knowing
8/16/2005 Category 5E vs. Category 6 - What is the difference?
7/26/2005 Understanding Data Cable Characteristics
7/12/2005 KVM Switches and Extenders
6/7/2005 New Additions - L-com's Fiber Products
4/5/2005 Cable Tester Month
3/22/2005 Fundamentals of Firewire
3/8/2005 75 Ohm, 50 Ohm - Which one is right for you?
2/22/2005 Industrial Ethernet
2/8/2005 Cable Management
1/25/2005 Fundamentals of USB
9/1/2004 Structured Wiring
8/2/2004 IEEE-1394 / Firewire
5/3/2004 SOHO Wireless Networking
4/1/2004 Universal Serial Bus (USB)
3/1/2004 Network Media Conversion