L-com Global Connectivity
  
Cart is Empty
  
USA & Canada (800) 341-5266     International +1 (978) 682-6936

Coaxial Connector Termination: Which Technique is Right for You
(Tuesday, September 15, 2015)
 
Typically, there are three ways to terminate a coaxial connector: crimp, clamp or twist-on.  Each method has its benefits, and choosing the right one is imperative for optimal performance of your coaxial cable assemblies.
 
Here is an overview of each method:
 
Crimp method is the most popular variation. It reduces installation time and provides good electrical and mechanical connection. The cable shield is crimped to the coaxial connector using the crimp ring. The
connector center conductor is attached to the cable center conductor by crimp or solder.



Clamp method is often used in cases where weather exposure is a factor, or when crimp tools are unavailable. With this technique the cable shield is clamped between the coaxial connector body and back nut. The connector center conductor is usually soldered to the cable center conductor.



Twist-on method is the quickest and easiest approach, though it can be less reliable than other methods. It is most often used in field applications because of its simplicity and no need for special tools.


Determining the right method of termination is dependent upon your specific application. Using the correct termination method will ensure optimal mechanical and electrical integrity of your connection.
 
Whichever coaxial connector termination method you choose, be sure to follow the manufacturer's recommendations regarding cable strip length and crimp die size.
 
Click here for more information on all of our coaxial products.

 

 


Other newsletters that may be of interest to you:
 
6/13/2016 The Benefits of 24 AWG Cable
5/24/2016 Why our Premium D-Sub Cables are Superior
5/17/2016 An A to Z review of the 802.11 standards
4/12/2016 USB Type-C Cable Assemblies Provide Legacy USB Connectivity
3/1/2016 Passive Intermodulation (PIM) Explained
2/2/2016 The Industrial Internet of Things (IIoT)
12/15/2015 Cable Shielding - How it Works
12/1/2015 Embedded Antennas and the IoT
11/10/2015 Long Live RS-232!
9/22/2015 The Differences between Solid and Stranded Cable
9/15/2015 Coaxial Connector Termination: Which Technique is Right for You
8/11/2015 802.11ah Breathes New Life to the 900 MHz Frequency Band
7/14/2015 Cable Options For Every Application
7/7/2015 900 MHz - Your NLOS Friend
6/2/2015 802.11ax Offers Blazing Fast Wi-Fi Connectivity
5/12/2015 The NBASE-T Alliance - Fostering Multi-Gig Speeds over Cat5e/6 Cabling
4/7/2015 L-com and The Internet of Things (IoT)
3/3/2015 802.3bt the Promise for Higher Power PoE
1/6/2015 L-com's Family of Brands - A Solution for Every Application
12/9/2014 Cat6a Products for High-Speed Networking
  Page:  1 of 15
    
 
Free Newsletter
L-com Global Connectivity           50 High Street           North Andover, MA 01845
www.L-com.com E-mail: sales@L-com.com 1-800-341-5266 www.Facebook.com/LcomGlobal


© Infinite Electronics International, Inc.