L-com Global Connectivity
  
Cart is Empty
  
USA & Canada (800) 341-5266     International +1 (978) 682-6936
 
802.11ah Breathes New Life to the 900 MHz Frequency Band
(Tuesday, August 11, 2015)
 
The IEEE is busy working on a new standard which promises to extend the range of Wi-Fi connectivity.
 
802.11ah is being developed to address the need for extended signal range, power efficiency and scalability required by today's Wi-Fi networks. Standardization of 802.11ah is slated for early 2016.
 
802.11ah operates on the ISM 900 MHz frequency band which is better at penetrating walls and other obstructions than 2.4 GHz and 5 GHz frequencies. Furthermore, 900 MHz offers longer distance reach than 2.4 and 5 GHz based systems. By utilizing 802.11ah access points, you will be able to extend the reach of your wireless signal with greater power efficiency.
 
802.11ah will also provide support for IoT applications as it is designed to work with relatively low cost battery powered sensors. With a minimum data rate of 150 Kbps the result is short bursty packets which result in limited on-time for sensors increasing battery life and power efficiency. 802.11ah will be a direct competitor of the already seasoned ZigBee technology as well as Z-wave which are both used in mainly sensor networks found in industrial, commercial and residential applications.
 
Some future applications for 802.11ah include smart-home and extended reach home Wi-Fi networks, industrial automation sensor networks, commercial network applications and wearable devices.
 
When 802.11ah becomes standardized and 802.11ah devices are deployed in the months to come,
L-com will be there with support from our wide range of high quality 900 MHz antennas, 900 MHz RF Amplifiers, 900 MHz splitters and filters.
 
In addition to our comprehensive off the shelf selection of 900 MHz connectivity products, L-com can also custom manufacture 900 MHz connectivity products to your specifications. Contact us today to find out more.

 


Other newsletters that may be of interest to you:
 
6/13/2016 The Benefits of 24 AWG Cable
5/24/2016 Why our Premium D-Sub Cables are Superior
5/17/2016 An A to Z review of the 802.11 standards
4/12/2016 USB Type-C Cable Assemblies Provide Legacy USB Connectivity
3/1/2016 Passive Intermodulation (PIM) Explained
2/2/2016 The Industrial Internet of Things (IIoT)
12/15/2015 Cable Shielding - How it Works
12/1/2015 Embedded Antennas and the IoT
11/10/2015 Long Live RS-232!
9/22/2015 The Differences between Solid and Stranded Cable
9/15/2015 Coaxial Connector Termination: Which Technique is Right for You
8/11/2015 802.11ah Breathes New Life to the 900 MHz Frequency Band
7/14/2015 Cable Options For Every Application
7/7/2015 900 MHz - Your NLOS Friend
6/2/2015 802.11ax Offers Blazing Fast Wi-Fi Connectivity
5/12/2015 The NBASE-T Alliance - Fostering Multi-Gig Speeds over Cat5e/6 Cabling
4/7/2015 L-com and The Internet of Things (IoT)
3/3/2015 802.3bt the Promise for Higher Power PoE
1/6/2015 L-com's Family of Brands - A Solution for Every Application
12/9/2014 Cat6a Products for High-Speed Networking
  Page:  1 of 15
    
 
Free Newsletter
L-com Global Connectivity           50 High Street           North Andover, MA 01845
www.L-com.com E-mail: sales@L-com.com 1-800-341-5266 www.Facebook.com/LcomGlobal


© Infinite Electronics International, Inc.