L-com Global Connectivity
  
Cart is Empty
  
USA & Canada (800) 341-5266     International +1 (978) 682-6936
 
Cable Options For Every Application
(Tuesday, July 14, 2015)
 

L-com manufactures many different types of cable assemblies to address just about every connectivity application imaginable. In order to meet the varied requirements of our customers we offer three different grades or lines of cable assemblies- off the shelf.

Premium Line

Our premium cable line offers features such as double shielding, 30µ gold plated contacts, 360 degree full metal back shell covers and more. Our premium cables are designed for the most demanding applications where EMI/RFI can pose a problem and where optimal performance is required.

Deluxe Line

L-com's deluxe cable line offers features including cable shielding, ferrite beads to address the adverse effects of EMI/RFI and more. Our deluxe cable line is well suited for most A/V and networking applications.

Economy Line

Our economy cable line offers the best value for the lowest price. Economy series cables feature gold flash contacts, foil shielding (typically) and more.  Our economy series cables can be used in applications where little to no EMI/RFI is present and in indoor controlled environments.

In addition to thousands of off the shelf cable assemblies, L-com can custom manufacture cables to your exact specifications.

To see a detailed feature list for each of our three lines, click on the link below to view our cable options overview which features USB, D-Subminiature, DVI, HDMI, VGA cable assemblies and more.

 

 

Download L-com's Cable Options Overview


Other newsletters that may be of interest to you:
 
6/13/2016 The Benefits of 24 AWG Cable
5/24/2016 Why our Premium D-Sub Cables are Superior
5/17/2016 An A to Z review of the 802.11 standards
4/12/2016 USB Type-C Cable Assemblies Provide Legacy USB Connectivity
3/1/2016 Passive Intermodulation (PIM) Explained
2/2/2016 The Industrial Internet of Things (IIoT)
12/15/2015 Cable Shielding - How it Works
12/1/2015 Embedded Antennas and the IoT
11/10/2015 Long Live RS-232!
9/22/2015 The Differences between Solid and Stranded Cable
9/15/2015 Coaxial Connector Termination: Which Technique is Right for You
8/11/2015 802.11ah Breathes New Life to the 900 MHz Frequency Band
7/14/2015 Cable Options For Every Application
7/7/2015 900 MHz - Your NLOS Friend
6/2/2015 802.11ax Offers Blazing Fast Wi-Fi Connectivity
5/12/2015 The NBASE-T Alliance - Fostering Multi-Gig Speeds over Cat5e/6 Cabling
4/7/2015 L-com and The Internet of Things (IoT)
3/3/2015 802.3bt the Promise for Higher Power PoE
1/6/2015 L-com's Family of Brands - A Solution for Every Application
12/9/2014 Cat6a Products for High-Speed Networking
  Page:  1 of 15
    
 
Free Newsletter
L-com Global Connectivity           50 High Street           North Andover, MA 01845
www.L-com.com E-mail: sales@L-com.com 1-800-341-5266 www.Facebook.com/LcomGlobal


© Infinite Electronics International, Inc.