L-com Global Connectivity
  
Cart is Empty
  
USA & Canada (800) 341-5266     International +1 (978) 682-6936

L-com and The Internet of Things (IoT)
(Tuesday, April 07, 2015)
 
IoTAs 2015 marches on, the buzz around the term "Internet of things" or "IoT" is ever increasing due to the fact that its impact on our society has the potential to be dramatic within a relatively short span of time.

IoT is the idea that just about every imaginable device that can provide either a control or monitoring function will someday have an IP address for access to the Internet. Cisco Systems calls it the "Internet of Everything", or the networked connection of people, processes, data, and things.

Imagine objects in your home, car, at work, and all around you having an IP address to connect to the cloud -providing immediate access via just about any device (Smart Phone, tablet, laptop, desktop computer, etc.).

And IoT is not just limited to devices; it's encroaching upon use with people and animals too! Livestock monitoring and tracking, medical devices for monitoring, and preventative medicine on humans are just some examples. The concept is to have multiple vertical sectors operating in one connected ecosystem.

IoT applications will require both wired and wireless networking infrastructures to operate.

Every device- such as a pressure sensor, temperature sensor, or flow control valve- will have an IP address that is connected to the internet or to an Ethernet network. Thus, any necessary equipment for Ethernet IP networks will be required.

L-com's products including Ethernet switches and converters, antennas and RF amplifiers are some examples of the products needed to support IoT applications.  As a designer and manufacturer of wired and wireless networking products we are excited to see where this IoT evolution will take us!

Other newsletters that may be of interest to you:
 
6/13/2016 The Benefits of 24 AWG Cable
5/24/2016 Why our Premium D-Sub Cables are Superior
5/17/2016 An A to Z review of the 802.11 standards
4/12/2016 USB Type-C Cable Assemblies Provide Legacy USB Connectivity
3/1/2016 Passive Intermodulation (PIM) Explained
2/2/2016 The Industrial Internet of Things (IIoT)
12/15/2015 Cable Shielding - How it Works
12/1/2015 Embedded Antennas and the IoT
11/10/2015 Long Live RS-232!
9/22/2015 The Differences between Solid and Stranded Cable
9/15/2015 Coaxial Connector Termination: Which Technique is Right for You
8/11/2015 802.11ah Breathes New Life to the 900 MHz Frequency Band
7/14/2015 Cable Options For Every Application
7/7/2015 900 MHz - Your NLOS Friend
6/2/2015 802.11ax Offers Blazing Fast Wi-Fi Connectivity
5/12/2015 The NBASE-T Alliance - Fostering Multi-Gig Speeds over Cat5e/6 Cabling
4/7/2015 L-com and The Internet of Things (IoT)
3/3/2015 802.3bt the Promise for Higher Power PoE
1/6/2015 L-com's Family of Brands - A Solution for Every Application
12/9/2014 Cat6a Products for High-Speed Networking
  Page:  1 of 15
    
 
Free Newsletter
L-com Global Connectivity           50 High Street           North Andover, MA 01845
www.L-com.com E-mail: sales@L-com.com 1-800-341-5266 www.Facebook.com/LcomGlobal


© Infinite Electronics International, Inc.