L-com Global Connectivity
  
Cart is Empty
  
USA & Canada (800) 341-5266     International +1 (978) 682-6936

802.3bt the Promise for Higher Power PoE
(Tuesday, March 03, 2015)
 

Today more than one million end devices are powered by Power over Ethernet (PoE).
One of the major benefits of PoE is that communications equipment such as IP phones and access points can be located where no AC power source is present or could not be installed due to the location of the equipment.
 
One limitation to the current standardized version of PoE is that the amount of power it provides to a device peaks at 25.5 Watts. This has limited PoE's penetration into other applications requiring more power.
 
To address the need for higher power PoE the IEEE has proposed a new standard, 802.3bt, which promises to double or even triple the power output of the current standard, 802.3at. Additionally the 802.3bt standard is looking to standardize PoE with 10Gbase-T.
 
L-com plans to support this new high powered version of PoE with innovative 802.3bt products and solutions when the standard becomes ratified.
 
While the details are being sorted out we continue to support 802.3af and 802.3at applications with a wide range of products that help you save time and money with your wired and wireless networking installations.

PoE Injectors and Splitters  PoE Injector Hubs
PoE Extenders PoE Ethernet Switches

 


Other newsletters that may be of interest to you:
 
6/13/2016 The Benefits of 24 AWG Cable
5/24/2016 Why our Premium D-Sub Cables are Superior
5/17/2016 An A to Z review of the 802.11 standards
4/12/2016 USB Type-C Cable Assemblies Provide Legacy USB Connectivity
3/1/2016 Passive Intermodulation (PIM) Explained
2/2/2016 The Industrial Internet of Things (IIoT)
12/15/2015 Cable Shielding - How it Works
12/1/2015 Embedded Antennas and the IoT
11/10/2015 Long Live RS-232!
9/22/2015 The Differences between Solid and Stranded Cable
9/15/2015 Coaxial Connector Termination: Which Technique is Right for You
8/11/2015 802.11ah Breathes New Life to the 900 MHz Frequency Band
7/14/2015 Cable Options For Every Application
7/7/2015 900 MHz - Your NLOS Friend
6/2/2015 802.11ax Offers Blazing Fast Wi-Fi Connectivity
5/12/2015 The NBASE-T Alliance - Fostering Multi-Gig Speeds over Cat5e/6 Cabling
4/7/2015 L-com and The Internet of Things (IoT)
3/3/2015 802.3bt the Promise for Higher Power PoE
1/6/2015 L-com's Family of Brands - A Solution for Every Application
12/9/2014 Cat6a Products for High-Speed Networking
  Page:  1 of 15
    
 
Free Newsletter



L-com Global Connectivity           50 High Street           North Andover, MA 01845
www.L-com.com E-mail: sales@L-com.com 1-800-341-5266 www.Facebook.com/LcomGlobal


© Infinite Electronics International, Inc.