L-com Global Connectivity
  
Cart is Empty
  
USA & Canada (800) 341-5266     International +1 (978) 682-6936
L-com explains RG-style coaxial cable
(Tuesday, June 18, 2013)
 
L-com home page
 
L-com explains RG-style coaxial cable
Easily Share This Email on Social Media Platforms
  Quick Order Free Catalog Custom / OEM New Products Sale Items  
This is part two of a two part series on coaxial cabling. Click here to see "L-com explains Low Loss coax cable".
L-com explains RG-style coax cable

As a follow up to our recent newsletter "L-com explains Low Loss coax cable", we wanted to explain the RG styles of coaxial cable. As one of the original standards for coaxial technology, the RG standard was created for the US military in the 1960's. The letters "RG" were used to stand for "Radio Guide" or "RF Government" (depending on who you ask) and were followed by a number which corresponded to a specific standard put forth for the different sets of specifications. Sometimes, a letter followed the number to specify some variations in the cable construction, and a "/U" was often included to stand for the "Universal" standard.

Over time, the robust coaxial technology came to be used in non-military commercial applications, and though the RG designations are still used today, there is no standardization to ensure every aspect of the cable is constant among manufacturers, so it helps to know the specifications of the cable you need.

This chart shows some of the RG-style coaxial cable types and applications still used today, over fifty years since they were designed:

Chart showing six of the most common RG-style coax cable types, with attenuation and nominal OD

You may notice that one of the key aspects of RG coax cables is the impedance. Unlike low-loss styles, which generally all have a 50 Ohm characteristic impedance, the RG styles can vary. Most often they are either 50 or 75 Ohms, but other impedances such as 92 Ohms also exist. Impedance is a complicated aspect to explain fully, though L-com has a helpful definition in its Coaxial Cable Tutorial. As a general rule of thumb, 75 Ohm cables are used in audio/video applications, and 50 Ohm cables are used in data applications. Due to the signal attenuation, the 50 Ohm RG cables are usually not appropriate for wireless applications, especially at longer lengths (which is why we recommend low-loss coax for wireless systems).

Click here to download our Low Loss coaxial cable applications guide  to download our RG coaxial cable applications guide.

L-com lists its 50 Ohm RG style coaxial bulk cable and cable assemblies in its Coaxial section, and the 75 Ohm RG style coaxial bulk cable and cable assemblies in its Audio/Video section.

Coaxial Connectors Tools Coaxial Terminators
Coaxial Connectors Coaxial crimping tools Coaxial Terminators

Friendly & Knowledgeable Service · In Stock Availability & Same Day Shipping · 100% Satisfaction Guaranteed

Other newsletters that may be of interest to you:
 
6/13/2016 The Benefits of 24 AWG Cable
5/24/2016 Why our Premium D-Sub Cables are Superior
5/17/2016 An A to Z review of the 802.11 standards
4/12/2016 USB Type-C Cable Assemblies Provide Legacy USB Connectivity
3/1/2016 Passive Intermodulation (PIM) Explained
2/2/2016 The Industrial Internet of Things (IIoT)
12/15/2015 Cable Shielding - How it Works
12/1/2015 Embedded Antennas and the IoT
11/10/2015 Long Live RS-232!
9/22/2015 The Differences between Solid and Stranded Cable
9/15/2015 Coaxial Connector Termination: Which Technique is Right for You
8/11/2015 802.11ah Breathes New Life to the 900 MHz Frequency Band
7/14/2015 Cable Options For Every Application
7/7/2015 900 MHz - Your NLOS Friend
6/2/2015 802.11ax Offers Blazing Fast Wi-Fi Connectivity
5/12/2015 The NBASE-T Alliance - Fostering Multi-Gig Speeds over Cat5e/6 Cabling
4/7/2015 L-com and The Internet of Things (IoT)
3/3/2015 802.3bt the Promise for Higher Power PoE
1/6/2015 L-com's Family of Brands - A Solution for Every Application
12/9/2014 Cat6a Products for High-Speed Networking
  Page:  1 of 15
    
 
Free Newsletter
L-com Global Connectivity           50 High Street           North Andover, MA 01845
www.L-com.com E-mail: sales@L-com.com 1-800-341-5266 www.Facebook.com/LcomGlobal


© Infinite Electronics International, Inc.