L-com Global Connectivity
  
Cart is Empty
  
USA & Canada (800) 341-5266     International +1 (978) 682-6936

What is a MIMO antenna? MIMO Antennas Explained
(Tuesday, December 11, 2012)
 
L-com home page
 
MIMO Antennas Explained
  Quick Order Free Catalog Custom / OEM New Products Sale Items  
What is a MIMO antenna? MIMO Antennas Explained

Multiple–Input Multiple-Output (MIMO) antennas have two or more antennas in a single physical package and are designed for use in IEEE 802.11n WiFi networks. By utilizing multiple antennas, data throughput and range are increased compared to a single antenna using the same radio transmit power. Additionally MIMO antennas improve link reliability and experience less fading than a single antenna system. By transmitting multiple data streams at the same time, wireless capacity is increased.

MIMO technology uses Multipath (when wireless signals “bounce” off of objects and arrive at the receiver at different times) to improve wireless performance. MIMO technology takes a single data stream and breaks it down into several separate data streams and sends it out over multiple antennas. This provides redundancy. The receiving MIMO antenna will “look” at each stream being sent to determine the strongest one to choose.

L-com stocks MIMO antennas in the following frequencies 2.4 GHz, 2.4/5.8 GHz, 3.5 GHz, 4.9/5.8 GHz, 5.1/5.8 GHz.

We also offer MIMO antennas in several different antenna form factors including:

Ceiling Mount MIMO antennas Omni directional MIMO Antennas
2.4 GHz 3 dBi Spatial Diversity MIMO Ceiling Antenna - 18in N-Female Connectors 2.4 GHz 10 dBi Dual Polarity Omnidirectional MIMO/802.11n Antenna - N-Female Connectors
Panel MIMO Antennas Sector MIMO Antennas
2.4 GHz 14 dBi Three Element, Dual Polarized Panel Antenna - N-Female Connectors 4.9-5.8 GHz Dual Polarity 17dBi Sector Antenna

Click here for the MIMO antenna product center

Friendly & Knowledgeable Service · In Stock Availability & Same Day Shipping · 100% Satisfaction Guaranteed

Other newsletters that may be of interest to you:
 
6/13/2016 The Benefits of 24 AWG Cable
5/24/2016 Why our Premium D-Sub Cables are Superior
5/17/2016 An A to Z review of the 802.11 standards
4/12/2016 USB Type-C Cable Assemblies Provide Legacy USB Connectivity
3/1/2016 Passive Intermodulation (PIM) Explained
2/2/2016 The Industrial Internet of Things (IIoT)
12/15/2015 Cable Shielding - How it Works
12/1/2015 Embedded Antennas and the IoT
11/10/2015 Long Live RS-232!
9/22/2015 The Differences between Solid and Stranded Cable
9/15/2015 Coaxial Connector Termination: Which Technique is Right for You
8/11/2015 802.11ah Breathes New Life to the 900 MHz Frequency Band
7/14/2015 Cable Options For Every Application
7/7/2015 900 MHz - Your NLOS Friend
6/2/2015 802.11ax Offers Blazing Fast Wi-Fi Connectivity
5/12/2015 The NBASE-T Alliance - Fostering Multi-Gig Speeds over Cat5e/6 Cabling
4/7/2015 L-com and The Internet of Things (IoT)
3/3/2015 802.3bt the Promise for Higher Power PoE
1/6/2015 L-com's Family of Brands - A Solution for Every Application
12/9/2014 Cat6a Products for High-Speed Networking
  Page:  1 of 15
    
 
Free Newsletter



L-com Global Connectivity           50 High Street           North Andover, MA 01845
www.L-com.com E-mail: sales@L-com.com 1-800-341-5266 www.Facebook.com/LcomGlobal


© Infinite Electronics International, Inc.