L-com Global Connectivity
  
Cart is Empty
  
USA & Canada (800) 341-5266     International +1 (978) 682-6936

To our valued customers: Our offices will be closed November 28th and 29th in observance of the Thanksgiving Day holiday.

Cable Management Accessories
(Tuesday, October 23, 2012)
 
L-com home page
 
Cable Management Accessories
  Quick Order Free Catalog Custom / OEM New Products Sale Items  
Cable Management Accessories

To the average consumer, the concept of cable management is minimal.  They may have four or five cables connecting their home theater or desktop setup, and use a tie wrap to keep it all together.  But there is a different, more essential form of cable management, that many IT professionals and network engineers are more familiar with: the wiring closet.  Setting up an office and running four or five hundred cables into a central closet and connecting them all up correctly is no menial chore, and keeping it organized and neat is very difficult, but very essential. A disorganized wiring closet has real costs, in the downtime for users and the time it takes for a technician to troubleshoot, isolate, and repair problems.

Fortunately, there are a lot of products available from L-com to drastically improve the organization of your wiring closet.

Cable Ties, Heat Shrink, and Tubing
A simple cable tie or tie-wrap

One of the simplest cable management accessories you can stock up on is the cable tie. They are cheap, abundantly available, and invaluable to have. L-com sells packages of 100 cable ties in various sizes. There are a few other, similar types of items that are small enough, light enough, and cheap enough for you to tack on to an order and then put in a desk drawer for emergency use. These items are things like heat shrink tubing (which is available in various sizes and contracts to form a tight seal when heated), expandable sleeving, and wrap tubing that allows greater flexibility and is less likely to damage the cables than cable ties.

Click here to learn more

Racks and Cable Management Products
Cable Management Panel for 19-inch Racks

A 19" steel rack is invaluable for mounting equipment and patch panels in a wiring closet. But you should always save a little space on your rack for cable management bars and panels. They are simple and easy to use, and will give your rack a "cable friendly" structure to keep things neat and organized. Along with the D-ring panels that are a staple, consider horizontal cable managers (which can come as a hinged version), horizontal cable trays, and lacer bars. Combining a lacer bar with the cable ties above is a great and easy way to keep the cables clear of equipment as they hang off of higher patch panels.

Click here to learn more

Color Coding and Labeling
A portable label printer helps organize any cabling project

One method that works well to keep wiring organized is a consistent color code. Many Ethernet cable assemblies and fiber optic cable assemblies come off-the-shelf in many different colors, enabling you to specify that all cables of a similar type or that come from a similar location have the same color. Then, when problems arise it is much easier to isolate and troubleshoot the problem, saving a lot of time and energy. Also, cable labelers are an investment that pays dividends later on. Spend a few minutes during setup to put a clear label on each wire or port, and later you're not fumbling with a toner to find the specific cable or port you need. Most labelers today are lightweight and portable, some with features like backlighting for darker rooms, and they allow a large variety of label texts and formats like die-cut labels.

Click here to learn more

Friendly & Knowledgeable Service · In Stock Availability & Same Day Shipping · 100% Satisfaction Guaranteed

Other newsletters that may be of interest to you:
 
6/13/2016 The Benefits of 24 AWG Cable
5/24/2016 Why our Premium D-Sub Cables are Superior
5/17/2016 An A to Z review of the 802.11 standards
4/12/2016 USB Type-C Cable Assemblies Provide Legacy USB Connectivity
3/1/2016 Passive Intermodulation (PIM) Explained
2/2/2016 The Industrial Internet of Things (IIoT)
12/15/2015 Cable Shielding - How it Works
12/1/2015 Embedded Antennas and the IoT
11/10/2015 Long Live RS-232!
9/22/2015 The Differences between Solid and Stranded Cable
9/15/2015 Coaxial Connector Termination: Which Technique is Right for You
8/11/2015 802.11ah Breathes New Life to the 900 MHz Frequency Band
7/14/2015 Cable Options For Every Application
7/7/2015 900 MHz - Your NLOS Friend
6/2/2015 802.11ax Offers Blazing Fast Wi-Fi Connectivity
5/12/2015 The NBASE-T Alliance - Fostering Multi-Gig Speeds over Cat5e/6 Cabling
4/7/2015 L-com and The Internet of Things (IoT)
3/3/2015 802.3bt the Promise for Higher Power PoE
1/6/2015 L-com's Family of Brands - A Solution for Every Application
12/9/2014 Cat6a Products for High-Speed Networking
  Page:  1 of 15
    
 
Free Newsletter



L-com Global Connectivity           50 High Street           North Andover, MA 01845
www.L-com.com E-mail: sales@L-com.com 1-800-341-5266 www.Facebook.com/LcomGlobal


© Infinite Electronics International, Inc.