L-com Global Connectivity
  
Cart is Empty
  
USA & Canada (800) 341-5266     International +1 (978) 682-6936
Customer-Premises Equipment for Wireless Networks
(Tuesday, May 22, 2012)
 
L-com Global Connectivity
 
Customer-Premises Equipment for Wireless Networks
  Quick Order Free Catalog Custom / OEM New Products Sale Items  

L-com Brand CPE Wireless Access Points

CPE Units mounted on poles

Today's wireless market, more specifically the outdoor wireless market, continues to demand higher transmit power, greater dependability and advanced feature sets, all while keeping the client-side cost down. L-com brand Customer-Premises Equipment (CPEs) are all-in-one cost-effective weatherproof wireless devices featuring high output power as well as all the essential features for both operating as an Access Point or a CPE Client. This dual approach offers greater flexibility and reduced inventory stock as these units can perform all that is required for establishing reliable wireless networks.

The L-com CPEs have been developed with all the latest enhancements in wireless security but also with backwards compatibility to fit into pre-existing networks. They feature WEP, WPA, WPA2, WPA-PSK, 802.1x as well as other security features to best meet your specific needs.

Two new models are available for all your WiFi coverage needs.

WLAN-LCCPE28-1

  • 2.4 GHz - IEEE 802.11b/g/n compliant
  • IP65 rated enclosure for outdoor use
  • Internal 8 dBi antenna plus port for external antenna
  • Access Point, Wireless Client, Bridge and Repeater modes
  • Includes PoE injector and power supply

WLAN-LCCPE516-1

  • 5.8 GHz - IEEE 802.11a/n compliant
  • IP65 rated enclosure for outdoor use
  • Dual-polarity 16 dBi internal antenna
  • Selectable 2x2 MIMO RF outputs for external antenna
  • Access Point, Wireless Client, Bridge and Repeater modes
  • Includes PoE injector and power supply

Four Operating Modes

Access Point (AP) Mode: Allows wireless equipment such as Smart Phones or Laptops to be connected to a wired network. In this mode the CPE unit is typically connected to a router on a wired network. Network/internet connectivity can then be provided to the wireless devices connected to the CPE unit. The CPE unit provides security features that allow only select wireless devices to connect to it.

Wireless Client Mode: In this mode the CPE unit connects to another active AP as if it was a wireless device like a Laptop. Once connected it can then provide network/internet connectivity to wired devices via its Ethernet port. This mode is ideal if you need to provide connectivity to devices without wireless functionality.

Bridge Mode: Wireless bridges are typically used to connect two or more network segments that are physically separated. Bridging mode is achieved by using Wireless Distribution System (WDS) settings in the CPE unit. This allows only the selected CPEs to communicate with each other and denies access to other wireless devices trying to access them. Bridges can be used in Point-to-Point or Point-to Multipoint applications. An example of a Point-to-Point bridge application is connecting two commercial buildings. An example of a Point-to-Multipoint application is connecting multiple buildings on a college campus.

Repeater Mode: This mode is used to extend the range of an existing AP. This mode is also ideal when an obstruction is preventing wireless connectivity within a select area. Repeaters are commonly used when providing wireless connectivity to multi-story buildings and large homes.

Different Applications

These CPE units can be used in any market that requires wireless network/internet connectivity. Common markets include:

  • Special Events/Convention Centers
  • Parks and Recreation Areas, Theme Parks
  • WISP providers
  • Commercial WiFi Installers
  • Residential, Home Users
  • Educational Facilities
  • State and Federal Complexes
  • Transportation Terminals (Air, Train, Bus, etc)

Click here to download the .pdf datasheet for the 2.4 GHz CPE unit.
Click here to download the .pdf datasheet for the 5.8 GHz CPE unit.

WLAN-LCCPE28-1

2.4 GHz 802.11b/g/n Outdoor CPE
WLAN-LCCPE516-1

5 GHz 802.11a/n Outdoor CPE
Components in WLAN-LCCPE28-1 Kit Components in WLAN-LCCPE516-1 Kit
RJ45 Jack for wired connection to device RJ45 Jacks for MIMO wired connection to device
Power over Ethernet (PoE) Injector Comes With Each Kit
Connect with L-com
Follow L-com on Twitter
Follow L-com on Facebook
Follow L-com on YouTube
Follow L-com on Google+
 
Latest News
Get the latest press releases from L-com here!

Helpful Links
L-com Home Page
Authorized Distributors
Custom Cables
Product Wizards
Product Comparisons
Technical Resources
Newsletter Archive
Newsletter Feedback
Friendly & Knowledgeable Service · In Stock Availability & Same Day Shipping · 100% Satisfaction Guaranteed

Other newsletters that may be of interest to you:
 
6/13/2016 The Benefits of 24 AWG Cable
5/24/2016 Why our Premium D-Sub Cables are Superior
5/17/2016 An A to Z review of the 802.11 standards
4/12/2016 USB Type-C Cable Assemblies Provide Legacy USB Connectivity
3/1/2016 Passive Intermodulation (PIM) Explained
2/2/2016 The Industrial Internet of Things (IIoT)
12/15/2015 Cable Shielding - How it Works
12/1/2015 Embedded Antennas and the IoT
11/10/2015 Long Live RS-232!
9/22/2015 The Differences between Solid and Stranded Cable
9/15/2015 Coaxial Connector Termination: Which Technique is Right for You
8/11/2015 802.11ah Breathes New Life to the 900 MHz Frequency Band
7/14/2015 Cable Options For Every Application
7/7/2015 900 MHz - Your NLOS Friend
6/2/2015 802.11ax Offers Blazing Fast Wi-Fi Connectivity
5/12/2015 The NBASE-T Alliance - Fostering Multi-Gig Speeds over Cat5e/6 Cabling
4/7/2015 L-com and The Internet of Things (IoT)
3/3/2015 802.3bt the Promise for Higher Power PoE
1/6/2015 L-com's Family of Brands - A Solution for Every Application
12/9/2014 Cat6a Products for High-Speed Networking
  Page:  1 of 15
    
 
Free Newsletter
L-com Global Connectivity           50 High Street           North Andover, MA 01845
www.L-com.com E-mail: sales@L-com.com 1-800-341-5266 www.Facebook.com/LcomGlobal


© Infinite Electronics International, Inc.