L-com Global Connectivity
  
Cart is Empty
  
USA & Canada (800) 341-5266     International +1 (978) 682-6936
PVC, LSZH, and Polyurethane: Know your cable jacket choices
(Tuesday, May 15, 2012)
 
L-com Global Connectivity
 
Cable Jacket Choices
  Quick Order Free Catalog Custom / OEM New Products Sale Items  
PVC, LSZH, and Polyurethane: Know your cable jacket choices Plenum, High Temperature Data Cable - Shielded, (25) 24 AWG Stranded Conductors, -40 C to 150 C

When you need to buy bulk cable or cable assemblies, you're probably concerned about things like conductor AWG size, shielding for EMI/RFI, connector molding construction, gold plating on the connectors and, ultimately, will the signal get from point A to point B quickly and with minimum loss or distortion.  That's a lot of factors to think about!  So why would you spare a thought to the jacket that just goes around the conductors?

It turns out that the cable jacket can be much more important than you may think.  Choosing the wrong cable jacket type can have implications in a range of things, from extending the life of your cable, to using the cable in the field, to basic health and safety.

Fire Codes
Click here to see L-com's video on jacket flammability codes.
Click here for a .pdf tip explaining some of the different cable jacket types.
Flammability and Toxicity Ratings on Different Cable Types

The most important aspect of any building or vehicle installation is how it impacts the safety of those working in and around it.  In particular, you should consider how the cable will respond in the event of a fire.  In most cases, a PVC jacket will be fine to use as a patch cord or for single in-wall runs.  But when you have many cables running in a confined space, like a Plenum area of an office building, there are a couple of dangers with using PVC jackets. 

The first danger is "leaping".  In a typical building, one of the first defenses against a catastrophe when a fire breaks out is to control the fire and stop it from quickly spreading. However, PVC cable jackets burn very easily and fire can actually "leap" from room to room or from floor to floor simply by burning along the cables in the Plenum.  For that reason, local and national building codes often require a Plenum rated jacket (sometimes called CMP, UL-910, or OFNP rated) which is self-extinguishing and will not allow the fire to burn along it.

The other danger is that PVC releases hazardous gasses when it burns. In a typical building with good fire exits, you can get out into the fresh air.  But for confined aerospace, marine, and military applications, getting outside isn't always an option.  In those cases, and in cases of rooms where it is not easy to get out quickly, you should always use a "low smoke zero halogen" cable (LSZH).

Cable Corrosion

Another problem with PVC is that it can corrode over time in certain conditions. One is oil.  PVC is a petroleum-based substance that will begin dissolving if coated with oil.  As oil and grease is common in busy factories and industrial settings, the life of a cable used there can be drastically improved by specifically getting an oil-resistant jacketed cable, such as Polyurethane.

Another condition that may reduce the life of a cable is UV exposure.  Cables that are installed where they may be in direct sunlight for extended periods of time will need to be replaced more often unless you pick a UV-resistant jacket.  Again, Polyurethane is a good choice, or any of several similar compounds (like Polyethylene, etc).  

Cable Colors

The color of a cable jacket is not merely an aesthetic choice. One of the advantages of cables and Typical Color Coding Setuppatch cords is that they can be unplugged or re-plugged to suit future needs. However, that only works if you plug the right cable into the right jack, and when you consider that future needs might not occur until months or years after an installation, you can understand the headaches that will occur at drop points and in cluttered wiring closets if the layout isn't clear. The easiest way to prevent these headaches is to set up a color-coded system from the start.  If you designated that blue cables always access the Ethernet, red cables for VoIP or phones, green cables for video security surveillance, etc., you will have a much easier time down the road.

Introducing new black-jacketed PVC premium double-shielded
D-Subminiature cables!


Premium Black D-sub 9 Position DB9 Male/Male Cables - Fully Populated, Double Shielded

Premium Black D-sub 15 Position DB15 Male/Male Cables - Fully Populated, Double Shielded

Premium Black D-sub 15 Position HD15 Male/Male Cables - Fully Populated, Double Shielded

Premium Black D-sub 25 Position DB25 Male/Male Cables - Fully Populated, Double Shielded

DB9 Cable Assemblies
Male to Male
Male to Female

DB15 Cable Assemblies
Male to Male
Male to Female

HD15 Cable Assemblies
Male to Male
Male to Female

DB25 Cable Assemblies
Male to Male
Male to Female

Connect with L-com
Follow L-com on Twitter
Follow L-com on Facebook
Follow L-com on YouTube
Follow L-com on Google+
 
Latest News
Get the latest press releases from L-com here!

Helpful Links
L-com Home Page
Authorized Distributors
Custom Cables
Product Wizards
Product Comparisons
Technical Resources
Newsletter Archive
Newsletter Feedback
Friendly & Knowledgeable Service · In Stock Availability & Same Day Shipping · 100% Satisfaction Guaranteed

Other newsletters that may be of interest to you:
 
6/13/2016 The Benefits of 24 AWG Cable
5/24/2016 Why our Premium D-Sub Cables are Superior
5/17/2016 An A to Z review of the 802.11 standards
4/12/2016 USB Type-C Cable Assemblies Provide Legacy USB Connectivity
3/1/2016 Passive Intermodulation (PIM) Explained
2/2/2016 The Industrial Internet of Things (IIoT)
12/15/2015 Cable Shielding - How it Works
12/1/2015 Embedded Antennas and the IoT
11/10/2015 Long Live RS-232!
9/22/2015 The Differences between Solid and Stranded Cable
9/15/2015 Coaxial Connector Termination: Which Technique is Right for You
8/11/2015 802.11ah Breathes New Life to the 900 MHz Frequency Band
7/14/2015 Cable Options For Every Application
7/7/2015 900 MHz - Your NLOS Friend
6/2/2015 802.11ax Offers Blazing Fast Wi-Fi Connectivity
5/12/2015 The NBASE-T Alliance - Fostering Multi-Gig Speeds over Cat5e/6 Cabling
4/7/2015 L-com and The Internet of Things (IoT)
3/3/2015 802.3bt the Promise for Higher Power PoE
1/6/2015 L-com's Family of Brands - A Solution for Every Application
12/9/2014 Cat6a Products for High-Speed Networking
  Page:  1 of 15
    
 
Free Newsletter
L-com Global Connectivity           50 High Street           North Andover, MA 01845
www.L-com.com E-mail: sales@L-com.com 1-800-341-5266 www.Facebook.com/LcomGlobal


© Infinite Electronics International, Inc.