Gearing up for Wi-Fi 6

September 19, 2019 at 8:00 AM

 

I don’t know about you, but we are definitely looking forward to the debut of Wi-Fi 6 later this year. This next generation Wi-Fi standard improves on the current 802.11ac standard with more than just faster speeds. So let’s take a closer look at what’s in store.

 

First, Wi-Fi 6, also known as 802.11 ax, is backwards compatible with its predecessor, 802.11ac (now deemed Wi-Fi 5). Wi-Fi 6 was created to help support the increasing number of devices in today’s homes and businesses. If you have a lot of devices connected, several smart home devices or if you’re using virtual reality devices, a Wi-Fi 6 router might be a great fit.

 

So how fast is it? Wi-Fi 6 is capable of streaming up to 9.6 Gbps and has delivered transfer speeds of 1,320 Mbps in some tests. That is around 30%-40% faster than 802.11 ac, and for US customers, it will be 1,000% times faster than the current average download speed of 119 Mbps.

 

How is this possible? Wi-Fi 6 utilizes 1024-QAM to deliver more data and more efficiency, along with a wider 160 MHz channel for faster speeds. This new standard also takes advantage of 8x8 uplink/downlink, MU-MIMO, OFDMA and BSS Color for a capacity that is up to 4 times larger and able to handle more devices.

 

As with any Wi-Fi standard, much of the speed capability will depend on the speed being delivered by your internet service provider (ISP). In order to take full advantage of Wi-Fi 6 speeds, you’ll need a plan with your ISP that is capable of delivering high speeds, as your plan acts much like a speed limit on how fast your internet connection can go. Plus, you’ll need both a Wi-Fi 6 router and Wi-Fi 6 capable devices to benefit from Wi-Fi 6 speeds. So hold on tight, because Wi-Fi 6 capable routers and devices are already rolling out and are sure to become standard in next generation wireless devices.

 

© L-com, Inc. All Rights Reserved. L-com, Inc., 50 High Street, West Mill, Third Floor, Suite 30, MA 01845