How Network Security is Changing

November 29, 2018 at 8:00 AM

 

With more users providing more information on more networks, and some of those networks being breached, it’s no wonder that network security is a hot topic for many people and businesses. In fact, network security is a top concern for many IT administrators. For, as network technology has become more advanced, so have the ways in which those networks can be hacked. Here, we’ll take a look some of the changes happening in network security to counteract those threats.

 

·        Network security will no longer be a small branch of IT, but rather a responsibility that encompasses the entire organization. The network is a part of every aspect of IT and thus it will need to be protected by all administrators. Plus, the network itself should be armed with tools to help avoid attacks by reinforcing network-based security such as firewalls and malware prevention.  

 

·        Today, so many things are being sent to the Cloud, and so will security. Many IT departments will take advantage of cloud-based services that will manage common security tasks as part of a contracted agreement. This allows a simple subscription plan to impart dynamic security measures that once took several hours for administrators to manage. Multi-Cloud security management platforms will also come into play to allow network security to be managed across public and private clouds via a single security control plane.

 

·        We’ve all seen the IT email alert go out warning of an email scam sent to employees to get them to click a link that then installs malware on the network. Because of these types of attacks, end-point security has become a priority. This has extended to include mobile device management for non-corporate owned devices. In the future, many of these end-point security measures will be simplified and condense the number of protection tools in place to provide better overall protection.

 

·        Penetration (pen) testing is a valuable tool used to detect security gaps that might not have been identified by IT staff. Outside firms are often hired to perform this testing for a true outside party perspective, but the service can be costly and needs to be done in a timely manner. With the development of new AI and automation technology, pen testing is becoming easier and less expensive, meaning that it can be done more often, which is especially beneficial to keep up with the increase of new viruses, malware and other cyber threats.

  

With these upgrades in network security, along with an increased focus on overarching enterprise wide security procedures, today’s networks will be able to keep up with tomorrow’s technology and do it securely.

 

© L-com, Inc. All Rights Reserved. L-com, Inc., 50 High Street, West Mill, Third Floor, Suite 30, North Andover, MA 01845