411 on 5G

November 1, 2018 at 8:00 AM

 

For the past few years, the world of technology has been abuzz with talk about the 5th generation mobile wireless (5G), and with full-scale rollouts set to begin next year, all that buzz can be expected to become a swarm. For example, when wireless networks transitioned from 3G to 4G, there were incremental improvements in technology and performance, but the upgrade from 4G to 5G is expected to be a complete revolution of wireless and connectivity. To make sure you’re prepared to take part in the revolution, here’s the 411 to get you up to speed on 5G.

 

The goal of the 5G network is to create a platform that makes it possible to deliver global connection. This means being able to connect everyone and everything, everywhere around the globe. In addition to that, 5G systems are slated to deliver data rates that far surpass 4G in a wider coverage area, while being more power efficient and reliable, presenting lower latency, supporting faster moving equipment and the influx of communication stemming from the Internet of Things (IoT). Plus, 5G will not only support mobile wireless users, it will also include enhanced wireless connectivity technology for use in applications such as automotive, smart homes, augmented and virtual reality.

 

In order to cross into all of those markets, the specifications for 5G performance have been debated and defined. The finalized specifications were set to be released by the International Telecommunications Union (ITU) and the 3rd Generation Partnership Project (3GPP) in 2020. Though mobile operators and service providers are urging the standardization organizations to accelerate that timetable.

 

With so much uncertainty still looming over the finalization of the standard, early releases are not shaping up exactly as planned. In the meantime, the non-standalone 5G new radio (NSA 5G NR) is the interim 5G specification and will help ease the transition from 4G to 5G. The NSA 5G NR supports many aspects of 5G including the sub-6 GHz spectrum, frequency bands, carrier aggregation and MIMO. With the new 5G frequency bands, NSA 5G NR is capable of 5G-like performance while utilizing existing technologies and infrastructure. This interim specification will provide the groundwork for future trials and deployments and allow for the technology to be better understood for the full 5G rollout.

 

With the excitement of early 5G availability, there have also been new application opportunities emerging that include fixed wireless (FWS) to the home. This development would use 5G wireless technology to provide last mile data services including television, home internet and voice-over-IP (VoIP) phone calling. As the launch of early 5G gets closer, there are bound to be additional new and existing applications to arise that would benefit from 5G’s lower latency, increased data rates and enhanced reliability. Until then, we will have to wait with great anticipation for the arrival of 5G.

 

Posted in: Wireless

Tags: , , , , ,

© L-com, Inc. All Rights Reserved. L-com, Inc., 50 High Street, West Mill, Third Floor, Suite 30, MA 01845