Hangin' Tough - Armored Cables

October 11, 2018 at 8:00 AM

 

When your cables need serious protection and the ability to stand up to the toughest conditions, an armored jacket might be the perfect solution. Armored cables are cables with a metal or plastic covering that provides a layer of protection that is much stronger than any traditional type of cable jacket. This suit of armor makes the cables extra tough and durable, now let’s take a look at just how tough they are.

 

The rugged characteristics of armored cables make them ideal for outdoor, industrial and military applications where these features are of the upmost importance. This includes factory automation, manufacturing and chemical and petroleum processing networks.

 

One of the biggest advantages of armored cables is there crush resistance rating. L-com’s metal armored cables offer a crush resistance of up to 1,500 PSI

which makes them well suited for just about any military or industrial application. Additionally these cables feature stainless steel armor that stands up to corrosion often found in extreme environments.

 

Plastic armor, although not as rugged as metal armor, offers an extra level of crush and abrasion resistance

when compared to non-armored cable jackets. L-com’s plastic armored cables feature a crush resistance of up 800PSI.

 

Even with all that armor, these cables are still capable of high speed transmission rates. Plus, they are offered in multiple varieties to suit a wide range of applications, including armored Ethernet, armored USB, armored HDMI, armored D-sub and armored DVI cable assemblies.

 

No doubt, armored cables are tough enough to withstand the abuse that might be faced in harsh environments and rugged conditions, and if you don’t believe us, watch this.

 

© L-com, Inc. All Rights Reserved. L-com, Inc., 50 High Street, West Mill, Third Floor, Suite 30, North Andover, MA 01845