Case Study: Union Electrica

September 27, 2018 at 8:00 AM

 

Union Electrica, a systems design and installation services company based in Uruguay and servicing all of Latin America, won a large contract with the city of Medellin, Columbia. They were tasked with the challenge of deploying a WiMAX network that connected more than 1,200 subscriber points, but they needed help. Fortunately, L-com had the perfect solution.

 

To successfully complete the WiMAX network rollout in Medellin, Union Electronica needed a system that would support the 3.5 GHz frequency with a focused directional wireless connection that could perform in all weather conditions. They also required low-loss cables and lightning and surge protectors to complete the installation.

 

L-com was able to fulfill all of Union Electrica’s network requirements with a 3.5 GHz antenna that was compact, minimized interference, supported vertical or horizontal polarization and featured a 25° beamwidth.

 

The L-com team also provided low-loss coaxial cable assemblies, surge protectors and COTS antennas and accessories, all of which were in-stock and available for immediate shipment to fulfill the accelerated installation schedule.

 

In the end, with the help of L-com, Union Electrica was able to successfully deliver a high-speed WiMAX network to the city of Medellin while meeting all budget and installation deadline requirements.

 

To read the entire case study click here.

 

© L-com, Inc. All Rights Reserved. L-com, Inc., 50 High Street, West Mill, Third Floor, Suite 30, North Andover, MA 01845