411 on Near-Field Communications (NFC)

September 6, 2018 at 8:00 AM

 

In this wild world of wireless technology, more and more short range communications standards are being introduced to support all of those wireless devices. As the name suggests, short range communication standards transmit over shorter distances than long range technologies, but they are still quite capable and are ideal for specialized applications. One standard in this short range category is near-field communications (NFC), used for communication between devices and secure payment applications like Apple Pay. In this post we’ll explore all you need to know about NFC and how it might replace your wallet.

 

NFC It is an ultra-short-range technology created for contactless communication between devices. It can be used with phones, tablets and laptops to share data with other NFC-enabled devices. It allows two-way communication without the use of Wi-Fi, 3G, LTE or any other wireless connection. Developed from radio-frequency identification (RFID) technology, NFC is similar in that it uses radio waves, but is limited to approximately 4 inches of communication distance, which is largely viewed as a security benefit and is helping to boost the popularity of NFC. One of the most popular uses is for secure payment applications, like Apple Pay, Android Pay and Samsung Pay, which transmit mobile payments that are dynamically encrypted.

 

NFC operates on the 13.56 MHz ISM frequency and unlike other short range communications like Bluetooth, NFC doesn’t require any device discovery or pairing to begin transferring data. With NFC, a connection is immediately established when another NFC-enabled device is within the 4-inch operating range. Once a contactless transaction is initiated, the NFC reader and device pass encrypted information back and forth to complete the process in mere seconds – making it not only easy, but much faster than conventional payment and data transfer options.

 

In addition to secure payment applications, there are other uses for the technology too. NFC can be used to transfer lots of other data between NFC-equipped devices. This includes sending a phone number, picture or document, sharing directions, launching an app on someone else’s phone and connecting with NFC tags (small, physical tags that contain NFC chips).

 

With the ease of use and convenience of NFC, soon we might need cash, cards or a wallet much less than we do now, if at all. Even more convenient is the fact that NFC is already installed in many smart phones. For a complete list of NFC-equipped devices, check out this list from NFC world.

  

© L-com, Inc. All Rights Reserved. L-com, Inc., 50 High Street, West Mill, Third Floor, Suite 30, North Andover, MA 01845