Case Study: Lineage Logistics

May 10, 2018 at 8:00 AM

 

As the second largest cold storage thrid-party provider in the US, Lineage Logistics provides cold storage solutions for leading grocery, food and retail  companies.

 

During a wireless network roll-out in their warehouses, Lineage Logistics needed to add multiple access points inside refrigeration units with temperatures as low as -40 degrees. The company’s engineers had designed a wireless access point that fulfilled the needs of the project, but wasn’t able to function unprotected in the cold temperatures.

 

Lineage Logistics began searching for an enclosure that would protect their access point, offer Power over Ethernet (PoE) over a single cable and meet cost requirements.

 

After rejecting a competitor’s offering, as it didn’t fully meet the requirements, Lineage Logistics came to L-com for help. Our team was able to develop a comprehensive solution that met all their needs. We created a custom NEMA enclosure that could house the access point and provide plently of room if adjustments were needed. We were also able to save Lineage Logistics time and money on installation by mounting the access points in the enclosures and providing all required cabling and antennas.

  

L-com was able to not only meet, but surpass this client’s expectations with the perfect solution to their problem.

 

To read the full case study, click here.

 

© L-com, Inc. All Rights Reserved. L-com, Inc., 50 High Street, West Mill, Third Floor, Suite 30, North Andover, MA 01845