HDMI & DVI - Your Questions Answered

October 5, 2017 at 8:00 AM


HDMI and DVI cables are the two most popular video cables used today. Both HDMI and DVI far outperform traditional VGA cables cables that only transmit analog video signals. These digital interconnects are used to link everything from desktop computers and LCD monitors to HDTV’s and entertainment sysyems.


DVI is commonly used to connect computers to monitors. They are the most similar to traditional VGA with 24 pins that support analog and digital video. DVI can stream up to 1920x1200 HD video pixels, or up to 2560x1600 pixels using dual-link DVI technology. If the DVI cable or port does not have all 24 pins, it is designed for lower resolution devices, but as long as all the pins are accounted for, it should be able to support the maximum resolution. One downfall of DVI is that it doesn’t support HDCP encryption by default, which means you may not be able to play full HD Blu-rays or other HD content if your harware only includes DVI ports.


HDMI is the standard cable used on newer HDTVs, Blu-ray players, Apple TVs, computers and many other video devices. HDMI cables and ports are easy to use and connect with no pins to align, it’s a simple plug and play connection similar to USB. These cables can stream both digital video and audio at the same time. They support up to 1920x1200 HD video and 8 channel audio, as well as HDCP for the newest HD content. HDMI is the first industry supported, uncompressed, all digital audio/video interface and is backwards compatible with DVI-D.



Still have questions? Here are some of the most frequently asked questions our support team gets asked about HDMI and DVI:


 -  What is the maximum length for a DVI cable?

  •    A DVI-D signal can travel 5 meters over a single cable. For distances longer than 5 meters, a DVI extender/repeater is needed.


 -  What is the maximum length for an HDMI cable?

  •    A HDMI signal can travel 5 meters over a single 28 AWG cable. A HDMI extender/repeater is needed for distances longer than 5    meters.


 -  When using a long HDMI cable, the monitor display is blank or the resolution looks bad. Why?

  •   Currently, HDMI cables up to 5 meters in length will operate properly. If the cable is longer than 5 meters, the signal begins to       degrade and a signal extender is needed.


 -  Can I get a HDMI to DVI adaptor?

  •   HDMI is only compatible with single-link DVI-D and single-link DVI-I. It is not compatible with DVI-A, dual-link DVI-D or dual-link      DVI-I, the adaptors will plug-in but will not work for these formats.


 -  Can I get a HDMI to VGA adaptor?

  •   No, HDMI is not compatible with VGA.


Posted in: Wired

Tags: , , , , , ,

© L-com, Inc. All Rights Reserved. L-com, Inc., 50 High Street, West Mill, Third Floor, Suite 30, MA 01845