Video Blog: Solid vs. Stranded Center Conductors

July 27, 2017 at 8:00 AM

 

All cables have either a solid and stranded conductor, no matter if they’re Cat5e, Cat6 or any other category rating. To figure out whether a solid or stranded cable will work best for your application, you’ll need to look at the advantages and disadvantages of both.

 

A solid cable’s conductors are made of solid metal, usually copper, making the cable more rigid.  Solid cables are typically used as infrastructure cabling in walls, ceilings and conduit where flexibility isn’t necessary because the cables aren’t moved after installation. They are also cheaper and transmit better over long distances with lower attenuation than stranded cable, but they are more likely to break if bent repeatedly.

 

Stranded cables are much more flexible because their conductors are made of thin metal wires that are twisted together to create a larger, thicker conductor. These cables are frequently used as patch cords and in shorter network cable runs that need extra flexibility.  Stranded cables are typically more expensive than solid cables, but they work well for shorter distances and can stand-up to repetitive bending without breaking.

 

There are other factors to take into consideration when choosing a cable. For more information on which cable type is best for your application, watch our video blog.

 

© L-com, Inc. All Rights Reserved. L-com, Inc., 50 High Street, West Mill, Third Floor, Suite 30, North Andover, MA 01845