How Wired & Wireless Technology Is Helping Healthcare

June 29, 2017 at 8:00 AM

 

Healthcare is a hot topic right now. It is something that touches everyone’s lives at some point, though we might not think about the technology that goes into building healthcare devices and keeping hospitals running smoothly. Here, we’ll look at the healthcare industry and how technology is used in devices and to build communications networks to keep medical centers connected.

 

OEM Medical Devices

 

A medical device may only be as good as the parts that it’s made ofand if you’re ever in need of a defibrillator, you’re surely going to want it to have been constructed with quality parts. Medical manufacturers use all types of connectivity products to build medical devices, these include USB cables and adapters, HDMI, VGA and D-subminiature cables and adapters. For all of these parts, there are strict design requirements that must be met to comply with federal safety regulations.  We work with medical device OEMs around the world to provide solutions to fit their requirements to build medical devices that will perform when they’re needed most.

 

In-Building Wireless Networks

 

Many of today’s hospitals and medical facilities have replaced old-school patient charts with portable, wireless tablets to keep track of patient information and records. Thus, they depend on reliable cellular and Wi-Fi coverage to keep devices used by doctors and nurses connected, plus those used by patients and visitors. Distributed antenna systems (DAS), access points, RF amplifiers and low-loss coaxial cables are used to ensure that medical staff and patients can stay connected with seamless cellular and Wi-Fi coverage.

 

Medical Campus Networks

 

When a medical facility spans across several separate buildings, a high-speed communications network is needed to share vital information such as patient records and test results. Wireless point-to multipoint networks use directional and Omni-directional antennas to send wireless signals throughout the campus. If a wireless network can’t be used because Line of Sight conditions are less that optimal, a wired fiber backbone can be implemented to connect the buildings. In this case, an intricate network of fiber cabling, media converters, routers and Ethernet switches are employed to provide comprehensive campus-wide coverage.

 

Wired Infrastructure/Data Center

 

Within hospitals and medical centers there can be numerous floors that all need to be connected to a main data center. A wide variety of cabling and connectivity products are used to build this wired communications infrastructure from the ground up, running from the IDFs to the data center.  Category 5e/6/6a cables, OFNP and LSZH cables, server racks, patch panels, switches, routers and more are all used to build a high-speed, fault-tolerant medical communications network to keep every floor, device and user connected.

 

For more information on how wired and wireless technology is helping healthcare, and how L-com’s products are being used, read our full healthcare industry overview.

 

© L-com, Inc. All Rights Reserved. L-com, Inc., 50 High Street, West Mill, Third Floor, Suite 30, MA 01845