Have you ever noticed that when multiple devices use your Wi-Fi connection, you get much slower download speeds and choppy video streams? This is because your Wi-Fi router probably uses single-user multiple-input, multiple-output (SU-MIMO), which means that all of your devices have to take turns because the router can only service one device at a time. This problem will soon be a thing of the past, with the next evolution of MIMO: Multi-user multiple-input, multiple-output (MU-MIMO).
MU-MIMO and is set to revolutionize the wireless networking world by allowing Wi-Fi routers to do something they’ve never done before – simultaneously send data to multiple devices. Instead of your phone, TV and tablet taking turns receiving transmissions from the router, MU-MIMO will allow all of your devices to simultaneously download data.
How MU-MIMO Works
Wireless routers are good at sending data, but they can only send it in one direction. This means they can only talk to one device at a time. With SU-MIMO, the router sends little bits of information, very quickly, one at a time to multiple devices – kind of like a data machine gun. You are likely to never notice this break in service, but because the router can only focus on one device at a time, your wireless internet connection slows down when there are multiple devices connected.
MU-MIMO eliminates sluggish Wi-Fi speeds by allowing the router to simultaneously transmit data to multiple wireless devices. The router communicates with all of the devices at the same time using a separate stream for each device, as if each has its own personal router. It provides a more dependable, faster Wi-Fi connection because each device doesn’t have to share a data stream with other devices. This brings about a noticeable improvement for video streaming or other high-data tasks, even when more devices are connected.
Benefits of MU-MIMO

MU-MIMO will improve everyday Wi-Fi use by making networks vastly more efficient.Not only will networks be faster, they will also have an increased network capacity. This means that home networks will be able to handle more Wi-Fi devices and public Wi-Fi networks with a lot of users will also perform better.
In order to utilize MU-MIMO, the devices must support the technology but non-MIMO devices will also see improved performance. With MU-MIMO devices being served more quickly, there will be more time for SU-MIMO and other devices to communicate with the router.
MU-MIMO devices are not required to have multiple antennas or perform as much signal processing as SU-MIMO requires. MU-MIMO also utilizes an easier, standardized beamforming method which will allow different manufacturers to support MU-MIMO technology more easily than they could with 802.11ac and SU-MIMO implementations. This new technology is also cheaper to implement and doesn’t require sophisticated Wi-Fi devices, unlike SU-MIMO. This is likely to result in more devices supporting the technology, and thus a bigger impact on Wi-Fi networks as a whole.
Plus, with MU-MIMO, data sent from the router to Wi-Fi devices can only be read by the intended recipient, the data is unreadable by other people/devices. The data is essentially encrypted, which provides an additional layer of protection for users.
Limitations of MU-MIMO
As great as MU-MIMO is, there are some limitations. To get the full benefit, the router and device must support MU-MIMO. MU-MIMO was added to the 802.11ac standard in 2013 and is slowly being incorporated into some products, but is not yet widely available.
Currently, MU-MIMO standards can service four devices downloading at the same time. Adding more devices will require them to share a data stream, leading to the same issues experienced with SU-MIMO. The technology also only works on the downlink connection (from the router to devices) it doesn’t improve uplink connections (data incoming to the router, i.e. an upload to the Internet).
MU-MIMO also works best with stationary devices. If you are walking around your house while watching a video on your phone, you will not get the full benefit.
MU-MIMO is one of the most impactful emerging technologies to hit the market in recent history. Allowing multiple devices to simultaneously download has the potential to revolutionize the world of wireless networking.
For more general information on MIMO, read our blog post How MIMO Can Help You.