Advantages of Fiber Cabling You May Not Have Considered

September 11, 2014 at 10:00 AM

 

 

First things first, we aren’t claiming that fiber is outright better than copper cabling.

 

We understand that as data and network design requirements vary, some applications may need copper cabling. In these cases, copper is likely the best choice and perfectly suited for that network or application.

 

What we ARE saying is that in other instances there may be advantages to using fiber in your application. 

 

When you consider the many elements that are involved in designing your network- such as cost, dependability, durability, resources, space, etc.- it will be helpful to know more about how using fiber can positively impact your network.

 

As with any technology related implementation, one might also want to consider the environmental impact that the network will have. Fiber has some environmental advantages that we will go over. 

 

So here they are, the facts about why fiber could be beneficial to your application!

1.       It generally requires less power

 

Overall, fiber uses less power to transmit at a longer distance.

 

Look at redundancy, for example. Copper backbones and Intermediate Distribution Frames (IDFs) could be converted to fiber optic direct from a centralized data center all the way to the desktop. When you eliminate the need for IDFs, you eliminate the need for all the extra space, cooling, cabling and power backup they require. This will generally mean less power consumption, especially at longer distances.

 

Copper also has limited run distances, so getting data from point A to point B can be an issue if the connection exceeds 100 meters, whereas fiber provides much further distance support.  

 

If you absolutely need copper, consider that higher quality copper cables result in less re-transmission of data and therefore less power consumption. Also, inexpensive and portable Wireless CPE units can be used remotely to provide a secondary communications link when fiber cannot be installed due to cost or physical barriers.

 

Note that fiber optic media converters can help transition your copper network to fiber optics if you choose a hybrid network design.

 

 

2.       Saves on Resources

 

Why? Fiber is lighter by nature of its composition. Therefore supporting structures can be less robust.

 

Also, since fiber runs all the way to the destination without a repeater for most networks, there is less need for intermediary network closets which saves on floor space and power consumption.  This also saves on HVAC needs too (which provides energy savings).

3.       Efficiency

 

Fiber cabling is as good as it gets for efficiency and security in network applications.  This is because it is free from threat of corrosion and is resistant to atmospheric conditions such as lightning or other electrical interference. Fiber is also resistant to environments where vibration and EMI/RFI interference might be present. And, fiber-optic cables don’t interfere with other devices.

 

Fiber proves its efficiency especially when you look at the use of materials over time for upgrading. Upgrades can be rather difficult with copper wire, though not with fiber because the real capacity of fiber is only partially utilized at today's network speeds. Cable and telephone providers often use fiber because it gives them greater reliability with the opportunity to offer new services, such as digital phone service and internet connections. 

 

With fiber cabling the signal also has a constrained loss rate, which means that very little signal is lost over rather long distances. Lastly, fiber is very hard to tap and steal data from since it transfers data with light.

 

 

4.       Saves on Waste

 

To put it into perspective, one fiber cable can do the work of TEN copper cables. That’s less material being used for manufacturing, thus less material ending up at the landfill.

 

As mentioned above, the reduced need for upgrading fiber networks also saves on waste as you are disposing of fewer cables over time.

  

All points considered, choosing the best connectivity media for your application is a balancing act. Armed with the facts you need about the implications of fiber technology, now you can consider what is most important to you and what best suits the requirements of your network.

 

© L-com, Inc. All Rights Reserved. L-com, Inc., 50 High Street, West Mill, Third Floor, Suite 30, MA 01845