How We’re Launching into the Future of Fiber & Wireless Technologies

May 1, 2014 at 10:00 AM

 

Picture this:

 

You’ve consistently worked hard on keeping up with the latest technologies and standards so that you can be the best in your business.

 

You’re confident in your knowledge and technique.

 

Then you get the call that you’re in. They want you.

 

And you have the opportunity to present this knowledge in front of some really important people……

 

That’s how we feel this month!

 

We’re honored to announce that we’ve been given the chance to present at a technology seminar at the Kennedy Space Center.

 

In the wave of 21st century technology, our sights are set on all that the future holds for our industry and we couldn’t be more proud to be a part of it. On Friday, May 9, 2014, our product managers and wireless application specialists will be presenting wireless application trends and the future of fiber optic communications. For NASA!

 


The Facts on Fiber

 

Our team plans to discuss a variety of fiber optic technology trends and future applications. The first will explain and examine the increasingly relevant crossover between commercial and military grade products.

 

It’s a common misconception that if an organization is qualified as a “government” or “military” entity, it absolutely must use military grade fiber products. This isn’t necessarily the case. What we want to emphasize is that it’s important to analyze all characteristics and factors within the application in order to get the best product match, as well as the best use of one’s money. 

 

For example: a military grade cable might be applicable in a certain outdoor location where large trucks and tanks run over it. But, if each end of that cable runs into a building where it‘s protected, a commercial grade connector or cable assembly could likely be a viable option.

 

It’s also important for us to mention how fiber has evolved. Fiber is no longer just a delicate and expensive cable option. Not only is fiber capable of being used in a rugged application, but it is also an efficient green choice that saves energy. To put this into perspective- one single fiber cable can be run 100 kilometers without a connection break-up or even having to use additional electrical repeater equipment for support along the way.

 

Other fiber optic topics that we’ll discuss are port density, cable weight, and the relatively new MPO connectors. Our hands-on discussion will also focus on how advancements in RF and optical networks will help NASA achieve new design insight. 

 

Lastly, we plan to touch on the topic of security in relation to fiber optics. In the past it was believed that fiber cable was “un-tapable.” However, there is knowledge to prove that fiber actually can be tapped into, so it might be worth considering taking certain safety precautions for the security of the data being passed.

 

 

What about Wireless?

 

In addition to our focus on fiber technology, we will also hold a technical discussion about the next generation Wi-Fi standard, 802.11ac technology. 802.11ac has the ability to support up to eight MIMO spatial streams, with a lot more functionality. Check out our recent post about 802.11ac technology here.

 

In relation to 802.11ac, we will also discuss MIMO technology and using MIMO compliant dual polarity antennas. Our presentation will include the latest in new MIMO wireless technology that provides improved spectral efficiency along with increased link capacity and reliability.  

 

By utilizing multiple antennas you can increase the data throughput and range, compared to a single antenna using the same radio transmit power. Additionally, MIMO antennas improve link reliability and experience less fading than a single antenna system. By transmitting multiple data streams at the same time, wireless capacity is increased.

 

Overall, there's lots of exciting stuff propagating in the world of wireless and fiber optic technology.


What do you foresee in the future?


© L-com, Inc. All Rights Reserved. L-com, Inc., 50 High Street, West Mill, Third Floor, Suite 30, North Andover, MA 01845