802.11ac: What’s all the buzz about?

March 13, 2014 at 10:00 AM

 

Amidst the bustling and overpopulated race to find better, faster WiFi, there now exists a new wireless standard that will help you get there. You may even come in first place.

 

The latest IEEE standard for wireless networking, 802.11ac, is bringing high speed gigabit wireless connectivity to business, home, and government communications systems everywhere. 802.11ac offers up to 1 Gbps wireless transmissions and the ability to support up to eight MIMO spatial streams as well as 80 MHz channel bandwidth. This new advancement in wireless technology promises flawless voice, video, and data transmission to multiple end users at the same time.

 

If slow WiFi has you feeling down, 802.11ac is worth looking into.

 

802.11ac delivers faster throughput and better range than the previous 802.11n standard. 802.11n can deliver up to 600 Mbps with four spatial streams using one 40 MHz-wide channel. 802.11ac is engineered to deliver up to 1Gbps which translates to higher data rates and happier end users.

 

The new amendment’s ultimate intention is to achieve higher multi-user throughput in wireless local area networks (WLANs) and improve WLAN user experience especially for bandwidth intensive applications such as streaming voice and video.

Here at L-com, we continue to support the latest standardized technologies by offering high quality, high performance products, including those for 802.11ac applications.

 

Our series of 802.11ac indoor and outdoor WiFi antennas feature 2.4-5.8 GHz operation for a variety of applications. L-com currently offers 802.11ac ceiling antennas, panel antennas, rubber duck antennas, and Omni antennas.

 

© L-com, Inc. All Rights Reserved. L-com, Inc., 50 High Street, West Mill, Third Floor, Suite 30, MA 01845