How to Utilize an RF Splitter

February 6, 2014 at 10:00 AM

 

True or False: Will an RF splitter help connect more than one antenna to a single radio?

 

The answer is true. This question commonly comes up at our technical service department so we wanted to share the facts with you.

  

A Radio Frequency (RF) Splitter/Combiner is a transmission component which divides or sums power between two or more ports. Typically they are used for connecting more than one antenna to a single radio and can also be used to connect multiple radios to a single antenna using the same frequency.

 

Generally most RF splitter products are 2 way, 3 way, or 4 way, and can split a variety of RF signals. At L-com, we offer RF splitters for 900 MHz, 2.4 GHz, and 3.5 GHz, 5.4 GHz, and 5.8 GHz WLAN applications. Additionally, we offer wideband 750 MHz to 2.4 GHz RF splitter/RF combiners which are ideal for DAS applications.

 

RF splitters have weatherproof construction and can be installed indoors or outdoors. These flexible splitters can be used with amplified systems since they will pass DC power to all ports. Remember as always, the type of RF splitter you need would vary depending on your application.

 

The following are some examples of an RF splitter in action:

 

 

 

By using a 2-way splitter in an application that requires wireless coverage on two sides of a building, a single radio can be used to feed two separate antennas covering two sides of the building.

The corner mounting bracket used in this design example is available for purchase.

  

 

© L-com, Inc. All Rights Reserved. L-com, Inc., 50 High Street, West Mill, Third Floor, Suite 30, MA 01845